<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX6ull DDR Test Tool</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-DDR-Test-Tool/m-p/1548534#M197188</link>
    <description>&lt;P&gt;Hi b45499&lt;BR /&gt;&lt;BR /&gt;The explanation was insufficient.&lt;BR /&gt;198MHz is the CPU core clock setting, not the DDR clock.&lt;BR /&gt;&lt;BR /&gt;I figured out what was causing the lock.&lt;BR /&gt;VDD_ARM voltage was too low when CPU core clock was set to 198MHz.&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;Best regards,&lt;BR /&gt;Koji Okuda&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 04 Nov 2022 00:03:32 GMT</pubDate>
    <dc:creator>okuda</dc:creator>
    <dc:date>2022-11-04T00:03:32Z</dc:date>
    <item>
      <title>iMX6ull DDR Test Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-DDR-Test-Tool/m-p/1542326#M196733</link>
      <description>&lt;P&gt;Hi.&lt;BR /&gt;&lt;BR /&gt;Currently, as shown in the attached image, a board using iMX6ull is being used for memory testing using DDR Test Tool.&lt;BR /&gt;&lt;BR /&gt;Which register of iMX6ull corresponds to the value of MR1 (setting value framed in red)?&lt;BR /&gt;&lt;BR /&gt;What effect does changing this value have?&lt;BR /&gt;（The default value is 0, and 8031 in the image is a meaningless value.）&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Koji Okuda&lt;/P&gt;</description>
      <pubDate>Mon, 24 Oct 2022 01:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-DDR-Test-Tool/m-p/1542326#M196733</guid>
      <dc:creator>okuda</dc:creator>
      <dc:date>2022-10-24T01:32:03Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ull DDR Test Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-DDR-Test-Tool/m-p/1543297#M196814</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;We suspected DDR memory from the phenomenon that kernel locks.&lt;BR /&gt;&lt;BR /&gt;As we proceeded with the investigation, we found the following.&lt;BR /&gt;&lt;BR /&gt;Currently, we are using it on demand, and when the clock setting is set to 198MHz, we found that the kernel cannot start normally.&lt;BR /&gt;With the fixed setting to high performance, the kernel starts fine.&lt;BR /&gt;&lt;BR /&gt;Anything wrong when the clock setting is set to 198MHz?&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Koji Okuda&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Oct 2022 09:11:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-DDR-Test-Tool/m-p/1543297#M196814</guid>
      <dc:creator>okuda</dc:creator>
      <dc:date>2022-10-25T09:11:18Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ull DDR Test Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-DDR-Test-Tool/m-p/1548255#M197167</link>
      <description>&lt;P&gt;You can refer to this &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M-Mini-Register-Programming-Aid-DRAM-PLL-setting/ta-p/1112094" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M-Mini-Register-Programming-Aid-DRAM-PLL-setting/ta-p/1112094&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I think you do not have proper clock for the 198MHz&lt;/P&gt;</description>
      <pubDate>Thu, 03 Nov 2022 11:03:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-DDR-Test-Tool/m-p/1548255#M197167</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2022-11-03T11:03:56Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ull DDR Test Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-DDR-Test-Tool/m-p/1548534#M197188</link>
      <description>&lt;P&gt;Hi b45499&lt;BR /&gt;&lt;BR /&gt;The explanation was insufficient.&lt;BR /&gt;198MHz is the CPU core clock setting, not the DDR clock.&lt;BR /&gt;&lt;BR /&gt;I figured out what was causing the lock.&lt;BR /&gt;VDD_ARM voltage was too low when CPU core clock was set to 198MHz.&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;Best regards,&lt;BR /&gt;Koji Okuda&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Nov 2022 00:03:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-DDR-Test-Tool/m-p/1548534#M197188</guid>
      <dc:creator>okuda</dc:creator>
      <dc:date>2022-11-04T00:03:32Z</dc:date>
    </item>
  </channel>
</rss>