<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8MP: SError how to debug source in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1548325#M197176</link>
    <description>&lt;P&gt;Actually I note that the RXD line is pulled low rather than high. This could be generating a continuous serial line BREAK condition. Could the ttymxc1 driver be doing something with this and due to a driver timing bug this is generating the SError somehow ?&lt;/P&gt;</description>
    <pubDate>Thu, 03 Nov 2022 13:19:15 GMT</pubDate>
    <dc:creator>TerryBarnaby1</dc:creator>
    <dc:date>2022-11-03T13:19:15Z</dc:date>
    <item>
      <title>IMX8MP: SError how to debug source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1546846#M197064</link>
      <description>&lt;P&gt;We have a custom IMX8MP board, based on the IMX8MP-EVK board, that runs for many hours doing video processing work with no issues. LPDDR4 passes memory stress test and all other tests we have tried.&lt;/P&gt;&lt;P&gt;However occasionally, when we power off or reboot the board and sometimes at powerup there is an SError thrown. See: &lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Yocto-hardknott-hang-on-poweroff-reboot/td-p/1544726" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Yocto-hardknott-hang-on-poweroff-reboot/td-p/1544726&lt;/A&gt;. Its a bit random in that changing things "appears" to affect the failure, for example adding a USB disk affects it and simply connecting the UART2_RXD line to a USB to serial lead that is showing ttymxc1 console printouts appears to eliminate it or at least make it happen less often. (UART2_RXD is connected like the IMX8MP-EVK board via a voltage translator chip).&lt;/P&gt;&lt;P&gt;We normally see this SError reported at the code address imx_uart_readl although sometimes there are no kernel messages just a cutoff printk message.&lt;/P&gt;&lt;P&gt;My question here is how to find out what caused the SError ? As far as I understand it one of the IMX8MP hardware blocks outside of the ARM CPU core generated it but how to find out which one ?&lt;/P&gt;&lt;P&gt;Terry&lt;/P&gt;</description>
      <pubDate>Tue, 01 Nov 2022 10:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1546846#M197064</guid>
      <dc:creator>TerryBarnaby1</dc:creator>
      <dc:date>2022-11-01T10:34:12Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP: SError how to debug source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1548006#M197141</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183571"&gt;@TerryBarnaby1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you share your design about uart?&lt;/P&gt;</description>
      <pubDate>Thu, 03 Nov 2022 02:39:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1548006#M197141</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-11-03T02:39:26Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP: SError how to debug source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1548060#M197147</link>
      <description>&lt;P&gt;Attached is the UART2 schematic (pieced together from overall schematic). I don't think this is a cause of the problem, just affects the issue somehow as the problem occurs fairly randomly and appears to be affected by timings of things that I suspect the kernel printk's affect.&lt;/P&gt;&lt;P&gt;However the main thing I want to find out is how to work out what caused an SError when it occurs ?&lt;/P&gt;</description>
      <pubDate>Thu, 03 Nov 2022 05:47:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1548060#M197147</guid>
      <dc:creator>TerryBarnaby1</dc:creator>
      <dc:date>2022-11-03T05:47:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP: SError how to debug source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1548325#M197176</link>
      <description>&lt;P&gt;Actually I note that the RXD line is pulled low rather than high. This could be generating a continuous serial line BREAK condition. Could the ttymxc1 driver be doing something with this and due to a driver timing bug this is generating the SError somehow ?&lt;/P&gt;</description>
      <pubDate>Thu, 03 Nov 2022 13:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1548325#M197176</guid>
      <dc:creator>TerryBarnaby1</dc:creator>
      <dc:date>2022-11-03T13:19:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP: SError how to debug source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1549333#M197245</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183571"&gt;@TerryBarnaby1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The SError normally caused by accessing the memory system, can you add more print to confirm this error happened in which uart ?&lt;/P&gt;
&lt;P&gt;From the comment, the&amp;nbsp;&lt;SPAN&gt;UCR2_SRST is cached, this could cause the SError.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;static u32 imx_uart_readl(struct imx_port *sport, u32 offset)
{
	switch (offset) {
	case UCR1:
		return sport-&amp;gt;ucr1;
		break;
	case UCR2:
		/*
		 * UCR2_SRST is the only bit in the cached registers that might
		 * differ from the value that was last written. As it only
		 * automatically becomes one after being cleared, reread
		 * conditionally.
		 */
		if (!(sport-&amp;gt;ucr2 &amp;amp; UCR2_SRST))
			sport-&amp;gt;ucr2 = readl(sport-&amp;gt;port.membase + offset);
		return sport-&amp;gt;ucr2;
		break;
	case UCR3:
		return sport-&amp;gt;ucr3;
		break;
	case UCR4:
		return sport-&amp;gt;ucr4;
		break;&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you use UART2 RXD test point to reproduce this issue on EVK?&lt;/P&gt;</description>
      <pubDate>Mon, 07 Nov 2022 06:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1549333#M197245</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-11-07T06:27:28Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP: SError how to debug source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1551009#M197358</link>
      <description>&lt;P&gt;"The SError normally caused by accessing the memory system, can you add more print to confirm this error happened in which uart ?". I am pretty sure this is with UART2, no others are in use. Obviously as it is an SError the kernel backtrace may not be related to where the SError happened.&lt;/P&gt;&lt;P&gt;"From the comment, the UCR2_SRST is cached, this could cause the SError.", actually UCR2_SRST is the only bit that is not read from memory cache but is read directly from the UART's registers. I did note that there was code in the uart driver that turns of the UART hardware clock for some reasons, maybe something has switched this off ?&lt;/P&gt;&lt;P&gt;"Can you use UART2 RXD test point to reproduce this issue on EVK?" I guess I can remove a resistor and tie the UART2_RXD line low to test. However it has taken me three weeks of work to get to a position where I can relatively reliably (within an hour or so) catch this fairly random fault. It obviously has a timing aspect. I think that using the EVK and start EVK code could be a 3 week or more job to get another example failure. So as I have a reasonable way to get the failure in my environment I would like to dig down and try and track down the source. Hence I need to find out why the SError occurred and if an address access what address.&lt;/P&gt;&lt;P&gt;Isn't there a standard way of determining what caused an SError interrupt on an IMX8MP ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the SError was generated due to some memory access issue, how do I find out what cause the SError and what memory location was being accessed ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Nov 2022 11:07:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-SError-how-to-debug-source/m-p/1551009#M197358</guid>
      <dc:creator>TerryBarnaby1</dc:creator>
      <dc:date>2022-11-09T11:07:00Z</dc:date>
    </item>
  </channel>
</rss>