<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 8MQ启动失败 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/8MQ%E5%90%AF%E5%8A%A8%E5%A4%B1%E8%B4%A5/m-p/1547690#M197115</link>
    <description>&lt;P&gt;king a node at [mem 0x0000000000000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] NUMA: NODE_DATA [mem 0xbffb7e00-0xbffb9bff]&lt;BR /&gt;[ 0.000000] Zone ranges:&lt;BR /&gt;[ 0.000000] DMA [mem 0x0000000040000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] Normal empty&lt;BR /&gt;[ 0.000000] Movable zone start for each node&lt;BR /&gt;[ 0.000000] Early memory node ranges&lt;BR /&gt;[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000b7ffffff]&lt;BR /&gt;[ 0.000000] node 0: [mem 0x00000000b8400000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] psci: probing for conduit method from DT.&lt;BR /&gt;[ 0.000000] psci: PSCIv1.1 detected in firmware.&lt;BR /&gt;[ 0.000000] psci: Using standard PSCI v0.2 function IDs&lt;BR /&gt;[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.&lt;BR /&gt;[ 0.000000] psci: SMC Calling Convention v1.1&lt;BR /&gt;[ 0.000000] percpu: Embedded 24 pages/cpu @ffff80007ff52000 s57624 r8192 d32488 u98304&lt;BR /&gt;[ 0.000000] Detected VIPT I-cache on CPU0&lt;BR /&gt;[ 0.000000] CPU features: enabling workaround for ARM erratum 845719&lt;BR /&gt;[ 0.000000] Speculative Store Bypass Disable mitigation not required&lt;BR /&gt;[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 515072&lt;BR /&gt;[ 0.000000] Policy zone: DMA&lt;BR /&gt;[ 0.000000] Kernel command line: console=ttymxc0,115200 earlycon=ec_imx6q,0x30860000,115200 root=/dev/mmcblk0p3 rootwait rw macaddr=&lt;BR /&gt;[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)&lt;BR /&gt;[ 0.000000] Memory: 1052472K/2093056K available (14140K kernel code, 1716K rwdata, 6368K rodata, 1280K init, 435K bss, 57544K reserved, 983040K cma-reserved)&lt;BR /&gt;[ 0.000000] Virtual kernel memory layout:&lt;BR /&gt;[ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB)&lt;BR /&gt;[ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB)&lt;BR /&gt;[ 0.000000] .text : 0xffff000008080000 - 0xffff000008e50000 ( 14144 KB)&lt;BR /&gt;[ 0.000000] .rodata : 0xffff000008e50000 - 0xffff000009490000 ( 6400 KB)&lt;BR /&gt;[ 0.000000] .init : 0xffff000009490000 - 0xffff0000095d0000 ( 1280 KB)&lt;BR /&gt;[ 0.000000] .data : 0xffff0000095d0000 - 0xffff00000977d200 ( 1717 KB)&lt;BR /&gt;[ 0.000000] .bss : 0xffff00000977d200 - 0xffff0000097e9f69 ( 436 KB)&lt;BR /&gt;[ 0.000000] fixed : 0xffff7dfffe7f9000 - 0xffff7dfffec00000 ( 4124 KB)&lt;BR /&gt;[ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB)&lt;BR /&gt;[ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum)&lt;BR /&gt;[ 0.000000] 0xffff7e0000000000 - 0xffff7e0002000000 ( 32 MB actual)&lt;BR /&gt;[ 0.000000] memory : 0xffff800000000000 - 0xffff800080000000 ( 2048 MB)&lt;BR /&gt;[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;BR /&gt;[ 0.000000] Preemptible hierarchical RCU implementation.&lt;BR /&gt;[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4.&lt;BR /&gt;[ 0.000000] Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] RCU: Adjusting geometry for rcu_fanout_▒&lt;/P&gt;&lt;P&gt;板子出现概率启动失败的现象，Log打印如上，求解？？？&lt;/P&gt;</description>
    <pubDate>Wed, 02 Nov 2022 10:04:32 GMT</pubDate>
    <dc:creator>Zyj</dc:creator>
    <dc:date>2022-11-02T10:04:32Z</dc:date>
    <item>
      <title>8MQ启动失败</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MQ%E5%90%AF%E5%8A%A8%E5%A4%B1%E8%B4%A5/m-p/1547690#M197115</link>
      <description>&lt;P&gt;king a node at [mem 0x0000000000000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] NUMA: NODE_DATA [mem 0xbffb7e00-0xbffb9bff]&lt;BR /&gt;[ 0.000000] Zone ranges:&lt;BR /&gt;[ 0.000000] DMA [mem 0x0000000040000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] Normal empty&lt;BR /&gt;[ 0.000000] Movable zone start for each node&lt;BR /&gt;[ 0.000000] Early memory node ranges&lt;BR /&gt;[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000b7ffffff]&lt;BR /&gt;[ 0.000000] node 0: [mem 0x00000000b8400000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] psci: probing for conduit method from DT.&lt;BR /&gt;[ 0.000000] psci: PSCIv1.1 detected in firmware.&lt;BR /&gt;[ 0.000000] psci: Using standard PSCI v0.2 function IDs&lt;BR /&gt;[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.&lt;BR /&gt;[ 0.000000] psci: SMC Calling Convention v1.1&lt;BR /&gt;[ 0.000000] percpu: Embedded 24 pages/cpu @ffff80007ff52000 s57624 r8192 d32488 u98304&lt;BR /&gt;[ 0.000000] Detected VIPT I-cache on CPU0&lt;BR /&gt;[ 0.000000] CPU features: enabling workaround for ARM erratum 845719&lt;BR /&gt;[ 0.000000] Speculative Store Bypass Disable mitigation not required&lt;BR /&gt;[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 515072&lt;BR /&gt;[ 0.000000] Policy zone: DMA&lt;BR /&gt;[ 0.000000] Kernel command line: console=ttymxc0,115200 earlycon=ec_imx6q,0x30860000,115200 root=/dev/mmcblk0p3 rootwait rw macaddr=&lt;BR /&gt;[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)&lt;BR /&gt;[ 0.000000] Memory: 1052472K/2093056K available (14140K kernel code, 1716K rwdata, 6368K rodata, 1280K init, 435K bss, 57544K reserved, 983040K cma-reserved)&lt;BR /&gt;[ 0.000000] Virtual kernel memory layout:&lt;BR /&gt;[ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB)&lt;BR /&gt;[ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB)&lt;BR /&gt;[ 0.000000] .text : 0xffff000008080000 - 0xffff000008e50000 ( 14144 KB)&lt;BR /&gt;[ 0.000000] .rodata : 0xffff000008e50000 - 0xffff000009490000 ( 6400 KB)&lt;BR /&gt;[ 0.000000] .init : 0xffff000009490000 - 0xffff0000095d0000 ( 1280 KB)&lt;BR /&gt;[ 0.000000] .data : 0xffff0000095d0000 - 0xffff00000977d200 ( 1717 KB)&lt;BR /&gt;[ 0.000000] .bss : 0xffff00000977d200 - 0xffff0000097e9f69 ( 436 KB)&lt;BR /&gt;[ 0.000000] fixed : 0xffff7dfffe7f9000 - 0xffff7dfffec00000 ( 4124 KB)&lt;BR /&gt;[ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB)&lt;BR /&gt;[ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum)&lt;BR /&gt;[ 0.000000] 0xffff7e0000000000 - 0xffff7e0002000000 ( 32 MB actual)&lt;BR /&gt;[ 0.000000] memory : 0xffff800000000000 - 0xffff800080000000 ( 2048 MB)&lt;BR /&gt;[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;BR /&gt;[ 0.000000] Preemptible hierarchical RCU implementation.&lt;BR /&gt;[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4.&lt;BR /&gt;[ 0.000000] Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] RCU: Adjusting geometry for rcu_fanout_▒&lt;/P&gt;&lt;P&gt;板子出现概率启动失败的现象，Log打印如上，求解？？？&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 10:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MQ%E5%90%AF%E5%8A%A8%E5%A4%B1%E8%B4%A5/m-p/1547690#M197115</guid>
      <dc:creator>Zyj</dc:creator>
      <dc:date>2022-11-02T10:04:32Z</dc:date>
    </item>
    <item>
      <title>Re: 8MQ启动失败</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MQ%E5%90%AF%E5%8A%A8%E5%A4%B1%E8%B4%A5/m-p/1552030#M197433</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, it will fail, please rebuild again the bsp and burn again.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Thu, 10 Nov 2022 14:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MQ%E5%90%AF%E5%8A%A8%E5%A4%B1%E8%B4%A5/m-p/1552030#M197433</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-11-10T14:25:47Z</dc:date>
    </item>
  </channel>
</rss>