<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8m-plus Basler daA4200-30mci camera not using Pylon software in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1544182#M196877</link>
    <description>&lt;P&gt;Hi Diana&lt;/P&gt;&lt;P&gt;Thank you for your feedback which I often find very helpful.&lt;/P&gt;&lt;P&gt;The current statement from Basler is that&amp;nbsp;basler-daa4200-30mci is only accessible via Basler Pylon software. Gstreamer support is provided via extra Pylon-plugin&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.baslerweb.com/en/company/news-press/news/pylon-gstreamer-plug-in-for-basler-cameras/877440/" target="_blank"&gt;https://www.baslerweb.com/en/company/news-press/news/pylon-gstreamer-plug-in-for-basler-cameras/877440/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I did not tested this yet but if it works fine, I don't mind using that.&lt;/P&gt;</description>
    <pubDate>Wed, 26 Oct 2022 15:55:52 GMT</pubDate>
    <dc:creator>malik_cisse</dc:creator>
    <dc:date>2022-10-26T15:55:52Z</dc:date>
    <item>
      <title>imx8m-plus Basler daA4200-30mci camera not using Pylon software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1539506#M196503</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Hi,&lt;BR /&gt;Is there a way to launch Basler daA4200-30mci camera module not using Pylon software.&lt;BR /&gt;&amp;nbsp;I was able to make the camera module work from within Basler's Pylon software UI interface.&lt;BR /&gt;&lt;BR /&gt;However I would also like to use the camera using gst-launch-1.0 (gstreamer command line) directly since this would be the way the QT application will use the camera.&lt;BR /&gt;So far I am unable to see any video playing when using similar commands to:&lt;BR /&gt;gst-launch-1.0 v4l2src device=/dev/video1 ! waylandsink&lt;BR /&gt;&lt;BR /&gt;also variants to this command will not give any error messages but no video is playing.&lt;BR /&gt;Any idea?&lt;BR /&gt;Thank you&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Oct 2022 16:36:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1539506#M196503</guid>
      <dc:creator>malik_cisse</dc:creator>
      <dc:date>2022-10-18T16:36:28Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m-plus Basler daA4200-30mci camera not using Pylon software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1539735#M196523</link>
      <description>&lt;P&gt;did you use nxp imx8mp board and demo images? if yes, current bsp supports this with gstreamer as default, this is from my test&lt;/P&gt;
&lt;P&gt;root@imx8mpevk:~# gst-launch-1.0 -v v4l2src ! "video/x-raw,width=3840,height=2160" ! waylandsink&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;Pipeline is live and does not need PREROLL ...&lt;BR /&gt;Pipeline is PREROLLED ...&lt;BR /&gt;Setting pipeline to PLAYING ...&lt;BR /&gt;New clock: GstSystemClock&lt;BR /&gt;/GstPipeline:pipeline0/GstV4l2Src:v4l2src0.GstPad:src: caps = video/x-raw, width=(int)3840, height=(int)2160, format=(string)YUY2, framerate=(fraction)30/1, colorimetry=(string)2:6:5:1&lt;BR /&gt;/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-raw, width=(int)3840, height=(int)2160, format=(string)YUY2, framerate=(fraction)30/1, colorimetry=(string)2:6:5:1&lt;BR /&gt;/GstPipeline:pipeline0/GstWaylandSink:waylandsink0.GstPad:sink: caps = video/x-raw, width=(int)3840, height=(int)2160, format=(string)YUY2, framerate=(fraction)30/1, colorimetry=(string)2:6:5:1&lt;BR /&gt;/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-raw, width=(int)3840, height=(int)2160, format=(string)YUY2, framerate=(fraction)30/1, colo[ 91.271506] unsupported dwe command 259&lt;BR /&gt;rimetry=(string)2:6:5:1&lt;BR /&gt;[ 91.271513] unsupported dwe command 260&lt;BR /&gt;[ 91.371595] enter isp_mi_stop&lt;BR /&gt;[ 91.380610] Not supported 3dnr&lt;BR /&gt;[ 91.911276] unsupported function isp_disable_bls&lt;BR /&gt;[ 91.911287] unsupported function isp_s_bls&lt;BR /&gt;[ 91.915991] unsupported function isp_enable_bls&lt;BR /&gt;[ 91.920136] unsupported function isp_enable_bls&lt;BR /&gt;[ 91.924712] enter isp_s_comp&lt;BR /&gt;[ 91.932180] enter isp_s_comp&lt;BR /&gt;[ 91.935205] enter isp_s_comp&lt;BR /&gt;[ 91.950880] enter isp_s_comp&lt;BR /&gt;[ 91.953892] enter wdr3_hw_init&lt;BR /&gt;[ 91.957021] wdr3 res: 3840 2160&lt;BR /&gt;[ 91.960861] enter isp_mi_start&lt;BR /&gt;[ 97.118141] ###### 30.49 fps ######&lt;BR /&gt;^Chandling interrupt.&lt;BR /&gt;Interrupt: Stopping pipeline ...&lt;BR /&gt;Execution ended after 0:00:08.425076875&lt;BR /&gt;Setting pipeline to NULL ...&lt;BR /&gt;[ 99.652238] enter isp_mi_stop&lt;BR /&gt;Total showed frames (227), playing for (0:00:08.425097500), fps (26.943).&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 04:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1539735#M196523</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-10-19T04:03:04Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m-plus Basler daA4200-30mci camera not using Pylon software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1539874#M196529</link>
      <description>&lt;P&gt;Hi Joanxie,&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;&lt;STRONG&gt;DART-MX8M-PLUS Evaluation Kit from Variscite:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.variscite.com/product/system-on-module-som/cortex-a53-krait/dart-mx8m-plus-nxp-i-mx-8m-plus/" target="_blank"&gt;https://www.variscite.com/product/system-on-module-som/cortex-a53-krait/dart-mx8m-plus-nxp-i-mx-8m-plus/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Are you sure you are&amp;nbsp;&lt;SPAN&gt;Basler daA4200-30mc? From your debug log I can see that imx8mp embedded ISP is used however&amp;nbsp;daA4200-30mci has its own independent&amp;nbsp;inbuilt ISP and it does not use imx8mp-ISP.&amp;nbsp;daA4200-30mci is rather based on ISI interface directly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Therefore I am not sure if your example uses this particular camera module.&lt;BR /&gt;Please give me your thoughts on this,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR, M.Cisse&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 07:39:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1539874#M196529</guid>
      <dc:creator>malik_cisse</dc:creator>
      <dc:date>2022-10-19T07:39:33Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m-plus Basler daA4200-30mci camera not using Pylon software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1541041#M196617</link>
      <description>&lt;P&gt;my module is DEV KIT DAA3840-30MC -IMXSAS, and which uses ISP, since you use the third party company board, I suggest that you can contact them to double confirm&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 09:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1541041#M196617</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-10-20T09:21:20Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m-plus Basler daA4200-30mci camera not using Pylon software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1541118#M196624</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/109210"&gt;@malik_cisse&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Did you check&amp;nbsp;&lt;A href="https://github.com/basler/meta-basler-imx8" target="_blank"&gt;https://github.com/basler/meta-basler-imx8&lt;/A&gt;&amp;nbsp;? I think it should be helpful. It's a yocto layer for Basler dart BCON MIPI cameras for i.MX8 platform.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I've seen they list in the example:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;
&lt;BLOCKQUOTE&gt;daA2500-60mci connected on CSI1, no camera on CSI2: imx8mp-evk-basler-isi0.dtb&lt;/BLOCKQUOTE&gt;
&lt;/LI&gt;
&lt;/UL&gt;
&lt;P class="1666263906278"&gt;It's not the same camera as yours, but it still has in-built ISP. Unfortunately we don't have any other Basler camera to test except for daA&lt;SPAN&gt;3840-30mc.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P class="1666263906278"&gt;Let me know what you think.&lt;/P&gt;
&lt;P class="1666263906278"&gt;Best regards,&lt;/P&gt;
&lt;P class="1666263906278"&gt;Diana&lt;/P&gt;
&lt;P class="1666263906278"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 11:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1541118#M196624</guid>
      <dc:creator>dianapredescu</dc:creator>
      <dc:date>2022-10-20T11:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m-plus Basler daA4200-30mci camera not using Pylon software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1544182#M196877</link>
      <description>&lt;P&gt;Hi Diana&lt;/P&gt;&lt;P&gt;Thank you for your feedback which I often find very helpful.&lt;/P&gt;&lt;P&gt;The current statement from Basler is that&amp;nbsp;basler-daa4200-30mci is only accessible via Basler Pylon software. Gstreamer support is provided via extra Pylon-plugin&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.baslerweb.com/en/company/news-press/news/pylon-gstreamer-plug-in-for-basler-cameras/877440/" target="_blank"&gt;https://www.baslerweb.com/en/company/news-press/news/pylon-gstreamer-plug-in-for-basler-cameras/877440/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I did not tested this yet but if it works fine, I don't mind using that.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Oct 2022 15:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1544182#M196877</guid>
      <dc:creator>malik_cisse</dc:creator>
      <dc:date>2022-10-26T15:55:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m-plus Basler daA4200-30mci camera not using Pylon software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1544829#M196918</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/109210"&gt;@malik_cisse&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for the information. Please let me know if you manage to build and try that &lt;EM&gt;pylonsrc&lt;/EM&gt; plugin. I might be interested as well. I'll&amp;nbsp;let you know if I'm going to try it on my side.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Diana&lt;/P&gt;</description>
      <pubDate>Thu, 27 Oct 2022 07:50:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1544829#M196918</guid>
      <dc:creator>dianapredescu</dc:creator>
      <dc:date>2022-10-27T07:50:54Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m-plus Basler daA4200-30mci camera not using Pylon software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1603846#M201881</link>
      <description>&lt;P&gt;How can I build the pluin with yocto?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Feb 2023 16:49:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-Basler-daA4200-30mci-camera-not-using-Pylon-software/m-p/1603846#M201881</guid>
      <dc:creator>dadi</dc:creator>
      <dc:date>2023-02-22T16:49:59Z</dc:date>
    </item>
  </channel>
</rss>