<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSignificant difference of AI inference result between CPU and NPU</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Significant-difference-of-AI-inference-result-between-CPU-and/m-p/1542452#M196749</link>
    <description>&lt;P&gt;Hi NXP AI Champs&lt;/P&gt;&lt;P&gt;We have some test result from bladder size calculation.&lt;/P&gt;&lt;P&gt;The project is to find out the size of the bladder by AI.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;They use Onnx, and made AI inference with CPU and NPU with the same quantized onnx model learned.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, even with the same quantized onnx model, the size (image) of the bladder inferred by the CPU is significantly about 10%–30% less than the size (image) of the bladder inferred by the NPU. There's also the opposite.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When measured with 105 input data, most of them differ by about 10%, and about 30 differ by more than 30%. It doesn't even show a certain proportion.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If they used the same Quantified onnx model, shouldn't the inference images of the CPU and NPU be almost the same? I would like to ask you an answer to this question, and if there is any way to solve it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 24 Oct 2022 06:03:07 GMT</pubDate>
    <dc:creator>JK-IMX</dc:creator>
    <dc:date>2022-10-24T06:03:07Z</dc:date>
    <item>
      <title>Significant difference of AI inference result between CPU and NPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Significant-difference-of-AI-inference-result-between-CPU-and/m-p/1542452#M196749</link>
      <description>&lt;P&gt;Hi NXP AI Champs&lt;/P&gt;&lt;P&gt;We have some test result from bladder size calculation.&lt;/P&gt;&lt;P&gt;The project is to find out the size of the bladder by AI.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;They use Onnx, and made AI inference with CPU and NPU with the same quantized onnx model learned.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, even with the same quantized onnx model, the size (image) of the bladder inferred by the CPU is significantly about 10%–30% less than the size (image) of the bladder inferred by the NPU. There's also the opposite.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When measured with 105 input data, most of them differ by about 10%, and about 30 differ by more than 30%. It doesn't even show a certain proportion.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If they used the same Quantified onnx model, shouldn't the inference images of the CPU and NPU be almost the same? I would like to ask you an answer to this question, and if there is any way to solve it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Oct 2022 06:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Significant-difference-of-AI-inference-result-between-CPU-and/m-p/1542452#M196749</guid>
      <dc:creator>JK-IMX</dc:creator>
      <dc:date>2022-10-24T06:03:07Z</dc:date>
    </item>
    <item>
      <title>Re: Significant difference of AI inference result between CPU and NPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Significant-difference-of-AI-inference-result-between-CPU-and/m-p/1542513#M196755</link>
      <description>&lt;P&gt;what processor do you use&lt;/P&gt;</description>
      <pubDate>Mon, 24 Oct 2022 07:53:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Significant-difference-of-AI-inference-result-between-CPU-and/m-p/1542513#M196755</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-10-24T07:53:20Z</dc:date>
    </item>
    <item>
      <title>Re: Significant difference of AI inference result between CPU and NPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Significant-difference-of-AI-inference-result-between-CPU-and/m-p/1542603#M196763</link>
      <description>&lt;P&gt;Hi Joanxie&lt;/P&gt;&lt;P&gt;The AP is used with i.MX 8M Plus&lt;/P&gt;&lt;P&gt;Part# :&amp;nbsp;MIMX8ML8DVNLZAB (i.MX8M Plus)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Oct 2022 09:23:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Significant-difference-of-AI-inference-result-between-CPU-and/m-p/1542603#M196763</guid>
      <dc:creator>JK-IMX</dc:creator>
      <dc:date>2022-10-24T09:23:23Z</dc:date>
    </item>
    <item>
      <title>Re: Significant difference of AI inference result between CPU and NPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Significant-difference-of-AI-inference-result-between-CPU-and/m-p/1549498#M197264</link>
      <description>&lt;P&gt;I have already mailed to you, pls check it&lt;/P&gt;</description>
      <pubDate>Mon, 07 Nov 2022 08:19:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Significant-difference-of-AI-inference-result-between-CPU-and/m-p/1549498#M197264</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-11-07T08:19:04Z</dc:date>
    </item>
  </channel>
</rss>