<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Capturing odd resolutions on iMX8M mini</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Capturing-odd-resolutions-on-iMX8M-mini/m-p/1541594#M196653</link>
    <description>&lt;P&gt;what format of data from your camera? pls refer to the CSI_IMAG_PARA in the reference manual and read this register to check&lt;/P&gt;</description>
    <pubDate>Fri, 21 Oct 2022 04:09:27 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2022-10-21T04:09:27Z</dc:date>
    <item>
      <title>Capturing odd resolutions on iMX8M mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capturing-odd-resolutions-on-iMX8M-mini/m-p/1540232#M196575</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a sensor driver for an iMX8M mini module. This sensor allows resolutions with odd Height values, for example width=240 x height=135.&lt;/P&gt;&lt;P&gt;I've noticed that every time I input an odd Height, this value is rounded to the next even number, in this example, is rounded from 135 to 136.&lt;/P&gt;&lt;P&gt;Is this some platform specific limitation? Is there any reason why odd resolutions could not be supported?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 16:32:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capturing-odd-resolutions-on-iMX8M-mini/m-p/1540232#M196575</guid>
      <dc:creator>alejandro_flores</dc:creator>
      <dc:date>2022-10-19T16:32:56Z</dc:date>
    </item>
    <item>
      <title>Re: Capturing odd resolutions on iMX8M mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capturing-odd-resolutions-on-iMX8M-mini/m-p/1541594#M196653</link>
      <description>&lt;P&gt;what format of data from your camera? pls refer to the CSI_IMAG_PARA in the reference manual and read this register to check&lt;/P&gt;</description>
      <pubDate>Fri, 21 Oct 2022 04:09:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capturing-odd-resolutions-on-iMX8M-mini/m-p/1541594#M196653</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-10-21T04:09:27Z</dc:date>
    </item>
    <item>
      <title>Re: Capturing odd resolutions on iMX8M mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capturing-odd-resolutions-on-iMX8M-mini/m-p/1547937#M197134</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;, thanks for your answer.&lt;/P&gt;&lt;P&gt;I am using multiple formats, however, that register that you mentioned gave me a huge hint of what might be the issue.&lt;BR /&gt;&lt;BR /&gt;The documentation of the&amp;nbsp;&lt;SPAN&gt;CSI_IMAG_PARA&lt;/SPAN&gt; register states the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;If the input data from the sensor is 8-bit/pixel format, the IMAGE_WIDTH should be a multiple of 8 pixels.&lt;/LI&gt;&lt;LI&gt;If the input data from the sensor is 10-bit/pixel or 16-bit/pixel format, the IMAGE_WIDTH should be a multiple of 4 pixels.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I believe that this the limitation that I was looking for, with this information I should be able to limit which resolutions can be used or not.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 21:56:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capturing-odd-resolutions-on-iMX8M-mini/m-p/1547937#M197134</guid>
      <dc:creator>alejandro_flores</dc:creator>
      <dc:date>2022-11-02T21:56:47Z</dc:date>
    </item>
  </channel>
</rss>