<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Slow down access to quad SPI flash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Slow-down-access-to-quad-SPI-flash/m-p/1540092#M196556</link>
    <description>&lt;P&gt;I have a proto board with mismatched trace lengths between the processor and SPI flash memory, which is causing timing problems.&amp;nbsp; Is it possible to slow down the SPI interface in mcuxpresso to a speed to allow programming and access?&lt;/P&gt;</description>
    <pubDate>Wed, 19 Oct 2022 12:18:31 GMT</pubDate>
    <dc:creator>BCVegas</dc:creator>
    <dc:date>2022-10-19T12:18:31Z</dc:date>
    <item>
      <title>Slow down access to quad SPI flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Slow-down-access-to-quad-SPI-flash/m-p/1540092#M196556</link>
      <description>&lt;P&gt;I have a proto board with mismatched trace lengths between the processor and SPI flash memory, which is causing timing problems.&amp;nbsp; Is it possible to slow down the SPI interface in mcuxpresso to a speed to allow programming and access?&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 12:18:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Slow-down-access-to-quad-SPI-flash/m-p/1540092#M196556</guid>
      <dc:creator>BCVegas</dc:creator>
      <dc:date>2022-10-19T12:18:31Z</dc:date>
    </item>
    <item>
      <title>Re: Slow down access to quad SPI flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Slow-down-access-to-quad-SPI-flash/m-p/1543242#M196810</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Yes, customer can slow down the SPI Flash serial clock.&lt;/P&gt;
&lt;P&gt;Just using SDK provided demo &amp;lt;flexspi_hyper_flash_polling_transfer&amp;gt;, the &amp;lt;app.h&amp;gt; has below function to initialise FlexSPI clock:&lt;/P&gt;
&lt;P&gt;static inline void flexspi_clock_init(void)&lt;/P&gt;
&lt;P&gt;Thanks for the attention.&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Tue, 25 Oct 2022 08:26:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Slow-down-access-to-quad-SPI-flash/m-p/1543242#M196810</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2022-10-25T08:26:33Z</dc:date>
    </item>
  </channel>
</rss>