<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Radio Tuner Chip</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Radio-Tuner-Chip/m-p/1539730#M196522</link>
    <description>&lt;P&gt;Anyone has any update on this? I am specifically looking for any FM radio module which can be plugged into the iMX8QXP MEK Board. Please help&lt;/P&gt;</description>
    <pubDate>Wed, 19 Oct 2022 03:52:04 GMT</pubDate>
    <dc:creator>sooraj_ms</dc:creator>
    <dc:date>2022-10-19T03:52:04Z</dc:date>
    <item>
      <title>Radio Tuner Chip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Radio-Tuner-Chip/m-p/1460135#M190537</link>
      <description>&lt;P&gt;I am working on android automotive 11 on imx 8 quadmax and I am exploring radio application.&lt;BR /&gt;As of now it seems there is no support for radio hardware on the board.&amp;nbsp;&lt;BR /&gt;Can anyone please provide any information regarding any Tuner chip availability which can be plugged and played.&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 15:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Radio-Tuner-Chip/m-p/1460135#M190537</guid>
      <dc:creator>SwayamDhondge</dc:creator>
      <dc:date>2022-05-18T15:16:31Z</dc:date>
    </item>
    <item>
      <title>Re: Radio Tuner Chip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Radio-Tuner-Chip/m-p/1464146#M190840</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am also working on a similar use case.&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195074"&gt;@SwayamDhondge&lt;/a&gt;&amp;nbsp;Did you find any such chip for the same ?&amp;nbsp;&lt;BR /&gt;Any help on the same will be very much appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Wed, 25 May 2022 18:05:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Radio-Tuner-Chip/m-p/1464146#M190840</guid>
      <dc:creator>swapnil</dc:creator>
      <dc:date>2022-05-25T18:05:41Z</dc:date>
    </item>
    <item>
      <title>Re: Radio Tuner Chip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Radio-Tuner-Chip/m-p/1539730#M196522</link>
      <description>&lt;P&gt;Anyone has any update on this? I am specifically looking for any FM radio module which can be plugged into the iMX8QXP MEK Board. Please help&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 03:52:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Radio-Tuner-Chip/m-p/1539730#M196522</guid>
      <dc:creator>sooraj_ms</dc:creator>
      <dc:date>2022-10-19T03:52:04Z</dc:date>
    </item>
    <item>
      <title>Re: Radio Tuner Chip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Radio-Tuner-Chip/m-p/1542199#M196712</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;A start might be to have a look in your kernel config to see if there's anything available in your specific build. In my iMX8 menuconfig I have two FM drivers,&amp;nbsp;Silicon laboratories 4761/64/68 AM/FM radio and the&amp;nbsp;TI WL1273 FM radio.&lt;/P&gt;&lt;P&gt;These are found in&amp;nbsp;Device Drivers &amp;gt; Multifunction device drivers. Often peripherals have similar industry standard interfaces and drivers can be adapted for different families of devices. Might be worth seeing what you have already in your build, get familiar with the drivers and see what chip sets are available that may come close 'code wise'. If you have a FM chipset in mind see is there is driver source for it and try building it (with a few mods probably) and probe it in and you never know!&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;Edit: Had a look at the si476x PDF and its controlled via I2C and the audio is delivered via I2S. So other chipsets are probably fairly similar. Start small, find a similar driver that has I2C and I2S, get the I2C talking, get the I2S running - job done!&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 22 Oct 2022 00:08:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Radio-Tuner-Chip/m-p/1542199#M196712</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2022-10-22T00:08:45Z</dc:date>
    </item>
    <item>
      <title>Re: Radio Tuner Chip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Radio-Tuner-Chip/m-p/1914730#M226491</link>
      <description>&lt;P&gt;i want to check imx8qxp board, In the board imx8qxp FM radio chipis si475x in series&amp;nbsp; FM. i need supporting drivers to play AM and FM&amp;nbsp; different frequency signals&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jul 2024 06:57:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Radio-Tuner-Chip/m-p/1914730#M226491</guid>
      <dc:creator>karthik2799</dc:creator>
      <dc:date>2024-07-23T06:57:13Z</dc:date>
    </item>
  </channel>
</rss>