<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Xen Hypervisor Deployment on IMX8 Quad Max in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Deployment-on-IMX8-Quad-Max/m-p/1538113#M196386</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to run Xen hypervisor on the imx8qm board. I am following the instructions on the AN13138&amp;nbsp;Xen Deployment on Layerscape Platforms application note. First, I did all instructions for the building phase (section 2.1) and I get all necessary generated files as expected:&lt;/P&gt;&lt;P&gt;-fsl-image-networking-imx8qmmek-20221011063852.rootfs.cpio.gz&lt;/P&gt;&lt;P&gt;-fsl-image-networking-imx8qmmek-20221011063852.rootfs.ext2&lt;/P&gt;&lt;P&gt;-fsl-imx8qm-mek.dtb&lt;/P&gt;&lt;P&gt;-Image&lt;/P&gt;&lt;P&gt;-xen-imx8qmmek&lt;/P&gt;&lt;P&gt;However, there is no u-boot file in the deploy folder and I load an external u-boot and cannot perform the TFTP commands which the application note uses in the section 2.2 Deployment. I run 'run xenmmcboot' command in u-boot but because of the TFTP failure, I encounter with some fdt address errors. I&amp;nbsp;&lt;SPAN&gt;would be very grateful if you could help me by explaining the TFTP part with which u-boot file. Briefly, can anyone helps to run Dom0 and create new DomU s?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 15 Oct 2022 21:54:05 GMT</pubDate>
    <dc:creator>nevozade</dc:creator>
    <dc:date>2022-10-15T21:54:05Z</dc:date>
    <item>
      <title>Xen Hypervisor Deployment on IMX8 Quad Max</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Deployment-on-IMX8-Quad-Max/m-p/1538113#M196386</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to run Xen hypervisor on the imx8qm board. I am following the instructions on the AN13138&amp;nbsp;Xen Deployment on Layerscape Platforms application note. First, I did all instructions for the building phase (section 2.1) and I get all necessary generated files as expected:&lt;/P&gt;&lt;P&gt;-fsl-image-networking-imx8qmmek-20221011063852.rootfs.cpio.gz&lt;/P&gt;&lt;P&gt;-fsl-image-networking-imx8qmmek-20221011063852.rootfs.ext2&lt;/P&gt;&lt;P&gt;-fsl-imx8qm-mek.dtb&lt;/P&gt;&lt;P&gt;-Image&lt;/P&gt;&lt;P&gt;-xen-imx8qmmek&lt;/P&gt;&lt;P&gt;However, there is no u-boot file in the deploy folder and I load an external u-boot and cannot perform the TFTP commands which the application note uses in the section 2.2 Deployment. I run 'run xenmmcboot' command in u-boot but because of the TFTP failure, I encounter with some fdt address errors. I&amp;nbsp;&lt;SPAN&gt;would be very grateful if you could help me by explaining the TFTP part with which u-boot file. Briefly, can anyone helps to run Dom0 and create new DomU s?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 15 Oct 2022 21:54:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Deployment-on-IMX8-Quad-Max/m-p/1538113#M196386</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-10-15T21:54:05Z</dc:date>
    </item>
    <item>
      <title>Re: Xen Hypervisor Deployment on IMX8 Quad Max</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Deployment-on-IMX8-Quad-Max/m-p/1540852#M196598</link>
      <description>&lt;P&gt;Please refer to the Chapter 12 in Linux User's guide (ver. L5.4.70_2.3.0).&lt;/P&gt;
&lt;P&gt;And the section 5.6.11 in i.MX Yocto User's guide.&lt;/P&gt;
&lt;P&gt;Please download the documentation from here: &lt;A href="https://www.nxp.com/webapp/Download?colCode=L5.4.70_2.3.0_LINUX_DOCS" target="_blank" rel="noopener" data-dtmsubaction="Documentation 5.4.70_2.3.0 link"&gt;Documentation&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 07:00:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Deployment-on-IMX8-Quad-Max/m-p/1540852#M196598</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-10-20T07:00:20Z</dc:date>
    </item>
  </channel>
</rss>