<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8 input:bitbake core-image-base  ，There is an error：“Function failed: do_rootfs”</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-input-bitbake-core-image-base-There-is-an-error-Function/m-p/1537581#M196355</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207416"&gt;@guoMr&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to suggest you use the latest BSP and build on host with least 20.04.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Harvey&lt;/P&gt;</description>
    <pubDate>Fri, 14 Oct 2022 06:39:26 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2022-10-14T06:39:26Z</dc:date>
    <item>
      <title>i.MX8 input:bitbake core-image-base  ，There is an error：“Function failed: do_rootfs”</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-input-bitbake-core-image-base-There-is-an-error-Function/m-p/1536937#M196313</link>
      <description>&lt;P&gt;开发环境（&lt;SPAN&gt;development environment&lt;/SPAN&gt;）：ununtu16.04TLS&amp;nbsp;&lt;/P&gt;&lt;P&gt;board：i.MX 8QuadXPlus&lt;/P&gt;&lt;P&gt;当我根据文件《i.MX_Yocto_Project_User's_Guide.pdf》进行开发，关键指令如下 ：&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-wayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build_imx8qxp&lt;/P&gt;&lt;P&gt;core-image-base&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;遇到错误：&lt;/P&gt;&lt;P&gt;WARNING: You have included the meta-gnome layer, but 'x11' has not been enabled in your DISTRO_FEATURES. Some bbappend files may not take effect. See the meta-gnome README for details on enabling meta-gnome support.&lt;BR /&gt;Loading cache: 100% |############################################| Time: 0:00:01&lt;BR /&gt;Loaded 3693 entries from dependency cache.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.40.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "ubuntu-16.04"&lt;BR /&gt;TARGET_SYS = "aarch64-poky-linux"&lt;BR /&gt;MACHINE = "imx8qxpmek"&lt;BR /&gt;DISTRO = "fsl-imx-wayland"&lt;BR /&gt;DISTRO_VERSION = "4.19-thud"&lt;BR /&gt;TUNE_FEATURES = "aarch64"&lt;BR /&gt;TARGET_FPU = ""&lt;BR /&gt;meta&lt;BR /&gt;meta-poky = "HEAD:50f33d3bfebcbfb1538d932fb487cfd789872026"&lt;BR /&gt;meta-oe&lt;BR /&gt;meta-multimedia = "HEAD:4cd3a39f22a2712bfa8fc657d09fe2c7765a4005"&lt;BR /&gt;meta-freescale = "HEAD:f5c932229c31b612cba38c2ed6f3c3ec6b800e92"&lt;BR /&gt;meta-freescale-3rdparty = "HEAD:c4b5ac6b20e4245ce0630e9197313aaef999a331"&lt;BR /&gt;meta-freescale-distro = "HEAD:4a244af3993ae662624c6f615464e6806cc719a2"&lt;BR /&gt;meta-bsp&lt;BR /&gt;meta-sdk&lt;BR /&gt;meta-ml = "HEAD:a36b16e20ec6bb8d02f18bab31cbe59712fa3def"&lt;BR /&gt;meta-browser = "HEAD:23e206d355e46d6f6e6a5638c574524492f91bc2"&lt;BR /&gt;meta-rust = "HEAD:84710b341be53cc2af13ecc8ae87773cf84687bf"&lt;BR /&gt;meta-gnome&lt;BR /&gt;meta-networking&lt;BR /&gt;meta-python&lt;BR /&gt;meta-filesystems = "HEAD:4cd3a39f22a2712bfa8fc657d09fe2c7765a4005"&lt;BR /&gt;meta-qt5 = "HEAD:0630018c0033c91fddda62a49f59a82ba6ec6850"&lt;/P&gt;&lt;P&gt;Initialising tasks: 100% |#######################################| Time: 0:00:01&lt;BR /&gt;Sstate summary: Wanted 2 Found 0 Missed 2 Current 1158 (0% match, 99% complete)&lt;BR /&gt;NOTE: Executing SetScene Tasks&lt;BR /&gt;NOTE: Executing RunQueue Tasks&lt;BR /&gt;ERROR: core-image-base-1.0-r0 do_rootfs: The postinstall intercept hook 'update_icon_cache' failed, details in /home/guo/imx-yocto-bsp/build_imx8qxp/tmp/work/imx8qxpmek-poky-linux/core-image-base/1.0-r0/temp/log.do_rootfs&lt;BR /&gt;ERROR: core-image-base-1.0-r0 do_rootfs: Function failed: do_rootfs&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/guo/imx-yocto-bsp/build_imx8qxp/tmp/work/imx8qxpmek-poky-linux/core-image-base/1.0-r0/temp/log.do_rootfs.2799&lt;BR /&gt;ERROR: Task (/home/guo/imx-yocto-bsp/sources/poky/meta/recipes-core/images/core-image-base.bb:do_rootfs) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 3453 tasks of which 3452 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;日志文件中内容 ：&lt;/P&gt;&lt;P&gt;ERROR: The postinstall intercept hook 'update_icon_cache' failed, details in /home/guo/imx-yocto-bsp/build_imx8qxp/tmp/work/imx8qxpmek-poky-linux/core-image-base/1.0-r0/temp/log.do_rootfs&lt;BR /&gt;DEBUG: Python function do_rootfs finished&lt;BR /&gt;ERROR: Function failed: do_rootfs&lt;/P&gt;&lt;P&gt;感谢大家给予帮助（&lt;SPAN&gt;Thank you all for your help:&lt;/SPAN&gt;）&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Oct 2022 07:54:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-input-bitbake-core-image-base-There-is-an-error-Function/m-p/1536937#M196313</guid>
      <dc:creator>guoMr</dc:creator>
      <dc:date>2022-10-13T07:54:32Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 input:bitbake core-image-base  ，There is an error：“Function failed: do_rootfs”</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-input-bitbake-core-image-base-There-is-an-error-Function/m-p/1537581#M196355</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207416"&gt;@guoMr&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to suggest you use the latest BSP and build on host with least 20.04.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 14 Oct 2022 06:39:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-input-bitbake-core-image-base-There-is-an-error-Function/m-p/1537581#M196355</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2022-10-14T06:39:26Z</dc:date>
    </item>
  </channel>
</rss>