<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Keyboard problem when debugging imx 8 quad x</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Keyboard-problem-when-debugging-imx-8-quad-x/m-p/1537309#M196347</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Could you share a bit more information, which MEK board revision are you using?&lt;BR /&gt;Also, which BSP version are you using for your test?&lt;BR /&gt;&lt;BR /&gt;I have tried on my side SCH-29683 REV C2, Linux 5.15.52-2.1.0 and couldn't reproduce your issue. I can interact with serial terminal no matter if USB Type-C is connected or not.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Thu, 13 Oct 2022 19:12:55 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2022-10-13T19:12:55Z</dc:date>
    <item>
      <title>Keyboard problem when debugging imx 8 quad x</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Keyboard-problem-when-debugging-imx-8-quad-x/m-p/1535483#M196201</link>
      <description>&lt;P&gt;Hi iMX champ&lt;/P&gt;&lt;P&gt;I am currently using imx8 qaud x.&lt;BR /&gt;I am downloading SW using a type-c cable in download mode and booting with a serial cable in emmc mode.&lt;BR /&gt;The keyboard did not work while checking debugging in tera term.&lt;BR /&gt;The keyboard works when both the serial cable and type-c cable are connected, but the keyboard does not work when only the serial cable is connected.&lt;BR /&gt;How can I solve it?&lt;/P&gt;&lt;P&gt;Thank for any help.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Oct 2022 08:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Keyboard-problem-when-debugging-imx-8-quad-x/m-p/1535483#M196201</guid>
      <dc:creator>mbj0010911</dc:creator>
      <dc:date>2022-10-11T08:38:24Z</dc:date>
    </item>
    <item>
      <title>Re: Keyboard problem when debugging imx 8 quad x</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Keyboard-problem-when-debugging-imx-8-quad-x/m-p/1537309#M196347</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Could you share a bit more information, which MEK board revision are you using?&lt;BR /&gt;Also, which BSP version are you using for your test?&lt;BR /&gt;&lt;BR /&gt;I have tried on my side SCH-29683 REV C2, Linux 5.15.52-2.1.0 and couldn't reproduce your issue. I can interact with serial terminal no matter if USB Type-C is connected or not.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Oct 2022 19:12:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Keyboard-problem-when-debugging-imx-8-quad-x/m-p/1537309#M196347</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-10-13T19:12:55Z</dc:date>
    </item>
  </channel>
</rss>