<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックXen Hypervisor Deployment on SD Card</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Deployment-on-SD-Card/m-p/1536005#M196251</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am following the application note AN13138 Xen Deployment on Layerscape Platforms (attached to this issue) to generate Xen hypervisor image and other needed files that work on imx8qm board. I completes the section 2.1 Build by following through the instructions here successfully and I generated the desired files in the desired directory.&lt;/P&gt;&lt;P&gt;However, in the section 2.2 Deployment, there are some tftp commands that should be given on u-boot but because of some problems, I cannot use the tftp properly and I do want to deploy xen hypervisor by using a SD card. Is it possible to load xen_addr, image, device tree blob etc. with SD card and if yes, how?&lt;/P&gt;&lt;P&gt;I would be very grateful if you could help me with running Xen and Dom0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
    <pubDate>Wed, 12 Oct 2022 06:15:25 GMT</pubDate>
    <dc:creator>nevozade</dc:creator>
    <dc:date>2022-10-12T06:15:25Z</dc:date>
    <item>
      <title>Xen Hypervisor Deployment on SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Deployment-on-SD-Card/m-p/1536005#M196251</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am following the application note AN13138 Xen Deployment on Layerscape Platforms (attached to this issue) to generate Xen hypervisor image and other needed files that work on imx8qm board. I completes the section 2.1 Build by following through the instructions here successfully and I generated the desired files in the desired directory.&lt;/P&gt;&lt;P&gt;However, in the section 2.2 Deployment, there are some tftp commands that should be given on u-boot but because of some problems, I cannot use the tftp properly and I do want to deploy xen hypervisor by using a SD card. Is it possible to load xen_addr, image, device tree blob etc. with SD card and if yes, how?&lt;/P&gt;&lt;P&gt;I would be very grateful if you could help me with running Xen and Dom0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Oct 2022 06:15:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Deployment-on-SD-Card/m-p/1536005#M196251</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-10-12T06:15:25Z</dc:date>
    </item>
    <item>
      <title>Re: Xen Hypervisor Deployment on SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Deployment-on-SD-Card/m-p/1538600#M196443</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You may following the yocto user guide document section 5.6.11 to build xen. This is for layerscape not necessarily works for MX8QM.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Mon, 17 Oct 2022 13:51:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-Hypervisor-Deployment-on-SD-Card/m-p/1538600#M196443</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-10-17T13:51:50Z</dc:date>
    </item>
  </channel>
</rss>