<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 回复： IMX6DL : Kernel hangs when configuring CONFIG_PCI_MSI in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-Kernel-hangs-when-configuring-CONFIG-PCI-MSI/m-p/1535420#M196200</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am porting I210 Ethernet control of imx8mm. I don't add the CONFIG so it can't work well.&lt;/P&gt;&lt;P&gt;#&lt;BR /&gt;# Bus support&lt;BR /&gt;#&lt;BR /&gt;CONFIG_PCI=y&lt;BR /&gt;CONFIG_PCI_DOMAINS=y&lt;BR /&gt;CONFIG_PCI_SYSCALL=y&lt;BR /&gt;CONFIG_PCI_MSI=y&lt;BR /&gt;#&lt;BR /&gt;# PCI host controller drivers&lt;BR /&gt;#&lt;BR /&gt;CONFIG_PCIE_DW=y&lt;BR /&gt;CONFIG_PCI_IMX6=y&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.youtube.com/shorts/3jO6BhMUrl8" target="_blank"&gt;(45) Intel i210 Plug in crash - YouTube&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How os your task ? Can you help me ?&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;tzeng015&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 11 Oct 2022 07:31:55 GMT</pubDate>
    <dc:creator>tzeng015</dc:creator>
    <dc:date>2022-10-11T07:31:55Z</dc:date>
    <item>
      <title>IMX6DL : Kernel hangs when configuring CONFIG_PCI_MSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-Kernel-hangs-when-configuring-CONFIG-PCI-MSI/m-p/973988#M144969</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a custom board with IMX6Duallite , in which the PCIE is connected to the i210 ethernet controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I have the CONFIG_PCI_MSI=y, &lt;STRONG&gt;the Linux kernel hangs&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel used&amp;nbsp; 4.9.123&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel config :&lt;/P&gt;&lt;P&gt;#&lt;BR /&gt;# Bus support&lt;BR /&gt;#&lt;BR /&gt;CONFIG_PCI=y&lt;BR /&gt;CONFIG_PCI_DOMAINS=y&lt;BR /&gt;CONFIG_PCI_DOMAINS_GENERIC=y&lt;BR /&gt;CONFIG_PCI_SYSCALL=y&lt;BR /&gt;CONFIG_PCIEPORTBUS=y&lt;BR /&gt;CONFIG_PCIEAER=y&lt;BR /&gt;# CONFIG_PCIE_ECRC is not set&lt;BR /&gt;# CONFIG_PCIEAER_INJECT is not set&lt;BR /&gt;CONFIG_PCIEASPM=y&lt;BR /&gt;# CONFIG_PCIEASPM_DEBUG is not set&lt;BR /&gt;# CONFIG_PCIEASPM_DEFAULT is not set&lt;BR /&gt;# CONFIG_PCIEASPM_POWERSAVE is not set&lt;BR /&gt;CONFIG_PCIEASPM_PERFORMANCE=y&lt;BR /&gt;CONFIG_PCIE_PME=y&lt;BR /&gt;# CONFIG_PCIE_DPC is not set&lt;BR /&gt;# CONFIG_PCIE_PTM is not set&lt;BR /&gt;CONFIG_PCI_MSI=y&lt;BR /&gt;CONFIG_PCI_MSI_IRQ_DOMAIN=y&lt;BR /&gt;# CONFIG_PCI_DEBUG is not set&lt;BR /&gt;# CONFIG_PCI_REALLOC_ENABLE_AUTO is not set&lt;BR /&gt;# CONFIG_PCI_STUB is not set&lt;BR /&gt;# CONFIG_PCI_IOV is not set&lt;BR /&gt;# CONFIG_PCI_PRI is not set&lt;BR /&gt;# CONFIG_PCI_PASID is not set&lt;BR /&gt;# CONFIG_HOTPLUG_PCI is not set&lt;/P&gt;&lt;P&gt;#&lt;BR /&gt;# PCI host controller drivers&lt;BR /&gt;#&lt;BR /&gt;# CONFIG_PCIE_DW_PLAT is not set&lt;BR /&gt;CONFIG_PCIE_DW=y&lt;BR /&gt;CONFIG_PCI_IMX6=y&lt;BR /&gt;# CONFIG_PCI_HOST_GENERIC is not set&lt;BR /&gt;# CONFIG_PCI_LAYERSCAPE is not set&lt;BR /&gt;# CONFIG_PCIE_ALTERA is not set&lt;BR /&gt;# CONFIG_PCCARD is not set&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Device tree :&lt;/P&gt;&lt;P&gt;&amp;amp;pcie {&lt;BR /&gt;&amp;nbsp;pinctrl-names = "default";&lt;BR /&gt;&amp;nbsp;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_pcie&amp;gt;;&lt;BR /&gt;&amp;nbsp;reset-gpio = &amp;lt;&amp;amp;gpio1 0 0&amp;gt;;&lt;BR /&gt;&amp;nbsp;status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;NOTE : the above same configuration works on a different version of the board with IMX6Q quad core.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any issue using MSI_IRQ in IMX6DL (dual core).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any help would be highly appreciable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Terry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2019 22:02:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-Kernel-hangs-when-configuring-CONFIG-PCI-MSI/m-p/973988#M144969</guid>
      <dc:creator>agnel_terry</dc:creator>
      <dc:date>2019-08-26T22:02:46Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6DL : Kernel hangs when configuring CONFIG_PCI_MSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-Kernel-hangs-when-configuring-CONFIG-PCI-MSI/m-p/973989#M144970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi agne&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;kernel 4.9.123 was not tested with i.MX6 and not recommended to use with i.MX6,&lt;/P&gt;&lt;P&gt;one can try with latest L4.14.78 or L4.14.98&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Linux&amp;nbsp; Documentation&lt;BR /&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tool:IMX-SW" title="https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tool:IMX-SW"&gt;i.MX Software | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2019 23:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-Kernel-hangs-when-configuring-CONFIG-PCI-MSI/m-p/973989#M144970</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-26T23:37:01Z</dc:date>
    </item>
    <item>
      <title>回复： IMX6DL : Kernel hangs when configuring CONFIG_PCI_MSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-Kernel-hangs-when-configuring-CONFIG-PCI-MSI/m-p/1535420#M196200</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am porting I210 Ethernet control of imx8mm. I don't add the CONFIG so it can't work well.&lt;/P&gt;&lt;P&gt;#&lt;BR /&gt;# Bus support&lt;BR /&gt;#&lt;BR /&gt;CONFIG_PCI=y&lt;BR /&gt;CONFIG_PCI_DOMAINS=y&lt;BR /&gt;CONFIG_PCI_SYSCALL=y&lt;BR /&gt;CONFIG_PCI_MSI=y&lt;BR /&gt;#&lt;BR /&gt;# PCI host controller drivers&lt;BR /&gt;#&lt;BR /&gt;CONFIG_PCIE_DW=y&lt;BR /&gt;CONFIG_PCI_IMX6=y&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.youtube.com/shorts/3jO6BhMUrl8" target="_blank"&gt;(45) Intel i210 Plug in crash - YouTube&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How os your task ? Can you help me ?&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;tzeng015&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Oct 2022 07:31:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-Kernel-hangs-when-configuring-CONFIG-PCI-MSI/m-p/1535420#M196200</guid>
      <dc:creator>tzeng015</dc:creator>
      <dc:date>2022-10-11T07:31:55Z</dc:date>
    </item>
  </channel>
</rss>