<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic sai_sdma_transfer example can't run with linux BSP? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/sai-sdma-transfer-example-can-t-run-with-linux-BSP/m-p/1533877#M196089</link>
    <description>&lt;P&gt;I notice that the readme.txt file associated with the sai_sdma_transfer example for the IMX8MMEVK states that the example cannot be run with the linux BSP.&amp;nbsp; My question is why?&amp;nbsp; I confess that I have not tried to find out the details on my own yet, but I thought that disabling the SAI on the linux side DT would do. Is this a limitation that can be removed by any means of customization of either the example or the Linux side?&lt;/P&gt;</description>
    <pubDate>Fri, 07 Oct 2022 13:57:56 GMT</pubDate>
    <dc:creator>mwilliams</dc:creator>
    <dc:date>2022-10-07T13:57:56Z</dc:date>
    <item>
      <title>sai_sdma_transfer example can't run with linux BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sai-sdma-transfer-example-can-t-run-with-linux-BSP/m-p/1533877#M196089</link>
      <description>&lt;P&gt;I notice that the readme.txt file associated with the sai_sdma_transfer example for the IMX8MMEVK states that the example cannot be run with the linux BSP.&amp;nbsp; My question is why?&amp;nbsp; I confess that I have not tried to find out the details on my own yet, but I thought that disabling the SAI on the linux side DT would do. Is this a limitation that can be removed by any means of customization of either the example or the Linux side?&lt;/P&gt;</description>
      <pubDate>Fri, 07 Oct 2022 13:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sai-sdma-transfer-example-can-t-run-with-linux-BSP/m-p/1533877#M196089</guid>
      <dc:creator>mwilliams</dc:creator>
      <dc:date>2022-10-07T13:57:56Z</dc:date>
    </item>
    <item>
      <title>Re: sai_sdma_transfer example can't run with linux BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sai-sdma-transfer-example-can-t-run-with-linux-BSP/m-p/1534971#M196170</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, this kind of examples it may need more than just disabling the same peripheral in linux dts, disabling clocks and maybe reserving a part of memory.&lt;BR /&gt;&lt;BR /&gt;In this particular case you may refer to the sai_low_power_audio example which should be interesting for you. It is inside the SDK package &amp;lt;SDK installation path&amp;gt;\boards\evkmimx8mn\demo_apps&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Oct 2022 15:10:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sai-sdma-transfer-example-can-t-run-with-linux-BSP/m-p/1534971#M196170</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-10-10T15:10:04Z</dc:date>
    </item>
    <item>
      <title>Re: sai_sdma_transfer example can't run with linux BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sai-sdma-transfer-example-can-t-run-with-linux-BSP/m-p/1535638#M196215</link>
      <description>&lt;P&gt;Hi AldoG,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&amp;nbsp; I have been able to run the SDMA transfer example and I will study the other example you point out.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Tue, 11 Oct 2022 12:28:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sai-sdma-transfer-example-can-t-run-with-linux-BSP/m-p/1535638#M196215</guid>
      <dc:creator>mwilliams</dc:creator>
      <dc:date>2022-10-11T12:28:25Z</dc:date>
    </item>
  </channel>
</rss>