<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX8QM Android Automotive Bootloader Image Issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Android-Automotive-Bootloader-Image-Issue/m-p/1533451#M196054</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I built Android Automotive 12.0.0_2.1.0(Linux 5.15.32 BSP) for the iMX8QM platform.&lt;/P&gt;&lt;P&gt;I tried to write the Bootloader image to the SD card with the command "&lt;STRONG&gt;sudo dd if=flash.bin of=/dev/sdb bs=1K seek=1&lt;/STRONG&gt;".&lt;/P&gt;&lt;P&gt;When I insert the SD card into the board, I can't see any boot activity in the Debug console.&lt;/P&gt;&lt;P&gt;Then I wrote the "&lt;STRONG&gt;bootloader-imx8qm.img&lt;/STRONG&gt;" and "&lt;STRONG&gt;u-boot-imx8qm-mek-uuu.imx&lt;/STRONG&gt;" files to the SD card using the same dd command, but I could not see a boot movement in the Debug console.&lt;/P&gt;&lt;P&gt;What bootloader binary do I need to use to see a U-Boot stream in the Debug console?&lt;/P&gt;&lt;P&gt;Also, could you suggest a dd command to write the bootloader image to the SD card?&lt;/P&gt;&lt;P&gt;What should the "&lt;STRONG&gt;seek&lt;/STRONG&gt;", "&lt;STRONG&gt;bs&lt;/STRONG&gt;" and "&lt;STRONG&gt;count&lt;/STRONG&gt;" parameters be for the iMX8QM in the dd command I will use?&lt;/P&gt;&lt;P&gt;Could you please help with these issues?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Efecan&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 06 Oct 2022 14:34:13 GMT</pubDate>
    <dc:creator>cbl</dc:creator>
    <dc:date>2022-10-06T14:34:13Z</dc:date>
    <item>
      <title>iMX8QM Android Automotive Bootloader Image Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Android-Automotive-Bootloader-Image-Issue/m-p/1533451#M196054</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I built Android Automotive 12.0.0_2.1.0(Linux 5.15.32 BSP) for the iMX8QM platform.&lt;/P&gt;&lt;P&gt;I tried to write the Bootloader image to the SD card with the command "&lt;STRONG&gt;sudo dd if=flash.bin of=/dev/sdb bs=1K seek=1&lt;/STRONG&gt;".&lt;/P&gt;&lt;P&gt;When I insert the SD card into the board, I can't see any boot activity in the Debug console.&lt;/P&gt;&lt;P&gt;Then I wrote the "&lt;STRONG&gt;bootloader-imx8qm.img&lt;/STRONG&gt;" and "&lt;STRONG&gt;u-boot-imx8qm-mek-uuu.imx&lt;/STRONG&gt;" files to the SD card using the same dd command, but I could not see a boot movement in the Debug console.&lt;/P&gt;&lt;P&gt;What bootloader binary do I need to use to see a U-Boot stream in the Debug console?&lt;/P&gt;&lt;P&gt;Also, could you suggest a dd command to write the bootloader image to the SD card?&lt;/P&gt;&lt;P&gt;What should the "&lt;STRONG&gt;seek&lt;/STRONG&gt;", "&lt;STRONG&gt;bs&lt;/STRONG&gt;" and "&lt;STRONG&gt;count&lt;/STRONG&gt;" parameters be for the iMX8QM in the dd command I will use?&lt;/P&gt;&lt;P&gt;Could you please help with these issues?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Efecan&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Oct 2022 14:34:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Android-Automotive-Bootloader-Image-Issue/m-p/1533451#M196054</guid>
      <dc:creator>cbl</dc:creator>
      <dc:date>2022-10-06T14:34:13Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM Android Automotive Bootloader Image Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Android-Automotive-Bootloader-Image-Issue/m-p/1533866#M196086</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You need to erase everything to burn again your sd, The first commends to burn is uboot with &lt;STRONG&gt;bootloader-imx8qm.img&lt;/STRONG&gt;" with &lt;STRONG&gt;bs=1K seek=1&lt;/STRONG&gt; but You have to use DDD to burn everything in android.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 07 Oct 2022 11:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Android-Automotive-Bootloader-Image-Issue/m-p/1533866#M196086</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-10-07T11:43:38Z</dc:date>
    </item>
  </channel>
</rss>