<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックu-boot SPL Build Error: undefined reference to `reset_cpu' and `fuse_read'</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-SPL-Build-Error-undefined-reference-to-reset-cpu-and-fuse/m-p/1532371#M195970</link>
    <description>&lt;P&gt;I have been using Yocto Project release Honister with meta-freescale for an i.MX6ul based target very similar to the&amp;nbsp;mx6ul_14x14_evk. u-boot-fslc_2021.07 with SPL builds and works fine.&lt;/P&gt;&lt;P&gt;I am in the process of updating to YP release Kirkstone. However, now with u-boot-fslc_2022.07 building SPL fails with the following messages:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;|   ( cd spl &amp;amp;&amp;amp; arm-altec-linux-gnueabi-ld.bfd  -T u-boot-spl.lds --gc-sections -Bstatic --gc-sections  --no-dynamic-linker --build-id=none -Ttext 0x00908000 arch/arm/cpu/armv7/start.o --whole-archive arch/arm/cpu/armv7/built-in.o arch/arm/cpu/built-in.o arch/arm/lib/built-in.o arch/arm/mach-imx/built-in.o board/freescale/mx6ul_14x14_evk/built-in.o board/freescale/common/built-in.o common/spl/built-in.o common/init/built-in.o boot/built-in.o common/built-in.o cmd/built-in.o env/built-in.o lib/built-in.o disk/built-in.o drivers/built-in.o drivers/usb/dwc3/built-in.o drivers/usb/cdns3/built-in.o dts/built-in.o fs/built-in.o  --no-whole-archive arch/arm/lib/eabi_compat.o arch/arm/lib/lib.a -Map u-boot-spl.map -o u-boot-spl )
| arm-altec-linux-gnueabi-ld.bfd: arch/arm/lib/reset.o: in function `do_reset':
| /develop/projects/altec/tcu/build/tmp/work/altectcu-altec-linux-gnueabi/u-boot-fslc/2022.07+gitAUTOINC+a21d7668eb-r0/git/arch/arm/lib/reset.c:42: undefined reference to `reset_cpu'
| arm-altec-linux-gnueabi-ld.bfd: arch/arm/mach-imx/hab.o: in function `imx_hab_is_enabled':&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Essentially the two symbols 'reset_cpu' and 'read_fuse' cannot be resolved. The configuration settings &lt;SPAN class=""&gt;CONFIG_SPL_LIBGENERIC_SUPPORT and CONFIG_SPL_LIBCOMMON_SUPPORT&lt;/SPAN&gt; are enabled. I am somewhat at a loss what could have changed. Maybe someone from the NXP team involved with u-boot can shed some light on it. Thank you.&lt;/P&gt;</description>
    <pubDate>Tue, 04 Oct 2022 23:47:45 GMT</pubDate>
    <dc:creator>rudolf_streif</dc:creator>
    <dc:date>2022-10-04T23:47:45Z</dc:date>
    <item>
      <title>u-boot SPL Build Error: undefined reference to `reset_cpu' and `fuse_read'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-SPL-Build-Error-undefined-reference-to-reset-cpu-and-fuse/m-p/1532371#M195970</link>
      <description>&lt;P&gt;I have been using Yocto Project release Honister with meta-freescale for an i.MX6ul based target very similar to the&amp;nbsp;mx6ul_14x14_evk. u-boot-fslc_2021.07 with SPL builds and works fine.&lt;/P&gt;&lt;P&gt;I am in the process of updating to YP release Kirkstone. However, now with u-boot-fslc_2022.07 building SPL fails with the following messages:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;|   ( cd spl &amp;amp;&amp;amp; arm-altec-linux-gnueabi-ld.bfd  -T u-boot-spl.lds --gc-sections -Bstatic --gc-sections  --no-dynamic-linker --build-id=none -Ttext 0x00908000 arch/arm/cpu/armv7/start.o --whole-archive arch/arm/cpu/armv7/built-in.o arch/arm/cpu/built-in.o arch/arm/lib/built-in.o arch/arm/mach-imx/built-in.o board/freescale/mx6ul_14x14_evk/built-in.o board/freescale/common/built-in.o common/spl/built-in.o common/init/built-in.o boot/built-in.o common/built-in.o cmd/built-in.o env/built-in.o lib/built-in.o disk/built-in.o drivers/built-in.o drivers/usb/dwc3/built-in.o drivers/usb/cdns3/built-in.o dts/built-in.o fs/built-in.o  --no-whole-archive arch/arm/lib/eabi_compat.o arch/arm/lib/lib.a -Map u-boot-spl.map -o u-boot-spl )
| arm-altec-linux-gnueabi-ld.bfd: arch/arm/lib/reset.o: in function `do_reset':
| /develop/projects/altec/tcu/build/tmp/work/altectcu-altec-linux-gnueabi/u-boot-fslc/2022.07+gitAUTOINC+a21d7668eb-r0/git/arch/arm/lib/reset.c:42: undefined reference to `reset_cpu'
| arm-altec-linux-gnueabi-ld.bfd: arch/arm/mach-imx/hab.o: in function `imx_hab_is_enabled':&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Essentially the two symbols 'reset_cpu' and 'read_fuse' cannot be resolved. The configuration settings &lt;SPAN class=""&gt;CONFIG_SPL_LIBGENERIC_SUPPORT and CONFIG_SPL_LIBCOMMON_SUPPORT&lt;/SPAN&gt; are enabled. I am somewhat at a loss what could have changed. Maybe someone from the NXP team involved with u-boot can shed some light on it. Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 04 Oct 2022 23:47:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-SPL-Build-Error-undefined-reference-to-reset-cpu-and-fuse/m-p/1532371#M195970</guid>
      <dc:creator>rudolf_streif</dc:creator>
      <dc:date>2022-10-04T23:47:45Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot SPL Build Error: undefined reference to `reset_cpu' and `fuse_read'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-SPL-Build-Error-undefined-reference-to-reset-cpu-and-fuse/m-p/1534392#M196128</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer this commit:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://patchwork.ozlabs.org/project/uboot/patch/1451881154-5686-1-git-send-email-peng.fan@nxp.com/" target="_blank"&gt;https://patchwork.ozlabs.org/project/uboot/patch/1451881154-5686-1-git-send-email-peng.fan@nxp.com/&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 09 Oct 2022 06:20:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-SPL-Build-Error-undefined-reference-to-reset-cpu-and-fuse/m-p/1534392#M196128</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-10-09T06:20:48Z</dc:date>
    </item>
  </channel>
</rss>