<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックmenuconfig imx8 android 12</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/menuconfig-imx8-android-12/m-p/1532340#M195968</link>
    <description>&lt;P&gt;How can I call menuconfig for kernel in proper way?&lt;BR /&gt;&lt;BR /&gt;For building image I make next:&lt;BR /&gt;1) I got AOSP sources and prepare build system&lt;BR /&gt;2) source build/envsetup.sh&lt;BR /&gt;3) lunch 63&amp;nbsp; /* imx8mp EVK */&lt;BR /&gt;4) ./imx-make.sh -j4&lt;BR /&gt;5) flash with UUU&lt;BR /&gt;&lt;BR /&gt;And it is works, BUT I need also add some features into kernel&lt;BR /&gt;&lt;BR /&gt;So how it is possible edit kernel(add driver) without manual changing of config files?&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Tue, 04 Oct 2022 21:12:41 GMT</pubDate>
    <dc:creator>YuriiA07</dc:creator>
    <dc:date>2022-10-04T21:12:41Z</dc:date>
    <item>
      <title>menuconfig imx8 android 12</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/menuconfig-imx8-android-12/m-p/1532340#M195968</link>
      <description>&lt;P&gt;How can I call menuconfig for kernel in proper way?&lt;BR /&gt;&lt;BR /&gt;For building image I make next:&lt;BR /&gt;1) I got AOSP sources and prepare build system&lt;BR /&gt;2) source build/envsetup.sh&lt;BR /&gt;3) lunch 63&amp;nbsp; /* imx8mp EVK */&lt;BR /&gt;4) ./imx-make.sh -j4&lt;BR /&gt;5) flash with UUU&lt;BR /&gt;&lt;BR /&gt;And it is works, BUT I need also add some features into kernel&lt;BR /&gt;&lt;BR /&gt;So how it is possible edit kernel(add driver) without manual changing of config files?&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 04 Oct 2022 21:12:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/menuconfig-imx8-android-12/m-p/1532340#M195968</guid>
      <dc:creator>YuriiA07</dc:creator>
      <dc:date>2022-10-04T21:12:41Z</dc:date>
    </item>
    <item>
      <title>Re: menuconfig imx8 android 12</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/menuconfig-imx8-android-12/m-p/1532619#M196000</link>
      <description>&lt;P&gt;Hello Yuri,&lt;/P&gt;
&lt;P&gt;The kernel can be configure by menuconfig, the android kernel please check:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.android.com/docs/core/architecture/kernel/config" target="_blank"&gt;https://source.android.com/docs/core/architecture/kernel/config&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 05 Oct 2022 12:56:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/menuconfig-imx8-android-12/m-p/1532619#M196000</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-10-05T12:56:45Z</dc:date>
    </item>
  </channel>
</rss>