<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックConfigTools doesn't recognize error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ConfigTools-doesn-t-recognize-error/m-p/1531004#M195858</link>
    <description>&lt;P&gt;I added I2C pins in my configuration and when I update code, I get this error:&lt;/P&gt;&lt;P&gt;board/peripherals.h:15:10: fatal error: fsl_lpi2c.h: No such file or directory&lt;/P&gt;&lt;P&gt;However, in the ConfigTools, there is no Problems. Usually, I could just right-click and "solve problem" (add missing dependencies).&lt;/P&gt;&lt;P&gt;The other weird thing is that after I add USB pins, I get multiple problems (including I2C error) which gets solved by right-clicking on a problem.&lt;/P&gt;&lt;P&gt;Is there a way to manually add "fsl_lpi2c.h" through the ConfigTools (I am reluctant to just copy and paste it from some other project)?&lt;/P&gt;</description>
    <pubDate>Fri, 30 Sep 2022 09:17:39 GMT</pubDate>
    <dc:creator>bosnian_beast</dc:creator>
    <dc:date>2022-09-30T09:17:39Z</dc:date>
    <item>
      <title>ConfigTools doesn't recognize error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ConfigTools-doesn-t-recognize-error/m-p/1531004#M195858</link>
      <description>&lt;P&gt;I added I2C pins in my configuration and when I update code, I get this error:&lt;/P&gt;&lt;P&gt;board/peripherals.h:15:10: fatal error: fsl_lpi2c.h: No such file or directory&lt;/P&gt;&lt;P&gt;However, in the ConfigTools, there is no Problems. Usually, I could just right-click and "solve problem" (add missing dependencies).&lt;/P&gt;&lt;P&gt;The other weird thing is that after I add USB pins, I get multiple problems (including I2C error) which gets solved by right-clicking on a problem.&lt;/P&gt;&lt;P&gt;Is there a way to manually add "fsl_lpi2c.h" through the ConfigTools (I am reluctant to just copy and paste it from some other project)?&lt;/P&gt;</description>
      <pubDate>Fri, 30 Sep 2022 09:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ConfigTools-doesn-t-recognize-error/m-p/1531004#M195858</guid>
      <dc:creator>bosnian_beast</dc:creator>
      <dc:date>2022-09-30T09:17:39Z</dc:date>
    </item>
    <item>
      <title>Re: ConfigTools doesn't recognize error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ConfigTools-doesn-t-recognize-error/m-p/1531833#M195916</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206746"&gt;@bosnian_beast&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can add the missing drivers by right clicking the project, under "SDK Management" &amp;gt; "Manage SDK Components". This will open the SDK component window where you can add the lpi2c driver. After doing this, the error should no longer show.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Mon, 03 Oct 2022 22:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ConfigTools-doesn-t-recognize-error/m-p/1531833#M195916</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2022-10-03T22:35:36Z</dc:date>
    </item>
    <item>
      <title>Re: ConfigTools doesn't recognize error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ConfigTools-doesn-t-recognize-error/m-p/1532065#M195947</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot_1.png" style="width: 351px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/195682iC2475B5B62A4965C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot_1.png" alt="Screenshot_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the drivers tab I have i2c checked (but I can't find lpi2c). However in the right column, it says LPI2C. Is it some naming issue?&lt;/P&gt;</description>
      <pubDate>Tue, 04 Oct 2022 09:57:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ConfigTools-doesn-t-recognize-error/m-p/1532065#M195947</guid>
      <dc:creator>bosnian_beast</dc:creator>
      <dc:date>2022-10-04T09:57:51Z</dc:date>
    </item>
    <item>
      <title>Re: ConfigTools doesn't recognize error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ConfigTools-doesn-t-recognize-error/m-p/1532259#M195962</link>
      <description>&lt;P&gt;After adding the i2c driver, you still don't see the "&lt;SPAN&gt;fsl_lpi2c.h&lt;/SPAN&gt;" file under the drivers folder? One more thing, could you please specify the part number you are using, as well as the installed release version you have for MCUXpresso, SDK and ConfigTools (if you are using the standalone release)?&lt;/P&gt;</description>
      <pubDate>Tue, 04 Oct 2022 17:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ConfigTools-doesn-t-recognize-error/m-p/1532259#M195962</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2022-10-04T17:22:42Z</dc:date>
    </item>
  </channel>
</rss>