<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Camera sensor os02g10 MIPI CSI for IMX8MM: Image issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Camera-sensor-os02g10-MIPI-CSI-for-IMX8MM-Image-issue/m-p/1530976#M195854</link>
    <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;Im going to use this command:&lt;BR /&gt;gst-launch-1.0 v4l2src num-buffers=1 ! jpegenc ! filesink location=/tmp/test.jpg&lt;BR /&gt;for now it is not working, comparison ov5640 vs os02g10 tells us that the API from the driver side is not sufficient.&lt;BR /&gt;ov5640 works.&lt;BR /&gt;&lt;BR /&gt;But I can use additional conversion on the PC computer to convert data file from the os02g10.&lt;BR /&gt;I use it:&lt;BR /&gt;&lt;BR /&gt;gst-launch-1.0 -v filesrc location=file_from_os02g10_sensor.raw blocksize=42923008 ! "video/x-bayer,format=bggr,width=1920,height=1080,framerate=1/1" ! bayer2rgb ! videoconvert ! avenc_mjpeg ! filesink location=oputput_file.jpeg&lt;/P&gt;&lt;/BLOCKQUOTE&gt;</description>
    <pubDate>Fri, 30 Sep 2022 08:25:04 GMT</pubDate>
    <dc:creator>btarnowski</dc:creator>
    <dc:date>2022-09-30T08:25:04Z</dc:date>
    <item>
      <title>Camera sensor os02g10 MIPI CSI for IMX8MM: Image issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-sensor-os02g10-MIPI-CSI-for-IMX8MM-Image-issue/m-p/1512386#M194329</link>
      <description>&lt;P&gt;Hi all,&lt;BR /&gt;I got the image from os02g10 camera sensor.&lt;BR /&gt;Settings are: RAW10, 1920x1080, pixelformat = BG10&lt;BR /&gt;hs-settle tested from 7 to 22&lt;/P&gt;&lt;P&gt;clk-settle tested for 0 , 1 ,2&lt;BR /&gt;&lt;BR /&gt;mipic-csi frequency tested in range 333MHz - 480MHz&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;All time the image is the same like below, a colorspace is also the issue.&lt;BR /&gt;What can be wrong?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191439i89D4BED804E829A8/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Aug 2022 13:13:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-sensor-os02g10-MIPI-CSI-for-IMX8MM-Image-issue/m-p/1512386#M194329</guid>
      <dc:creator>btarnowski</dc:creator>
      <dc:date>2022-08-26T13:13:15Z</dc:date>
    </item>
    <item>
      <title>Re: Camera sensor os02g10 MIPI CSI for IMX8MM: Image issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-sensor-os02g10-MIPI-CSI-for-IMX8MM-Image-issue/m-p/1517303#M194754</link>
      <description>&lt;P&gt;FYI.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-Support-Camera-RAW10/m-p/983379#M146063" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-Support-Camera-RAW10/m-p/983379#M146063&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Sep 2022 02:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-sensor-os02g10-MIPI-CSI-for-IMX8MM-Image-issue/m-p/1517303#M194754</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-09-06T02:44:41Z</dc:date>
    </item>
    <item>
      <title>Re: Camera sensor os02g10 MIPI CSI for IMX8MM: Image issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-sensor-os02g10-MIPI-CSI-for-IMX8MM-Image-issue/m-p/1527315#M195540</link>
      <description>&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;I fixed image misalignment issue by this piece of patch:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;@@ -471,7 +505,9 @@ static void csi_init_interface(struct mx6s_csi_dev *csi_dev)
 	val |= BIT_MCLKEN;
 	__raw_writel(val, csi_dev-&amp;gt;regbase + CSI_CSICR1);
 
-	imag_para = (640 &amp;lt;&amp;lt; 16) | 960;
+	dev_info(csi_dev-&amp;gt;dev,"in function: csi_init_interface\n");
+
+	imag_para = (1080 &amp;lt;&amp;lt; 16) | 1920;
 	__raw_writel(imag_para, csi_dev-&amp;gt;regbase + CSI_CSIIMAG_PARA);&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But still there is format issue (color space) and double image issue&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="btarnowski_0-1663928864396.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/194763i9BFA6C4A3ACDE384/image-size/medium?v=v2&amp;amp;px=400" role="button" title="btarnowski_0-1663928864396.png" alt="btarnowski_0-1663928864396.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 23 Sep 2022 10:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-sensor-os02g10-MIPI-CSI-for-IMX8MM-Image-issue/m-p/1527315#M195540</guid>
      <dc:creator>btarnowski</dc:creator>
      <dc:date>2022-09-23T10:27:56Z</dc:date>
    </item>
    <item>
      <title>Re: Camera sensor os02g10 MIPI CSI for IMX8MM: Image issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-sensor-os02g10-MIPI-CSI-for-IMX8MM-Image-issue/m-p/1530976#M195854</link>
      <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;Im going to use this command:&lt;BR /&gt;gst-launch-1.0 v4l2src num-buffers=1 ! jpegenc ! filesink location=/tmp/test.jpg&lt;BR /&gt;for now it is not working, comparison ov5640 vs os02g10 tells us that the API from the driver side is not sufficient.&lt;BR /&gt;ov5640 works.&lt;BR /&gt;&lt;BR /&gt;But I can use additional conversion on the PC computer to convert data file from the os02g10.&lt;BR /&gt;I use it:&lt;BR /&gt;&lt;BR /&gt;gst-launch-1.0 -v filesrc location=file_from_os02g10_sensor.raw blocksize=42923008 ! "video/x-bayer,format=bggr,width=1920,height=1080,framerate=1/1" ! bayer2rgb ! videoconvert ! avenc_mjpeg ! filesink location=oputput_file.jpeg&lt;/P&gt;&lt;/BLOCKQUOTE&gt;</description>
      <pubDate>Fri, 30 Sep 2022 08:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-sensor-os02g10-MIPI-CSI-for-IMX8MM-Image-issue/m-p/1530976#M195854</guid>
      <dc:creator>btarnowski</dc:creator>
      <dc:date>2022-09-30T08:25:04Z</dc:date>
    </item>
    <item>
      <title>Re: Camera sensor os02g10 MIPI CSI for IMX8MM: Image issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-sensor-os02g10-MIPI-CSI-for-IMX8MM-Image-issue/m-p/1575817#M199345</link>
      <description>&lt;P&gt;We found solution for this and more issues, there is more details for RAW10 support on IMX8MM&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Graphics/gst-launch-1-0-returns-Internal-data-stream-error/m-p/1573923#M388" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Graphics/gst-launch-1-0-returns-Internal-data-stream-error/m-p/1573923#M388&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Dec 2022 09:54:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-sensor-os02g10-MIPI-CSI-for-IMX8MM-Image-issue/m-p/1575817#M199345</guid>
      <dc:creator>btarnowski</dc:creator>
      <dc:date>2022-12-30T09:54:06Z</dc:date>
    </item>
  </channel>
</rss>