<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX 8M Mini DRM crash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1529865#M195762</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I do not know which Linux version are you running but we already have a workaround for this scenario, please refer to the following commit:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/commit/?h=lf-5.15.y&amp;amp;id=97b4737f3370e683f585ca6533b01358c21430db" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/commit/?h=lf-5.15.y&amp;amp;id=97b4737f3370e683f585ca6533b01358c21430db&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Wed, 28 Sep 2022 23:54:52 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2022-09-28T23:54:52Z</dc:date>
    <item>
      <title>i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1526692#M195504</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I was trying out the DSI to HDMI bridge on the i.MX 8M Mini EVK. I was plugging in and out two monitors when DRM suddenly crashed. I wanted to report this in the hope you can fix this in an upcoming release.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[  100.445376] [CRTC:33:crtc-0] vblank wait timed out
[  100.450240] WARNING: CPU: 2 PID: 32 at drivers/gpu/drm/drm_atomic_helper.c:1514 drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x2a0
[  100.462255] Modules linked in: overlay fsl_jr_uio caam_jr caamkeyblob_desc caamhash_desc caamalg_desc crypto_engine rng_core authenc libdes imx8m_ddrc crct10dif_ce snd_soc_ak5558 snd_soc_ak4458 caam secvio error snd_soc_fsl_spdif snd_soc_fsl_sai snd_soc_fsl_micfil governor_userspace snd_soc_imx_spdif gpio_ir_recv rc_core imx_bus snd_soc_imx_card fuse
[  100.493347] CPU: 2 PID: 32 Comm: kworker/2:1 Not tainted 5.15.32-lts-next+gfa6c3168595c #1
[  100.501615] Hardware name: FSL i.MX8MM EVK board (DT)
[  100.506669] Workqueue: events adv7511_hpd_work
[  100.511123] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[  100.518088] pc : drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x2a0
[  100.524619] lr : drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x2a0
[  100.531154] sp : ffff80000a04ba00
[  100.534469] x29: ffff80000a04ba00 x28: 0000000000000e21 x27: 0000000000000000
[  100.541613] x26: 0000000000000001 x25: 0000000000000038 x24: ffff0000056e1800
[  100.548758] x23: 0000000000000001 x22: 0000000000000000 x21: ffff000008e9af80
[  100.555899] x20: ffff0000048c1088 x19: 0000000000000000 x18: ffffffffffffffff
[  100.563043] x17: 000000040044ffff x16: 00400032b5503510 x15: ffff80008a04b717
[  100.570188] x14: 0000000000000000 x13: ffff800009c21f40 x12: 000000000000057f
[  100.577332] x11: 00000000000001d5 x10: ffff800009c21f40 x9 : ffff800009c21f40
[  100.584478] x8 : 00000000ffffefff x7 : ffff800009c79f40 x6 : ffff800009c79f40
[  100.591622] x5 : 0000000000000000 x4 : ffff000055b969d0 x3 : ffff000055b99950
[  100.598768] x2 : 0000000000000000 x1 : 0000000000000000 x0 : ffff0000041da940
[  100.605914] Call trace:
[  100.608361]  drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x2a0
[  100.614549]  drm_atomic_helper_wait_for_vblanks+0x1c/0x30
[  100.619953]  lcdif_drm_atomic_commit_tail+0x58/0x80
[  100.624837]  commit_tail+0xa4/0x184
[  100.628330]  drm_atomic_helper_commit+0x160/0x370
[  100.633041]  drm_atomic_commit+0x50/0x60
[  100.636970]  drm_client_modeset_commit_atomic+0x1c8/0x260
[  100.642375]  drm_client_modeset_commit_locked+0x60/0x19c
[  100.647689]  drm_client_modeset_commit+0x34/0x60
[  100.652312]  drm_fb_helper_set_par+0xcc/0x124
[  100.656671]  drm_fb_helper_hotplug_event.part.0+0xb0/0xe0
[  100.662076]  drm_fbdev_client_hotplug+0x180/0x230
[  100.666786]  drm_client_dev_hotplug+0x88/0xe0
[  100.671149]  drm_kms_helper_hotplug_event+0x38/0x50
[  100.676036]  adv7511_hpd_work+0x94/0x184
[  100.679962]  process_one_work+0x1d0/0x354
[  100.683980]  worker_thread+0x13c/0x470
[  100.687731]  kthread+0x154/0x160
[  100.690965]  ret_from_fork+0x10/0x20
[  100.694545] ---[ end trace 74c1803f4c5a8138 ]---

[  120.548728] [drm:drm_crtc_commit_wait] *ERROR* flip_done timed out
[  120.554956] [drm:drm_atomic_helper_wait_for_dependencies] *ERROR* [CRTC:33:crtc-0] commit wait timed out
[  130.788742] [drm:drm_crtc_commit_wait] *ERROR* flip_done timed out
[  130.794970] [drm:drm_atomic_helper_wait_for_dependencies] *ERROR* [CONNECTOR:35:HDMI-A-1] commit wait timed out&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Philippe&lt;/P&gt;</description>
      <pubDate>Thu, 22 Sep 2022 10:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1526692#M195504</guid>
      <dc:creator>philippe_schenk</dc:creator>
      <dc:date>2022-09-22T10:13:02Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1529865#M195762</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I do not know which Linux version are you running but we already have a workaround for this scenario, please refer to the following commit:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/commit/?h=lf-5.15.y&amp;amp;id=97b4737f3370e683f585ca6533b01358c21430db" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/commit/?h=lf-5.15.y&amp;amp;id=97b4737f3370e683f585ca6533b01358c21430db&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 23:54:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1529865#M195762</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-09-28T23:54:52Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1530288#M195792</link>
      <description>&lt;P&gt;Thanks for your reply. The patch you linked is already in the kernel we are using. We are specifically using `Linux 5.15.32_2.0.0`&lt;/P&gt;</description>
      <pubDate>Thu, 29 Sep 2022 08:50:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1530288#M195792</guid>
      <dc:creator>philippe_schenk</dc:creator>
      <dc:date>2022-09-29T08:50:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1533057#M196023</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Thank you for confirmation, we have a more recent Linux version but I do not see anything different at source code I will discuss this internally.&lt;BR /&gt;&lt;BR /&gt;Thank you for your report,&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Oct 2022 00:25:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1533057#M196023</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-10-06T00:25:20Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1534661#M196148</link>
      <description>&lt;P&gt;Thank you for taking this up!&lt;/P&gt;&lt;P&gt;I'm looking forward to the outcome.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Philippe&lt;/P&gt;</description>
      <pubDate>Mon, 10 Oct 2022 07:35:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1534661#M196148</guid>
      <dc:creator>philippe_schenk</dc:creator>
      <dc:date>2022-10-10T07:35:33Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1538030#M196378</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I have tried on my side multiple times to replicate the crash but I couldn’t, I'm using the following setup:&lt;BR /&gt;&lt;BR /&gt;i.MX8MMini LPDDR4 (CPU2) EVK.&lt;BR /&gt;MIPI-DSI to HDMI bridge&lt;BR /&gt;HDMI Bi-Direction Switch&lt;BR /&gt;2 different HDMI Monitors&lt;BR /&gt;Linux version 5.15.32&lt;BR /&gt;&lt;BR /&gt;I have used the switch to keep changing between the 2 HDMI monitors but no crash seen on DRM.&lt;BR /&gt;Next, I tried only using one or the other by plugging in and out HDMI, but same result no crash seen on DRM.&lt;BR /&gt;&lt;BR /&gt;Could you share detailed steps to replicate?&lt;BR /&gt;Also, how easy is to reproduce this?&lt;BR /&gt;Does it happen randomly?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Oct 2022 20:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1538030#M196378</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-10-14T20:58:14Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1538669#M196453</link>
      <description>&lt;P&gt;Hi Aldo,&lt;/P&gt;&lt;P&gt;Thank you very much for answering and trying to reproduce the issue. I also tried again and compiled a detailed step-by-step guide how to reproduce this issue. I am aware that this seems a very "niche" bug however it indicates that DRM handles EDID wrongly - hence it probably only occurs when using different resolution monitors.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;# Boot NXP i.MX Release Distro 5.15-kirkstone
# On i.MX8M Mini EVK
# With attached DSI-to-HDMI adapter

# In U-Boot
setenv fdtfile imx8mm-evk.dtb
saveenv
boot
# In Linux
systemctl stop weston
## Plug in first monitor
## Then force the default-mode of the monitor
modetest -s 35:#0
## Press &amp;lt;enter&amp;gt; to terminate modetest

## Plug in second monitor
## - I cannot reproduce it with two Full-HD monitors
## - I use a 1280x1024 and 1920x1080 monitor&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Philippe&lt;/P&gt;</description>
      <pubDate>Mon, 17 Oct 2022 15:26:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1538669#M196453</guid>
      <dc:creator>philippe_schenk</dc:creator>
      <dc:date>2022-10-17T15:26:17Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1547237#M197078</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I'm still working with internal team regarding this issue, team is testing with different resolutions, but would it be possible to test with lower resolution (720p) on your side?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Nov 2022 23:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1547237#M197078</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-11-01T23:47:30Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1547735#M197119</link>
      <description>&lt;P&gt;Hi Aldo,&lt;/P&gt;&lt;P&gt;Thanks for coming back to me. If you still couldn't reproduce on your side I suggest we don't waste our times on this issue. It is not that important after all and very specific use-case that is not often used most probably.&lt;BR /&gt;&lt;BR /&gt;Thanks and Best Regards,&lt;BR /&gt;Philippe&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 12:00:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1547735#M197119</guid>
      <dc:creator>philippe_schenk</dc:creator>
      <dc:date>2022-11-02T12:00:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1547960#M197136</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Thank you for your consideration, I'll continue investigating the issue with low priority and let you know of the results here later.&lt;BR /&gt;&lt;BR /&gt;Thank you for your report,&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Nov 2022 00:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1547960#M197136</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-11-03T00:07:20Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1560655#M198099</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I think I found another way to reproduce this issue. I do the following steps:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;Boot with 1920x1080 display connected&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Disconnect 1920x1080 display&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;Wait 10s (because of polling mode)&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Connect 1280x720 display&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;reboot&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Then this message appears:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[   53.647167] ------------[ cut here ]------------
[   53.651901] [CRTC:33:crtc-0] vblank wait timed out
[   53.656829] WARNING: CPU: 0 PID: 1 at drivers/gpu/drm/drm_atomic_helper.c:1524 drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x2a0
[   53.668974] Modules linked in: rfcomm algif_hash algif_skcipher af_alg fsl_jr_uio caam_jr caamkeyblob_desc caamhash_desc caamalg_desc mcp251xfd crypto_engine rng_core authenc libdes can_dev crct10dif_ce mwifiex_sdio mwifiex imx8m_ddrc btmrvl_sdio btmrvl sec_mipi_dsim_imx bluetooth sec_dsim governor_userspace imx_be
[   53.709642] CPU: 0 PID: 1 Comm: systemd Tainted: G           O      5.15.77-6.1.0-devel+git.8053ffcbece2 #1
[   53.719555] Hardware name: Toradex Verdin iMX8M Mini WB on Verdin Development Board (DT)
[   53.727786] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   53.734871] pc : drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x2a0
[   53.741518] lr : drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x2a0
[   53.748162] sp : ffff800009c4b930
[   53.751535] x29: ffff800009c4b930 x28: 00000000000006f6 x27: 0000000000000000
[   53.758803] x26: 0000000000000001 x25: 0000000000000038 x24: ffff00000117e800
[   53.766071] x23: 0000000000000001 x22: 0000000000000000 x21: ffff00000c1f5280
[   53.773336] x20: ffff000000480088 x19: 0000000000000000 x18: ffffffffffffffff
[   53.780604] x17: 000000040044ffff x16: 0000000000000001 x15: ffff800089c4b647
[   53.787871] x14: 0000000000000000 x13: ffff800009a12500 x12: 0000000000000528
[   53.795137] x11: 00000000000001b8 x10: ffff800009a12500 x9 : ffff800009a12500
[   53.802403] x8 : 00000000ffffefff x7 : ffff800009a6a500 x6 : ffff800009a6a500
[   53.809670] x5 : 0000000000000000 x4 : ffff00003fd809d0 x3 : ffff00003fd83990
[   53.816937] x2 : 0000000000000000 x1 : 0000000000000000 x0 : ffff0000000a8000
[   53.824203] Call trace:
[   53.826694]  drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x2a0
[   53.832986]  drm_atomic_helper_wait_for_vblanks+0x18/0x30
[   53.838482]  lcdif_drm_atomic_commit_tail+0x54/0x70
[   53.843454]  commit_tail+0xa0/0x180
[   53.847008]  drm_atomic_helper_commit+0x160/0x370
[   53.851798]  drm_atomic_commit+0x4c/0x60
[   53.855795]  drm_client_modeset_commit_atomic+0x1c8/0x260
[   53.861291]  drm_client_modeset_commit_locked+0x5c/0x1a0
[   53.866698]  drm_client_modeset_commit+0x30/0x60
[   53.871399]  drm_fb_helper_set_par+0xc8/0x120
[   53.875835]  drm_fb_helper_hotplug_event.part.0+0xb0/0xe0
[   53.881333]  drm_fbdev_client_restore+0x98/0xd0
[   53.888947]  drm_client_dev_restore+0x84/0xdc
[   53.896367]  drm_lastclose+0x6c/0x7c
[   53.902874]  drm_release+0xfc/0x114
[   53.909153]  __fput+0x70/0x240
[   53.914857]  ____fput+0x10/0x20
[   53.920502]  task_work_run+0x80/0x180
[   53.926544]  do_notify_resume+0x200/0x12ec
[   53.932898]  el0_svc+0x6c/0x80
[   53.938089]  el0t_64_sync_handler+0xa4/0x130
[   53.944425]  el0t_64_sync+0x1a0/0x1a4
[   53.950067] ---[ end trace 5ea06ebb2e853670 ]---&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;It is not exactly the same but it is also related to drm_fb_helper_hotplug_event.part. I think it is because the drm drivers are unloaded/not fully working anymore when fbdev wants to process the hotplug event.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Nov 2022 13:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1560655#M198099</guid>
      <dc:creator>stefan_eichenberger</dc:creator>
      <dc:date>2022-11-28T13:43:40Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1565425#M198417</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Thank you for sharing more details, I have forwarded to internal team so they can continue investigating this issue.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 20:45:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1565425#M198417</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-12-06T20:45:06Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini DRM crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1586302#M200474</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144876"&gt;@philippe_schenk&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;We are still looking into this, could you share the details of the monitor/display that you're using for myour test, like brand and model?&lt;BR /&gt;&lt;BR /&gt;Thank you,&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jan 2023 22:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-DRM-crash/m-p/1586302#M200474</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-01-20T22:57:33Z</dc:date>
    </item>
  </channel>
</rss>