<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX6UL EVK : how do I use the Arduino shield UART ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-EVK-how-do-I-use-the-Arduino-shield-UART/m-p/1529397#M195729</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to use the UART brought to the Arduino shield footprint on the EVK baseboard.&lt;/P&gt;&lt;P&gt;I am running Linux off the SD card provided with the EVK.&lt;/P&gt;&lt;P&gt;"dmesg" shows that two UART are setup : ttymxc0 and ttymxc1, with the former being used for the console (USB-to-UART adapter chip).&lt;/P&gt;&lt;P&gt;I assume that it means ttymxc1 is the UART available on the shield pads. However, I can't get anything out of it.&lt;/P&gt;&lt;P&gt;I use minicom to send out bytes and check with an oscilloscope, nothing comes out. I tried shorting TX and RX, and I get no echo. The pins are both stuck to 3.3 V all the time.&lt;/P&gt;&lt;P&gt;I'm rather in a hurry and would like to avoid a deep dive into the EVK and the way Linux is setup. I'm hoping there's something simple I'm missing. Any help will be welcome.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jean Roch&lt;/P&gt;</description>
    <pubDate>Wed, 28 Sep 2022 08:48:56 GMT</pubDate>
    <dc:creator>Nefastor</dc:creator>
    <dc:date>2022-09-28T08:48:56Z</dc:date>
    <item>
      <title>iMX6UL EVK : how do I use the Arduino shield UART ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-EVK-how-do-I-use-the-Arduino-shield-UART/m-p/1529397#M195729</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to use the UART brought to the Arduino shield footprint on the EVK baseboard.&lt;/P&gt;&lt;P&gt;I am running Linux off the SD card provided with the EVK.&lt;/P&gt;&lt;P&gt;"dmesg" shows that two UART are setup : ttymxc0 and ttymxc1, with the former being used for the console (USB-to-UART adapter chip).&lt;/P&gt;&lt;P&gt;I assume that it means ttymxc1 is the UART available on the shield pads. However, I can't get anything out of it.&lt;/P&gt;&lt;P&gt;I use minicom to send out bytes and check with an oscilloscope, nothing comes out. I tried shorting TX and RX, and I get no echo. The pins are both stuck to 3.3 V all the time.&lt;/P&gt;&lt;P&gt;I'm rather in a hurry and would like to avoid a deep dive into the EVK and the way Linux is setup. I'm hoping there's something simple I'm missing. Any help will be welcome.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jean Roch&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 08:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-EVK-how-do-I-use-the-Arduino-shield-UART/m-p/1529397#M195729</guid>
      <dc:creator>Nefastor</dc:creator>
      <dc:date>2022-09-28T08:48:56Z</dc:date>
    </item>
  </channel>
</rss>