<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6 UL PIN MULTIPLEXING</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-UL-PIN-MULTIPLEXING/m-p/1527861#M195595</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201596"&gt;@riteshmpatel&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Hope you are doing well.&lt;/P&gt;&lt;P&gt;Can I configure the pin at runtime?&lt;/P&gt;&lt;P&gt;Or should I need to reboot every time for new configuration?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Hamza Hassan&lt;/P&gt;</description>
    <pubDate>Mon, 26 Sep 2022 05:58:00 GMT</pubDate>
    <dc:creator>Hamza_Hassan</dc:creator>
    <dc:date>2022-09-26T05:58:00Z</dc:date>
    <item>
      <title>IMX6 UL PIN MULTIPLEXING</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-UL-PIN-MULTIPLEXING/m-p/1525842#M195448</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using IMX6.UL processor pin . I am using RS232 transmitter using serial port. Can i use the same pin as GPIO for transmitting IR signal.&lt;/P&gt;&lt;P&gt;Is there any support in IMX6?&lt;/P&gt;&lt;P&gt;Please guide me on this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 21 Sep 2022 11:37:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-UL-PIN-MULTIPLEXING/m-p/1525842#M195448</guid>
      <dc:creator>Hamza_Hassan</dc:creator>
      <dc:date>2022-09-21T11:37:00Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 UL PIN MULTIPLEXING</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-UL-PIN-MULTIPLEXING/m-p/1527368#M195544</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205449"&gt;@Hamza_Hassan&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;One can check the Available mux options of the pin which is configured as a RS232 Transmitter in RM. If the possible pad is GPIO*, then you can configure the same pin as a GPIO for transmitting IR signal.&lt;BR /&gt;Please note that once you configure this pin as a GPIO, After that you will not be able to use the same pin as Rs232 Transmitter.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Fri, 23 Sep 2022 12:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-UL-PIN-MULTIPLEXING/m-p/1527368#M195544</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2022-09-23T12:16:41Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 UL PIN MULTIPLEXING</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-UL-PIN-MULTIPLEXING/m-p/1527861#M195595</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201596"&gt;@riteshmpatel&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Hope you are doing well.&lt;/P&gt;&lt;P&gt;Can I configure the pin at runtime?&lt;/P&gt;&lt;P&gt;Or should I need to reboot every time for new configuration?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Hamza Hassan&lt;/P&gt;</description>
      <pubDate>Mon, 26 Sep 2022 05:58:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-UL-PIN-MULTIPLEXING/m-p/1527861#M195595</guid>
      <dc:creator>Hamza_Hassan</dc:creator>
      <dc:date>2022-09-26T05:58:00Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 UL PIN MULTIPLEXING</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-UL-PIN-MULTIPLEXING/m-p/1528039#M195609</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205449"&gt;@Hamza_Hassan&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Unforutnately, doing runtime configurations is not possible.&lt;/P&gt;
&lt;P&gt;The configurations must be done in dts.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Mon, 26 Sep 2022 09:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-UL-PIN-MULTIPLEXING/m-p/1528039#M195609</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2022-09-26T09:20:11Z</dc:date>
    </item>
  </channel>
</rss>