<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックConfiguring LPSPI to transfer data using DMA</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-LPSPI-to-transfer-data-using-DMA/m-p/1527652#M195580</link>
    <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I need help configuring the LPSPI module of the IMXRT1062 processor to use DMA unit to transfer data to an external DAC from a sine lookup table. I want to generate a 1 kHz AM sine wave. The CPU is preoccupied with other necessary tasks and assigning the generation of the sine wave to the CPU would badly affect the system performance. I also want a callback function to be called when a complete cycle of a sine wave is generated. The lookup table has 128 entries for a complete sine wave cycle. We are using MQX RTOS. Any help and preferably examples would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Sun, 25 Sep 2022 06:02:36 GMT</pubDate>
    <dc:creator>Amrit_9t8</dc:creator>
    <dc:date>2022-09-25T06:02:36Z</dc:date>
    <item>
      <title>Configuring LPSPI to transfer data using DMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-LPSPI-to-transfer-data-using-DMA/m-p/1527652#M195580</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I need help configuring the LPSPI module of the IMXRT1062 processor to use DMA unit to transfer data to an external DAC from a sine lookup table. I want to generate a 1 kHz AM sine wave. The CPU is preoccupied with other necessary tasks and assigning the generation of the sine wave to the CPU would badly affect the system performance. I also want a callback function to be called when a complete cycle of a sine wave is generated. The lookup table has 128 entries for a complete sine wave cycle. We are using MQX RTOS. Any help and preferably examples would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Sun, 25 Sep 2022 06:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-LPSPI-to-transfer-data-using-DMA/m-p/1527652#M195580</guid>
      <dc:creator>Amrit_9t8</dc:creator>
      <dc:date>2022-09-25T06:02:36Z</dc:date>
    </item>
  </channel>
</rss>