<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Cannot connect/ succeed to flash with uuu on iMX8QM COM module</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-connect-succeed-to-flash-with-uuu-on-iMX8QM-COM-module/m-p/1524538#M195331</link>
    <description>&lt;P&gt;Yea, when I will need to write one I shall.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you also please improve the English version documentation of UUU .. ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some of the messages and the text in the doc look like uses English letters but not making much sense.&lt;/P&gt;</description>
    <pubDate>Mon, 19 Sep 2022 23:50:32 GMT</pubDate>
    <dc:creator>dry</dc:creator>
    <dc:date>2022-09-19T23:50:32Z</dc:date>
    <item>
      <title>Cannot connect/ succeed to flash with uuu on iMX8QM COM module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-connect-succeed-to-flash-with-uuu-on-iMX8QM-COM-module/m-p/1518037#M194830</link>
      <description>&lt;P&gt;I got a module from Kontron based on iMX8QM.&lt;/P&gt;&lt;P&gt;Here is what U-boot shows :&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;U-Boot 2019.04-4.19.35-1.1.0+g4d37753 (Jun 02 2022 - 21:24:12 +0000)

CPU: NXP i.MX8QM RevB A53 at 1200 MHz at 33C

BuildInfo:
- SCFW 4e91f37b, SECO-FW d7523fe8, IMX-MKIMAGE 1c2277b9, ATF 70fa7bc
- U-Boot 2019.04-4.19.35-1.1.0+g4d37753&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to burn in / update Linux image - or actually at the moment any image, U-boot or /and Linux&amp;nbsp; - using the UUU utility, with no success.&lt;/P&gt;&lt;P&gt;I can set to board/COM into the manufacturing mode per board doc, where supposedly it should be ready to use for UUU.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is what the dev shows up as when I plug it into Win10 PC when the module is in "recovery" or manufacturing mode:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dry_0-1662511956875.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/192735i5F9E18F930A80410/image-size/medium?v=v2&amp;amp;px=400" role="button" title="dry_0-1662511956875.png" alt="dry_0-1662511956875.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;uuu -lsusb
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51

Connected Known USB Devices
        Path     Chip    Pro     Vid     Pid     BcdVersion
        ==================================================
        1:83114  MX8QM   SDPS:   0x1FC9 0x0129   0x0002&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And from here I cannot get anywhere ...&amp;nbsp; E.g:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;&amp;gt;uuu -b emmc  kontron-image-qt5-validation-samx-kontron-samx8-qm.sdcard.bz2/*
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51

Success 0    Failure 1


1:83114  1/ 1 [HID(W):LIBUSB_ERROR_PIPE              ] SDPS: boot -f kontron-image-qt5-validation-samx-kontron-samx8-qm.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;uuu -b emmc imx-boot-kontron-samx8-qm-fspi-8GB.bin
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51

Success 0    Failure 1


1:83114  1/ 1 [HID(W):LIBUSB_ERROR_PIPE              ] SDPS: boot -f imx-boot-kontron-samx8-qm-fspi-8GB.bin&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is just a delay, then device resets and back into the default internally programmed u-boot shell.&lt;/P&gt;&lt;P&gt;Always ends up in that.&lt;/P&gt;&lt;P&gt;There is very little helpful messages from uuu.&amp;nbsp; Is the device correct, why does it always end into libusb error ... ?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Sep 2022 01:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-connect-succeed-to-flash-with-uuu-on-iMX8QM-COM-module/m-p/1518037#M194830</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2022-09-07T01:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect/ succeed to flash with uuu on iMX8QM COM module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-connect-succeed-to-flash-with-uuu-on-iMX8QM-COM-module/m-p/1519002#M194902</link>
      <description>&lt;P&gt;If I start the "fastboot" from inside the U-boot, then I can update U-boot, rootfs using the FB protocol.&lt;/P&gt;&lt;P&gt;But need to figure out how I can do update over SPD(s?) too, in case U-boot is kaputt.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Sep 2022 05:31:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-connect-succeed-to-flash-with-uuu-on-iMX8QM-COM-module/m-p/1519002#M194902</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2022-09-08T05:31:11Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect/ succeed to flash with uuu on iMX8QM COM module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-connect-succeed-to-flash-with-uuu-on-iMX8QM-COM-module/m-p/1523422#M195249</link>
      <description>&lt;P&gt;Please read the &lt;A class="Truncate" href="https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.4.243/UUU.pdf" rel="nofollow" data-skip-pjax="true" data-turbo="false" data-view-component="true" target="_blank"&gt; &lt;SPAN class="Truncate-text text-bold" data-view-component="true"&gt;UUU.pdf&lt;/SPAN&gt;&amp;nbsp; &lt;/A&gt;for how to write the script to program the board.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Sep 2022 06:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-connect-succeed-to-flash-with-uuu-on-iMX8QM-COM-module/m-p/1523422#M195249</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-09-16T06:26:14Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect/ succeed to flash with uuu on iMX8QM COM module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-connect-succeed-to-flash-with-uuu-on-iMX8QM-COM-module/m-p/1524538#M195331</link>
      <description>&lt;P&gt;Yea, when I will need to write one I shall.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you also please improve the English version documentation of UUU .. ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some of the messages and the text in the doc look like uses English letters but not making much sense.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Sep 2022 23:50:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-connect-succeed-to-flash-with-uuu-on-iMX8QM-COM-module/m-p/1524538#M195331</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2022-09-19T23:50:32Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect/ succeed to flash with uuu on iMX8QM COM module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-connect-succeed-to-flash-with-uuu-on-iMX8QM-COM-module/m-p/1529862#M195761</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/1422"&gt;@jimmychan&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please assist with the following issue I'm having.&lt;/P&gt;&lt;P&gt;Firstly, I can flash flash_scfw.bin - that is, my own built image of the scfw from the official sources, it is flashed and started Ok as I can very by seing SCFW traces on a UART (built with debug enabled).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dry_1-1664407363632.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/195220i7559062072787F58/image-size/medium?v=v2&amp;amp;px=400" role="button" title="dry_1-1664407363632.png" alt="dry_1-1664407363632.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But anything seems large in size - like image with U-boot - FAILS to be uploaded &amp;amp; started, at least per the UUU traces.&amp;nbsp;&lt;BR /&gt;In my test I try to upload the "flash" image (without linux) with U-boot as was created by Yocto imx8qm (my soc) build. In this case I get same error trace from UUU as I have originally posted, and the board re-starts:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dry_2-1664407648755.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/195222i5486338F0DFE20A4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="dry_2-1664407648755.png" alt="dry_2-1664407648755.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So why ... ? Is this a USB transfer problem or ..?&lt;/P&gt;&lt;P&gt;I'm attaching the firmware blob - this was generated by Yocto , under ...&amp;nbsp;imx-boot/0.2-r0/git/iMX8QM/, file flash.bin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 23:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-connect-succeed-to-flash-with-uuu-on-iMX8QM-COM-module/m-p/1529862#M195761</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2022-09-28T23:31:27Z</dc:date>
    </item>
  </channel>
</rss>