<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1176 JTAG_MOD pin in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1524506#M195330</link>
    <description>&lt;P&gt;Hello &lt;BR /&gt;Hope you are well.&lt;/P&gt;
&lt;P&gt;When JTAG_MOD is &lt;STRONG&gt;low&lt;/STRONG&gt;, the JTAG interface is configured for a common software debug, adding all the system TAPs to the chain. &lt;BR /&gt;When JTAG_MOD is &lt;STRONG&gt;high&lt;/STRONG&gt;, the JTAG interface is configured to a mode compliant with the IEEE 1149.1 standard.&lt;BR /&gt;JTAG_MOD shall be externally connected to GND for normal operation in a system. The termination to GND through an external pull-down resistor is allowed using a 4.7-kΩ resistor.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Mon, 19 Sep 2022 22:40:06 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2022-09-19T22:40:06Z</dc:date>
    <item>
      <title>RT1176 JTAG_MOD pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1523069#M195231</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We designed a custom board with IMXRT1176. We connected to board all JTAG pins. But JTAG_MOD pin is float. We can not make JTAG connection. What can you suggested us?&lt;/P&gt;</description>
      <pubDate>Thu, 15 Sep 2022 16:46:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1523069#M195231</guid>
      <dc:creator>karaca</dc:creator>
      <dc:date>2022-09-15T16:46:55Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 JTAG_MOD pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1524506#M195330</link>
      <description>&lt;P&gt;Hello &lt;BR /&gt;Hope you are well.&lt;/P&gt;
&lt;P&gt;When JTAG_MOD is &lt;STRONG&gt;low&lt;/STRONG&gt;, the JTAG interface is configured for a common software debug, adding all the system TAPs to the chain. &lt;BR /&gt;When JTAG_MOD is &lt;STRONG&gt;high&lt;/STRONG&gt;, the JTAG interface is configured to a mode compliant with the IEEE 1149.1 standard.&lt;BR /&gt;JTAG_MOD shall be externally connected to GND for normal operation in a system. The termination to GND through an external pull-down resistor is allowed using a 4.7-kΩ resistor.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 19 Sep 2022 22:40:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1524506#M195330</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-09-19T22:40:06Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 JTAG_MOD pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1524718#M195349</link>
      <description>&lt;P&gt;Hi Omar,&lt;/P&gt;&lt;P&gt;Thanks for your information. JTAG_MOD is float in our hardware. Can we change JTAG_MOD pin to float with software? We can use USB and UART communications but we need JTAG.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Sep 2022 06:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1524718#M195349</guid>
      <dc:creator>karaca</dc:creator>
      <dc:date>2022-09-20T06:12:02Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 JTAG_MOD pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1525225#M195386</link>
      <description>&lt;P&gt;Unfortunately, JTAG_MOD needs to be externally connected to GND so JTAG works correctly.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Tue, 20 Sep 2022 18:28:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1525225#M195386</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-09-20T18:28:33Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 JTAG_MOD pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1525567#M195416</link>
      <description>&lt;P&gt;Hi Omar,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We connected JTAG_MOD pin to GND with rework. But we still can not connect JTAG. Our connection in below.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="karaca_0-1663741931538.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/194446iDBC04D4EF5759701/image-size/medium?v=v2&amp;amp;px=400" role="button" title="karaca_0-1663741931538.png" alt="karaca_0-1663741931538.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you have any suggestion?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks. Regards.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Sep 2022 06:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1525567#M195416</guid>
      <dc:creator>karaca</dc:creator>
      <dc:date>2022-09-21T06:32:33Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 JTAG_MOD pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1527015#M195522</link>
      <description>&lt;P&gt;It is important that you´ve followed the recommendations from the Hardware Development Guide. External resistors can be used with all JTAG signals except for JTAG_TDO, but they are not required. &lt;BR /&gt;Did you burn any fuse?&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 22 Sep 2022 23:37:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-JTAG-MOD-pin/m-p/1527015#M195522</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-09-22T23:37:17Z</dc:date>
    </item>
  </channel>
</rss>