<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8QM SDK2.9 PWM driver missing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-SDK2-9-PWM-driver-missing/m-p/1524063#M195292</link>
    <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for the reply&lt;/P&gt;&lt;P&gt;Is there any plan for supporting the PWM module ? if not, is it possible to port the pwm.c/.h from another SDK for use with the IMX8QM ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 19 Sep 2022 07:19:09 GMT</pubDate>
    <dc:creator>AhmedMobarez</dc:creator>
    <dc:date>2022-09-19T07:19:09Z</dc:date>
    <item>
      <title>IMX8QM SDK2.9 PWM driver missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-SDK2-9-PWM-driver-missing/m-p/1519768#M194967</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I just started using IMX8 QuadMax, going through the reference manual I can see that there are multiple ways to generate PWM, which are:&lt;/P&gt;&lt;P&gt;- TPM module : fsl_tpm.c , fsl_tpm.h&lt;/P&gt;&lt;P&gt;- FTM module : fsl_ftm.c, fsl_ftm.h&lt;/P&gt;&lt;P&gt;- PWM module : No driver available&lt;/P&gt;&lt;P&gt;In the latest available SDK2.9 there is no "fsl_pwm.c/.h" drivers available, is there something I am missing ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;please let me know if this driver is available or not, I know it should be there as it is mentioned in the datasheet and also the online SDK&amp;nbsp;&lt;A href="https://mcuxpresso.nxp.com/api_doc/dev/1523/a00063.html" target="_blank"&gt;https://mcuxpresso.nxp.com/api_doc/dev/1523/a00063.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I would like to use the PWM module rather than the other ones as I have more PWM pins available on the board I am using.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Fri, 09 Sep 2022 07:10:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-SDK2-9-PWM-driver-missing/m-p/1519768#M194967</guid>
      <dc:creator>AhmedMobarez</dc:creator>
      <dc:date>2022-09-09T07:10:43Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM SDK2.9 PWM driver missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-SDK2-9-PWM-driver-missing/m-p/1524049#M195291</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206043"&gt;@AhmedMobarez&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Yes, you are right, there is no build error or anything that you have missed. But for i.MX8QM, there is no specific PWM driver support.&lt;/P&gt;
&lt;P&gt;One can take reference of &lt;EM&gt;"/boards/mekmimx8qm/driver_examples/tpm/".&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Dhruvit.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Sep 2022 07:07:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-SDK2-9-PWM-driver-missing/m-p/1524049#M195291</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2022-09-19T07:07:50Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM SDK2.9 PWM driver missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-SDK2-9-PWM-driver-missing/m-p/1524063#M195292</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for the reply&lt;/P&gt;&lt;P&gt;Is there any plan for supporting the PWM module ? if not, is it possible to port the pwm.c/.h from another SDK for use with the IMX8QM ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Sep 2022 07:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-SDK2-9-PWM-driver-missing/m-p/1524063#M195292</guid>
      <dc:creator>AhmedMobarez</dc:creator>
      <dc:date>2022-09-19T07:19:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM SDK2.9 PWM driver missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-SDK2-9-PWM-driver-missing/m-p/1524144#M195302</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206043"&gt;@AhmedMobarez&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;There is no update planned related to this PWM driver for i.MX8QM as of now.&lt;/P&gt;
&lt;P&gt;Yes, one can port&amp;nbsp;the pwm.c/.h from another SDK for use with the IMX8QM, but NXP does not provide any support for it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Dhruvit.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Sep 2022 08:41:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-SDK2-9-PWM-driver-missing/m-p/1524144#M195302</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2022-09-19T08:41:25Z</dc:date>
    </item>
  </channel>
</rss>