<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx6sl can't boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6sl-can-t-boot/m-p/1522958#M195216</link>
    <description>&lt;P&gt;The PCBA board we used before works normally. And&amp;nbsp;there is mass production.&lt;/P&gt;&lt;P&gt;But, the pcba produced this time cannot be started normally. The software uses the same one. If we replace the ixm6sl, it will work normally. Compared with imx6sl Part Number, there are the following differences：&lt;/P&gt;&lt;P&gt;MCIMX6L8DVN10AA :can't boot&amp;nbsp;completely.&lt;/P&gt;&lt;P&gt;MCIMX6L8DVN10AB: it works well.&lt;/P&gt;&lt;P&gt;Each problematic board runs to the same log and stops.See the attachment for details.&lt;/P&gt;</description>
    <pubDate>Thu, 15 Sep 2022 13:48:11 GMT</pubDate>
    <dc:creator>Oman</dc:creator>
    <dc:date>2022-09-15T13:48:11Z</dc:date>
    <item>
      <title>imx6sl can't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6sl-can-t-boot/m-p/1522958#M195216</link>
      <description>&lt;P&gt;The PCBA board we used before works normally. And&amp;nbsp;there is mass production.&lt;/P&gt;&lt;P&gt;But, the pcba produced this time cannot be started normally. The software uses the same one. If we replace the ixm6sl, it will work normally. Compared with imx6sl Part Number, there are the following differences：&lt;/P&gt;&lt;P&gt;MCIMX6L8DVN10AA :can't boot&amp;nbsp;completely.&lt;/P&gt;&lt;P&gt;MCIMX6L8DVN10AB: it works well.&lt;/P&gt;&lt;P&gt;Each problematic board runs to the same log and stops.See the attachment for details.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Sep 2022 13:48:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6sl-can-t-boot/m-p/1522958#M195216</guid>
      <dc:creator>Oman</dc:creator>
      <dc:date>2022-09-15T13:48:11Z</dc:date>
    </item>
    <item>
      <title>回复： imx6sl can't boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6sl-can-t-boot/m-p/1523923#M195284</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;,dear, could you help me?&lt;/P&gt;</description>
      <pubDate>Mon, 19 Sep 2022 02:29:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6sl-can-t-boot/m-p/1523923#M195284</guid>
      <dc:creator>Oman</dc:creator>
      <dc:date>2022-09-19T02:29:19Z</dc:date>
    </item>
  </channel>
</rss>