<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8MP - enableing MMC_DEBUG_CONFIG</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-enableing-MMC-DEBUG-CONFIG/m-p/1521463#M195088</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;There are a number of options in your menuconfig -&amp;gt; bitbake linux-imx -c menuconfig (or some kernel name). Check -&amp;gt; Device drivers -&amp;gt;&amp;nbsp; MMC/SD/SDIO support -&amp;gt;&amp;nbsp; [*] MMC host drivers debugging&lt;/P&gt;&lt;P&gt;&amp;lt;help&amp;gt; CONFIG_MMC_DEBUG: This enables MMC host driver debugging.&amp;nbsp;&amp;nbsp;There's some other debug stuff in there as well.&lt;/P&gt;&lt;P&gt;Worst case there's printk which can be added like printf in drivers and that woud require enabling under&amp;nbsp;'kernel hacking'. Inside 'kernel hacking' there are lots of other debugging options in there as well.&lt;/P&gt;&lt;P&gt;After any changes do a rebuild. Beware kernel changes can be lost after kernel cleans etc..&lt;/P&gt;&lt;P&gt;Check dmesg as well for kernel info..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope any of this helps.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Sep 2022 21:44:01 GMT</pubDate>
    <dc:creator>edwardtyrrell</dc:creator>
    <dc:date>2022-09-13T21:44:01Z</dc:date>
    <item>
      <title>IMX8MP - enableing MMC_DEBUG_CONFIG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-enableing-MMC-DEBUG-CONFIG/m-p/1519925#M194978</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have an i.MX8MP board (Phytec phycore to be precise) and am building a custom yocto recipe.&lt;/P&gt;&lt;P&gt;I am adding an second MMC on usdhc1 (mmc0)&lt;/P&gt;&lt;P&gt;I unfortunately have some communication problems and would like to have more MMC debugging data.&lt;/P&gt;&lt;P&gt;I enabled CONFIG_MMC_DEBUG in my fragment.cfg (and checked it was applied in my build directory)&lt;/P&gt;&lt;P&gt;Unfortunately I have no extra messages in dmeg / run/log/journal (using klog for logging)&lt;/P&gt;&lt;P&gt;is there another option that needs to be activated to see mmc debugging messages?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help!&lt;/P&gt;&lt;P&gt;Liliane&lt;/P&gt;</description>
      <pubDate>Fri, 09 Sep 2022 09:42:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-enableing-MMC-DEBUG-CONFIG/m-p/1519925#M194978</guid>
      <dc:creator>LilianeD</dc:creator>
      <dc:date>2022-09-09T09:42:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP - enableing MMC_DEBUG_CONFIG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-enableing-MMC-DEBUG-CONFIG/m-p/1521463#M195088</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;There are a number of options in your menuconfig -&amp;gt; bitbake linux-imx -c menuconfig (or some kernel name). Check -&amp;gt; Device drivers -&amp;gt;&amp;nbsp; MMC/SD/SDIO support -&amp;gt;&amp;nbsp; [*] MMC host drivers debugging&lt;/P&gt;&lt;P&gt;&amp;lt;help&amp;gt; CONFIG_MMC_DEBUG: This enables MMC host driver debugging.&amp;nbsp;&amp;nbsp;There's some other debug stuff in there as well.&lt;/P&gt;&lt;P&gt;Worst case there's printk which can be added like printf in drivers and that woud require enabling under&amp;nbsp;'kernel hacking'. Inside 'kernel hacking' there are lots of other debugging options in there as well.&lt;/P&gt;&lt;P&gt;After any changes do a rebuild. Beware kernel changes can be lost after kernel cleans etc..&lt;/P&gt;&lt;P&gt;Check dmesg as well for kernel info..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope any of this helps.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Sep 2022 21:44:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-enableing-MMC-DEBUG-CONFIG/m-p/1521463#M195088</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2022-09-13T21:44:01Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP - enableing MMC_DEBUG_CONFIG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-enableing-MMC-DEBUG-CONFIG/m-p/1526752#M195511</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201566"&gt;@LilianeD&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please try adding printk for the prints and changing the print debug level to the max for all prints?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Dhruvit.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Sep 2022 12:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-enableing-MMC-DEBUG-CONFIG/m-p/1526752#M195511</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2022-09-22T12:22:35Z</dc:date>
    </item>
  </channel>
</rss>