<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.mx8 audio; Using SAI as slave with external MCLK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8-audio-Using-SAI-as-slave-with-external-MCLK/m-p/1520632#M195037</link>
    <description>&lt;P&gt;I am looking for help to use an external clock source to drive an SAI on the i.mx8.&amp;nbsp; I need to connect the M4F core to the SAI so I need some device tree modifications.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Suppose you have an external clock source (from a codec that is the master of the I2S clocks) to be used to clock SAI2 and that the M4F core will be doing SDMA.&amp;nbsp; I gather that there are two ways to do this; one is to feed the external clock to the CCM and then on to the SAI as MCLK, the other is to feed the external clock to SAI MCLK once it is configured as an input.&amp;nbsp; I think the latter would be best but I would like to explore both options, although I struggle with how to do either.&amp;nbsp; Am I correct in thinking I can do this?&lt;/P&gt;&lt;P&gt;Here is a rough diagram to indicate what I hope to configure:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SAI_CONFIG.png" style="width: 866px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193976i56A62E5E4361E165/image-size/large?v=v2&amp;amp;px=999" role="button" title="SAI_CONFIG.png" alt="SAI_CONFIG.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;SAI_CONFIG.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I want RMCLK from codec to clock SAI2.&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 16 Sep 2022 15:06:41 GMT</pubDate>
    <dc:creator>mwilliams</dc:creator>
    <dc:date>2022-09-16T15:06:41Z</dc:date>
    <item>
      <title>i.mx8 audio; Using SAI as slave with external MCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8-audio-Using-SAI-as-slave-with-external-MCLK/m-p/1520632#M195037</link>
      <description>&lt;P&gt;I am looking for help to use an external clock source to drive an SAI on the i.mx8.&amp;nbsp; I need to connect the M4F core to the SAI so I need some device tree modifications.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Suppose you have an external clock source (from a codec that is the master of the I2S clocks) to be used to clock SAI2 and that the M4F core will be doing SDMA.&amp;nbsp; I gather that there are two ways to do this; one is to feed the external clock to the CCM and then on to the SAI as MCLK, the other is to feed the external clock to SAI MCLK once it is configured as an input.&amp;nbsp; I think the latter would be best but I would like to explore both options, although I struggle with how to do either.&amp;nbsp; Am I correct in thinking I can do this?&lt;/P&gt;&lt;P&gt;Here is a rough diagram to indicate what I hope to configure:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SAI_CONFIG.png" style="width: 866px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193976i56A62E5E4361E165/image-size/large?v=v2&amp;amp;px=999" role="button" title="SAI_CONFIG.png" alt="SAI_CONFIG.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;SAI_CONFIG.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I want RMCLK from codec to clock SAI2.&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Sep 2022 15:06:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8-audio-Using-SAI-as-slave-with-external-MCLK/m-p/1520632#M195037</guid>
      <dc:creator>mwilliams</dc:creator>
      <dc:date>2022-09-16T15:06:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx8 audio; Using SAI as slave with external MCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8-audio-Using-SAI-as-slave-with-external-MCLK/m-p/1521873#M195121</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Any help appreciated.. This is a useful book that may give you some pointers.&lt;/P&gt;&lt;P&gt;&lt;A href="https://douran.academy/wp-content/uploads/ebooks/linux-device-driver-development.pdf" target="_self"&gt;https://douran.academy/wp-content/uploads/ebooks/linux-device-driver-development.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Chapter 06: ALSA SoC&lt;/P&gt;&lt;P&gt;Section: Clocking and formatting considerations&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 09:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8-audio-Using-SAI-as-slave-with-external-MCLK/m-p/1521873#M195121</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2022-09-14T09:51:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx8 audio; Using SAI as slave with external MCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8-audio-Using-SAI-as-slave-with-external-MCLK/m-p/1523652#M195264</link>
      <description>&lt;P&gt;Thanks, for your reply.&amp;nbsp; I have this book but I am interested in specifically the pinmux arrangement that is necessary.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Sep 2022 13:07:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8-audio-Using-SAI-as-slave-with-external-MCLK/m-p/1523652#M195264</guid>
      <dc:creator>mwilliams</dc:creator>
      <dc:date>2022-09-16T13:07:22Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx8 audio; Using SAI as slave with external MCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8-audio-Using-SAI-as-slave-with-external-MCLK/m-p/1528747#M195676</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bit more info about the SAI in this doc&amp;nbsp; &amp;nbsp;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Also this is good:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;STRONG&gt;Section&amp;nbsp;14.1.1.1 SAI Master Clock Inputs/Outputs&amp;nbsp;&lt;/STRONG&gt;for internal clock root description in IMX8MPRM document.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Sep 2022 11:07:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8-audio-Using-SAI-as-slave-with-external-MCLK/m-p/1528747#M195676</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2022-09-27T11:07:12Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx8 audio; Using SAI as slave with external MCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8-audio-Using-SAI-as-slave-with-external-MCLK/m-p/1859765#M223334</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/92942"&gt;@edwardtyrrell&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Section&amp;nbsp;14.1.1.1 looks clear for clock configuration, but seems unclear for the software modification. would you please share example how to modify dts and other necessary files? Thanks for your reply.&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 06 May 2024 14:12:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8-audio-Using-SAI-as-slave-with-external-MCLK/m-p/1859765#M223334</guid>
      <dc:creator>zouhui</dc:creator>
      <dc:date>2024-05-06T14:12:12Z</dc:date>
    </item>
  </channel>
</rss>