<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUSB Camera Not Working on IMx8QM MEK Android</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Camera-Not-Working-on-IMx8QM-MEK-Android/m-p/1520565#M195032</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am trying to develop some Camera application in iMx8QM MEK running Android Q.&lt;/P&gt;&lt;P&gt;I am using "Logitech C270 HD WEBCAM" for my application.&lt;/P&gt;&lt;P&gt;In the MEK, I have observed that the default camera application is not working. PFA the logs&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My initial requirement is to develop a sample Android camera application that uses external USB camera as the input.&lt;/P&gt;&lt;P&gt;The app should be able to detect the USB camera as the default camera option using camera2 API.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any configuration to be done to enable USB camera in iMx8QM MEK with Android 10?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ajmal&lt;/P&gt;</description>
    <pubDate>Mon, 12 Sep 2022 13:09:21 GMT</pubDate>
    <dc:creator>ajmalmali</dc:creator>
    <dc:date>2022-09-12T13:09:21Z</dc:date>
    <item>
      <title>USB Camera Not Working on IMx8QM MEK Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Camera-Not-Working-on-IMx8QM-MEK-Android/m-p/1520565#M195032</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am trying to develop some Camera application in iMx8QM MEK running Android Q.&lt;/P&gt;&lt;P&gt;I am using "Logitech C270 HD WEBCAM" for my application.&lt;/P&gt;&lt;P&gt;In the MEK, I have observed that the default camera application is not working. PFA the logs&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My initial requirement is to develop a sample Android camera application that uses external USB camera as the input.&lt;/P&gt;&lt;P&gt;The app should be able to detect the USB camera as the default camera option using camera2 API.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any configuration to be done to enable USB camera in iMx8QM MEK with Android 10?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ajmal&lt;/P&gt;</description>
      <pubDate>Mon, 12 Sep 2022 13:09:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Camera-Not-Working-on-IMx8QM-MEK-Android/m-p/1520565#M195032</guid>
      <dc:creator>ajmalmali</dc:creator>
      <dc:date>2022-09-12T13:09:21Z</dc:date>
    </item>
    <item>
      <title>Re: USB Camera Not Working on IMx8QM MEK Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Camera-Not-Working-on-IMx8QM-MEK-Android/m-p/1525510#M195409</link>
      <description>&lt;P&gt;Have you write selinux policy for your usb camera?&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.android.com/docs/security/features/selinux/device-policy" target="_blank" rel="noopener"&gt;https://source.android.com/docs/security/features/selinux/device-policy&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://android.googlesource.com/device/lge/hammerhead/+/marshmallow-dev/sepolicy/file_contexts#21" target="_blank" rel="noopener"&gt;https://android.googlesource.com/device/lge/hammerhead/+/marshmallow-dev/sepolicy/file_contexts#21&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please provide kernel log and Android individually.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Sep 2022 05:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Camera-Not-Working-on-IMx8QM-MEK-Android/m-p/1525510#M195409</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-09-21T05:29:54Z</dc:date>
    </item>
  </channel>
</rss>