<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using GPIO intrrupt with freeRTOS on IMXRT 1052 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-GPIO-intrrupt-with-freeRTOS-on-IMXRT-1052/m-p/1520063#M194992</link>
    <description>&lt;P&gt;Hello, Im trying to generate 2 Gpios Interrupt usigning FreeRTOS!&lt;/P&gt;&lt;P&gt;i would like to know how to creater another interrupt whith the same type of interrupt that is in the project.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Using-GPIO-intrrupt-with-freeRTOS-on-IMXRT-1176/td-p/1392691" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Using-GPIO-intrrupt-with-freeRTOS-on-IMXRT-1176/td-p/1392691&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This link help me a lot with the things that i want to do but I'm getting problem when I try to add another interrupt.&lt;/P&gt;&lt;P&gt;I attached my project to allow you see my code example.&lt;/P&gt;&lt;P&gt;Thanks for all!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 09 Sep 2022 14:57:30 GMT</pubDate>
    <dc:creator>Jimmywder03</dc:creator>
    <dc:date>2022-09-09T14:57:30Z</dc:date>
    <item>
      <title>Using GPIO intrrupt with freeRTOS on IMXRT 1052</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-GPIO-intrrupt-with-freeRTOS-on-IMXRT-1052/m-p/1520063#M194992</link>
      <description>&lt;P&gt;Hello, Im trying to generate 2 Gpios Interrupt usigning FreeRTOS!&lt;/P&gt;&lt;P&gt;i would like to know how to creater another interrupt whith the same type of interrupt that is in the project.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Using-GPIO-intrrupt-with-freeRTOS-on-IMXRT-1176/td-p/1392691" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Using-GPIO-intrrupt-with-freeRTOS-on-IMXRT-1176/td-p/1392691&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This link help me a lot with the things that i want to do but I'm getting problem when I try to add another interrupt.&lt;/P&gt;&lt;P&gt;I attached my project to allow you see my code example.&lt;/P&gt;&lt;P&gt;Thanks for all!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Sep 2022 14:57:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-GPIO-intrrupt-with-freeRTOS-on-IMXRT-1052/m-p/1520063#M194992</guid>
      <dc:creator>Jimmywder03</dc:creator>
      <dc:date>2022-09-09T14:57:30Z</dc:date>
    </item>
  </channel>
</rss>