<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RTC doesn't works properly with HAL enabled in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RTC-doesn-t-works-properly-with-HAL-enabled/m-p/1520002#M194990</link>
    <description>&lt;P&gt;In addiction seems that LP_SEC_VIO and SV1 bits of HPSVSR register are high.&lt;/P&gt;</description>
    <pubDate>Fri, 09 Sep 2022 12:50:15 GMT</pubDate>
    <dc:creator>stefano6641</dc:creator>
    <dc:date>2022-09-09T12:50:15Z</dc:date>
    <item>
      <title>RTC doesn't works properly with HAL enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-doesn-t-works-properly-with-HAL-enabled/m-p/1519994#M194987</link>
      <description>&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have some problems with my iMX 1021 board with HAL enabled. The application failed to write HPRC register in SNVS bank, no error reported but data aren't set.&lt;/P&gt;&lt;P&gt;The same binary file, loaded on a bord without HAL active, works properly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some help?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;</description>
      <pubDate>Fri, 09 Sep 2022 12:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-doesn-t-works-properly-with-HAL-enabled/m-p/1519994#M194987</guid>
      <dc:creator>stefano6641</dc:creator>
      <dc:date>2022-09-09T12:28:00Z</dc:date>
    </item>
    <item>
      <title>Re: RTC doesn't works properly with HAL enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-doesn-t-works-properly-with-HAL-enabled/m-p/1520002#M194990</link>
      <description>&lt;P&gt;In addiction seems that LP_SEC_VIO and SV1 bits of HPSVSR register are high.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Sep 2022 12:50:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-doesn-t-works-properly-with-HAL-enabled/m-p/1520002#M194990</guid>
      <dc:creator>stefano6641</dc:creator>
      <dc:date>2022-09-09T12:50:15Z</dc:date>
    </item>
    <item>
      <title>Re: RTC doesn't works properly with HAL enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-doesn-t-works-properly-with-HAL-enabled/m-p/1520399#M195021</link>
      <description>&lt;P&gt;Another addiction: I can write in&amp;nbsp;HPRC register just under boot, for some time. After that I can't do it. I'm not sure which condition lock the write on&amp;nbsp;HPRC register.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;</description>
      <pubDate>Mon, 12 Sep 2022 07:54:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-doesn-t-works-properly-with-HAL-enabled/m-p/1520399#M195021</guid>
      <dc:creator>stefano6641</dc:creator>
      <dc:date>2022-09-12T07:54:00Z</dc:date>
    </item>
    <item>
      <title>Re: RTC doesn't works properly with HAL enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-doesn-t-works-properly-with-HAL-enabled/m-p/1522933#M195209</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, sorry for the later reply.&lt;/P&gt;
&lt;P&gt;I am not sure if you refer the &lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-software-development-kit-sdk:MCUXpresso-SDK" target="_self"&gt;MCUXpresso SDK&lt;/A&gt; example &amp;lt;snvs_hp_rtc&amp;gt; for RT1020?&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Thu, 15 Sep 2022 12:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-doesn-t-works-properly-with-HAL-enabled/m-p/1522933#M195209</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2022-09-15T12:45:20Z</dc:date>
    </item>
  </channel>
</rss>