<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using SCU-UART as UART Debug on Uboot and Kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-SCU-UART-as-UART-Debug-on-Uboot-and-Kernel/m-p/1519270#M194925</link>
    <description>&lt;P&gt;Hi i.MX champ&lt;/P&gt;&lt;P&gt;A customer would like to use SCU-UART as main debug port on Uboot and Kernel debug.&lt;/P&gt;&lt;P&gt;Can you please let us know if SCU-UART can be used for a UART Debug Port on Uboot and Kernel log message in addition to earlier bring up message from SCFW.&lt;/P&gt;&lt;P&gt;This is asked since 4x UART ports need to be used for extenel device control interface.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jack&lt;/P&gt;</description>
    <pubDate>Thu, 08 Sep 2022 10:42:45 GMT</pubDate>
    <dc:creator>JK-IMX</dc:creator>
    <dc:date>2022-09-08T10:42:45Z</dc:date>
    <item>
      <title>Using SCU-UART as UART Debug on Uboot and Kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-SCU-UART-as-UART-Debug-on-Uboot-and-Kernel/m-p/1519270#M194925</link>
      <description>&lt;P&gt;Hi i.MX champ&lt;/P&gt;&lt;P&gt;A customer would like to use SCU-UART as main debug port on Uboot and Kernel debug.&lt;/P&gt;&lt;P&gt;Can you please let us know if SCU-UART can be used for a UART Debug Port on Uboot and Kernel log message in addition to earlier bring up message from SCFW.&lt;/P&gt;&lt;P&gt;This is asked since 4x UART ports need to be used for extenel device control interface.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jack&lt;/P&gt;</description>
      <pubDate>Thu, 08 Sep 2022 10:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-SCU-UART-as-UART-Debug-on-Uboot-and-Kernel/m-p/1519270#M194925</guid>
      <dc:creator>JK-IMX</dc:creator>
      <dc:date>2022-09-08T10:42:45Z</dc:date>
    </item>
    <item>
      <title>Re: Using SCU-UART as UART Debug on Uboot and Kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-SCU-UART-as-UART-Debug-on-Uboot-and-Kernel/m-p/1522843#M195196</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191000"&gt;@JK-IMX&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to the following links,&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Use-UART0-RX-TX-as-SCU-UART-debug-port-on-iMX8QXP-boards/ta-p/1119371" target="_self"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Use-UART0-RX-TX-as-SCU-UART-debug-port-on-iMX8QXP-boards/ta-p/1119371&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Pad-configuration-service/ta-p/1124213" target="_self"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Pad-configuration-service/ta-p/1124213&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Dhruvit.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Sep 2022 10:05:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-SCU-UART-as-UART-Debug-on-Uboot-and-Kernel/m-p/1522843#M195196</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2022-09-15T10:05:39Z</dc:date>
    </item>
  </channel>
</rss>