<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX8MM: LCDIF maximum possible resolution</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MM-LCDIF-maximum-possible-resolution/m-p/1517648#M194793</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to connect a MIPI-DSI display to my Toradex Verdin iMX8MM module and I am not sure which maximum resolution is possible with this SoC.&lt;/P&gt;&lt;P&gt;The &lt;A href="https://www.nxp.com/docs/en/data-sheet/IMX8MMIEC.pdf" target="_self"&gt;datasheet&lt;/A&gt; of the iMX8MM (Rev. 1, 07/2020) says on page 3 that the LCDIF does support up to 1080p60. But the &lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MMRM" target="_self"&gt;reference manual&lt;/A&gt; (Rev. 3, 11/2020) indicates in section 1.4.11, 13.1.1.1 and 13.5.2 that the LCDIF und the MIPI-DSI supports up to 1200p60.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Which one is the right number? I suppose that the reference manuel is correct since the MIPI DSI maximum resolution support was changed from revision 2 to revision 3 (section A.1.1).&lt;/P&gt;&lt;P&gt;Can someone confirm this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;</description>
    <pubDate>Tue, 06 Sep 2022 10:17:53 GMT</pubDate>
    <dc:creator>Mowlwurf</dc:creator>
    <dc:date>2022-09-06T10:17:53Z</dc:date>
    <item>
      <title>iMX8MM: LCDIF maximum possible resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MM-LCDIF-maximum-possible-resolution/m-p/1517648#M194793</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to connect a MIPI-DSI display to my Toradex Verdin iMX8MM module and I am not sure which maximum resolution is possible with this SoC.&lt;/P&gt;&lt;P&gt;The &lt;A href="https://www.nxp.com/docs/en/data-sheet/IMX8MMIEC.pdf" target="_self"&gt;datasheet&lt;/A&gt; of the iMX8MM (Rev. 1, 07/2020) says on page 3 that the LCDIF does support up to 1080p60. But the &lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MMRM" target="_self"&gt;reference manual&lt;/A&gt; (Rev. 3, 11/2020) indicates in section 1.4.11, 13.1.1.1 and 13.5.2 that the LCDIF und the MIPI-DSI supports up to 1200p60.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Which one is the right number? I suppose that the reference manuel is correct since the MIPI DSI maximum resolution support was changed from revision 2 to revision 3 (section A.1.1).&lt;/P&gt;&lt;P&gt;Can someone confirm this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;</description>
      <pubDate>Tue, 06 Sep 2022 10:17:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MM-LCDIF-maximum-possible-resolution/m-p/1517648#M194793</guid>
      <dc:creator>Mowlwurf</dc:creator>
      <dc:date>2022-09-06T10:17:53Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MM: LCDIF maximum possible resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MM-LCDIF-maximum-possible-resolution/m-p/1522711#M195188</link>
      <description>&lt;P&gt;I got the following response from a NXP employee:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;You are right, the reference manual is ok.&lt;BR /&gt;&lt;BR /&gt;If you have questions about this topic, you can find in the&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13573.pdf" target="_blank" rel="noopener"&gt;AN13573&lt;/A&gt; (&lt;A href="https://i.MX" target="_blank" rel="noopener"&gt;i.MX&lt;/A&gt; 8/RT MIPI DSI/CSI-2), in the chapter 3.2.1.1 (Pixel clock and resolution relationship) is explained the resolution and frame rate.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Markus&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Sep 2022 08:17:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MM-LCDIF-maximum-possible-resolution/m-p/1522711#M195188</guid>
      <dc:creator>Mowlwurf</dc:creator>
      <dc:date>2022-09-15T08:17:43Z</dc:date>
    </item>
  </channel>
</rss>