<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8QXP boot logo in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-boot-logo/m-p/1517056#M194733</link>
    <description>&lt;P&gt;We need display output as fast as possible so using the kernel logo feature is not quick enough. I got it now as far as having a valid dual channel LVDS output in uboot by patching imx8_lvds.c with support for the an aux ldb as it is done in the kernel. We tried to follow the path of what is done when&amp;nbsp;&lt;SPAN&gt;fsl,dual-channel; is set in the kernel device tree.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;But now we see a stretched image (only left half of uboot splashscreen is visible). Do you have any hint what can be done to fix this behavior?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Mon, 05 Sep 2022 12:30:18 GMT</pubDate>
    <dc:creator>mod42</dc:creator>
    <dc:date>2022-09-05T12:30:18Z</dc:date>
    <item>
      <title>i.MX8QXP boot logo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-boot-logo/m-p/1401780#M186013</link>
      <description>&lt;P&gt;We have a custom board with a display connected over LVDS to an iMX8QXP. When u-boot starts we show a logo bitmap from eMMC. After u-boot has loaded the kernel the display is switched of and comes back when weston is started. This causes the display to be black for a couple of seconds which is anything but nice. Is there any solution to this problem? We use our own BSP heavily based on the latest release&amp;nbsp;5.10.72_2.2.0.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jan 2022 14:16:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-boot-logo/m-p/1401780#M186013</guid>
      <dc:creator>mod42</dc:creator>
      <dc:date>2022-01-19T14:16:54Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP boot logo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-boot-logo/m-p/1409916#M186715</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can custom your kernel logo during this black display.&lt;/P&gt;
&lt;P&gt;Useful link: &lt;A href="https://developer.toradex.com/knowledge-base/splash-screen-linux" target="_blank"&gt;https://developer.toradex.com/knowledge-base/splash-screen-linux&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Feb 2022 02:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-boot-logo/m-p/1409916#M186715</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-02-08T02:15:32Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP boot logo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-boot-logo/m-p/1409920#M186716</link>
      <description>&lt;P&gt;yes&lt;/P&gt;</description>
      <pubDate>Tue, 08 Feb 2022 02:28:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-boot-logo/m-p/1409920#M186716</guid>
      <dc:creator>josephzhou1</dc:creator>
      <dc:date>2022-02-08T02:28:35Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP boot logo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-boot-logo/m-p/1517056#M194733</link>
      <description>&lt;P&gt;We need display output as fast as possible so using the kernel logo feature is not quick enough. I got it now as far as having a valid dual channel LVDS output in uboot by patching imx8_lvds.c with support for the an aux ldb as it is done in the kernel. We tried to follow the path of what is done when&amp;nbsp;&lt;SPAN&gt;fsl,dual-channel; is set in the kernel device tree.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;But now we see a stretched image (only left half of uboot splashscreen is visible). Do you have any hint what can be done to fix this behavior?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 05 Sep 2022 12:30:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-boot-logo/m-p/1517056#M194733</guid>
      <dc:creator>mod42</dc:creator>
      <dc:date>2022-09-05T12:30:18Z</dc:date>
    </item>
  </channel>
</rss>