<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic problems about &amp;quot;Building and Running CHIP Linux Examples for i.MX 8M Mini EVK&amp;quot; in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/problems-about-quot-Building-and-Running-CHIP-Linux-Examples-for/m-p/1516954#M194718</link>
    <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I am studying "Building and Running CHIP Linux Examples for i.MX 8M Mini EVK"&lt;BR /&gt;(which the document is in github &lt;A href="https://github.com/project-chip/connectedhomeip/blob/4cdecc94488f2c89e8bb9d90637b" target="_blank"&gt;https://github.com/project-chip/connectedhomeip/blob/4cdecc94488f2c89e8bb9d90637b&lt;/A&gt;&lt;BR /&gt;0eea97bb919a/docs/guides/nxp_imx8m_linux_examples.md#running-the-examples-on-imx-8m-mini-evk)&lt;/P&gt;&lt;P&gt;and I meet some problems.&lt;/P&gt;&lt;P&gt;I finished all the steps before the subtitle "Build the example application" .&lt;BR /&gt;In subtitle "Build the example application" ,it describes there are two files named build_example.py and imxlinux_example.sh,&lt;BR /&gt;but I can not find these two files. Also I can not find the file "scripts/activate.sh".&lt;/P&gt;&lt;P&gt;I saw there is a statemet as "Assuming that the working directory is changed to the top level directory of this project",&lt;BR /&gt;is the directory means "xwayland"?&lt;/P&gt;&lt;P&gt;Also, do I need to input the command "git submodule update --init"? What does this command mean?&lt;/P&gt;&lt;P&gt;Thank you for replying&lt;/P&gt;&lt;P&gt;Best Regaeds&lt;/P&gt;</description>
    <pubDate>Mon, 05 Sep 2022 09:58:34 GMT</pubDate>
    <dc:creator>MikeYJ</dc:creator>
    <dc:date>2022-09-05T09:58:34Z</dc:date>
    <item>
      <title>problems about "Building and Running CHIP Linux Examples for i.MX 8M Mini EVK"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problems-about-quot-Building-and-Running-CHIP-Linux-Examples-for/m-p/1516954#M194718</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I am studying "Building and Running CHIP Linux Examples for i.MX 8M Mini EVK"&lt;BR /&gt;(which the document is in github &lt;A href="https://github.com/project-chip/connectedhomeip/blob/4cdecc94488f2c89e8bb9d90637b" target="_blank"&gt;https://github.com/project-chip/connectedhomeip/blob/4cdecc94488f2c89e8bb9d90637b&lt;/A&gt;&lt;BR /&gt;0eea97bb919a/docs/guides/nxp_imx8m_linux_examples.md#running-the-examples-on-imx-8m-mini-evk)&lt;/P&gt;&lt;P&gt;and I meet some problems.&lt;/P&gt;&lt;P&gt;I finished all the steps before the subtitle "Build the example application" .&lt;BR /&gt;In subtitle "Build the example application" ,it describes there are two files named build_example.py and imxlinux_example.sh,&lt;BR /&gt;but I can not find these two files. Also I can not find the file "scripts/activate.sh".&lt;/P&gt;&lt;P&gt;I saw there is a statemet as "Assuming that the working directory is changed to the top level directory of this project",&lt;BR /&gt;is the directory means "xwayland"?&lt;/P&gt;&lt;P&gt;Also, do I need to input the command "git submodule update --init"? What does this command mean?&lt;/P&gt;&lt;P&gt;Thank you for replying&lt;/P&gt;&lt;P&gt;Best Regaeds&lt;/P&gt;</description>
      <pubDate>Mon, 05 Sep 2022 09:58:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problems-about-quot-Building-and-Running-CHIP-Linux-Examples-for/m-p/1516954#M194718</guid>
      <dc:creator>MikeYJ</dc:creator>
      <dc:date>2022-09-05T09:58:34Z</dc:date>
    </item>
    <item>
      <title>Re: problems about "Building and Running CHIP Linux Examples for i.MX 8M Mini EVK"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problems-about-quot-Building-and-Running-CHIP-Linux-Examples-for/m-p/1523031#M195226</link>
      <description>&lt;P&gt;build_example.py is in &lt;A href="https://github.com/project-chip/connectedhomeip/tree/4cdecc94488f2c89e8bb9d90637b0eea97bb919a/scripts/build" target="_self"&gt;here&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;imxlinux_example.sh is in &lt;A href="https://github.com/project-chip/connectedhomeip/tree/4cdecc94488f2c89e8bb9d90637b0eea97bb919a/scripts/examples" target="_self"&gt;here&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;activate.sh is in &lt;A href="https://github.com/project-chip/connectedhomeip/tree/4cdecc94488f2c89e8bb9d90637b0eea97bb919a/scripts" target="_self"&gt;here&lt;/A&gt;.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Sep 2022 15:34:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problems-about-quot-Building-and-Running-CHIP-Linux-Examples-for/m-p/1523031#M195226</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-09-15T15:34:36Z</dc:date>
    </item>
  </channel>
</rss>