<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6ULL DDR IO pad reassignment in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-DDR-IO-pad-reassignment/m-p/1514765#M194549</link>
    <description>&lt;P&gt;Should be OK thanks&lt;/P&gt;</description>
    <pubDate>Wed, 31 Aug 2022 16:09:54 GMT</pubDate>
    <dc:creator>mobileoverlord</dc:creator>
    <dc:date>2022-08-31T16:09:54Z</dc:date>
    <item>
      <title>iMX6ULL DDR IO pad reassignment</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-DDR-IO-pad-reassignment/m-p/1502840#M193595</link>
      <description>&lt;P&gt;According to the &lt;A href="https://www.nxp.com/files-static/soft_dev_tools/doc/user_guide/IMX6ULLHDG.pdf?&amp;amp;fasp=1&amp;amp;WT_TYPE=Users%20Guides&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" target="_self"&gt;Hardware design guide&lt;/A&gt;&amp;nbsp;Section 3.5.1 discusses data line swapping for the DDR routing configuration. It has the following note:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN&gt;If the byte lane swapping was done, the target DDR IC register read value must be transposed according to the data line swapping.&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The &lt;A href="https://www.nxp.com/webapp-signup/updateUser?userType=EXTENDED&amp;amp;mandatory=YES&amp;amp;TARGETURL=webapp%2FDownload%3FcolCode%3DIMX6ULLRM" target="_self"&gt;Hardware reference&lt;/A&gt;&amp;nbsp;IO pin max configuration section 4.1.1 describes the MMDC DATA* pins are muxed to their corresponding pads with No Mixing (ALT0). I am under the impression that I need to remap this pin to pad mux to reflect the four data line swaps that were made in the custom layout I am working with. In my layout D1 &amp;amp; D4 are swapped and D2 &amp;amp; D7 are swapped. Please advise what changes need to be reflected in the registers. Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 00:17:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-DDR-IO-pad-reassignment/m-p/1502840#M193595</guid>
      <dc:creator>mobileoverlord</dc:creator>
      <dc:date>2022-08-09T00:17:26Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ULL DDR IO pad reassignment</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-DDR-IO-pad-reassignment/m-p/1502847#M193596</link>
      <description>&lt;P&gt;sorry, I think I misunderstood the requirements. I believe I only need to ensure the pad configuration is set for all DDR data pins in use. The bit swapping will “just work”&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 00:58:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-DDR-IO-pad-reassignment/m-p/1502847#M193596</guid>
      <dc:creator>mobileoverlord</dc:creator>
      <dc:date>2022-08-09T00:58:19Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ULL DDR IO pad reassignment</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-DDR-IO-pad-reassignment/m-p/1514715#M194546</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204787"&gt;@mobileoverlord&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;I think your issue is resolved. Can i mark this ticket to close state?&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;
&lt;P&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 14:49:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-DDR-IO-pad-reassignment/m-p/1514715#M194546</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2022-08-31T14:49:00Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ULL DDR IO pad reassignment</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-DDR-IO-pad-reassignment/m-p/1514765#M194549</link>
      <description>&lt;P&gt;Should be OK thanks&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 16:09:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-DDR-IO-pad-reassignment/m-p/1514765#M194549</guid>
      <dc:creator>mobileoverlord</dc:creator>
      <dc:date>2022-08-31T16:09:54Z</dc:date>
    </item>
  </channel>
</rss>