<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8m Plus Boundary Scan Issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8m-Plus-Boundary-Scan-Issue/m-p/1514704#M194543</link>
    <description>&lt;P&gt;I'm building a custom board using IMX8m Plus, and I want to use boundary scan to test the connections of the board. In order to do so, I am experimenting on the (8MPLUSLPD4-EVK) to check the JTAG connections and what need to be done to enter Boundary Scan Mode. I removed R32 (JTAG_MOD connection to GND) and soldered R313 2.2KOhm (JTAG_MOD to VDD_1V8). In addition, in SW4 I changed all the BOOT_MODE status to High, and I Measured the Voltage of POR and it is high. When I tried to check the chain to start the test, the Power LED (D25) turns off and when I disconnect XJLINK it goes back ON. The message I got from XJLINK2:&lt;/P&gt;&lt;P&gt;Starting Check Chain ...&lt;/P&gt;&lt;P&gt;No valid data returned from the JTAG chain.&lt;/P&gt;&lt;P&gt;perhaps the pin map is incorrect, or the board is not powered.&lt;/P&gt;&lt;P&gt;Check chain failed&lt;/P&gt;&lt;P&gt;Any idea what seems to be the problem?&lt;/P&gt;</description>
    <pubDate>Wed, 31 Aug 2022 14:36:03 GMT</pubDate>
    <dc:creator>Talal</dc:creator>
    <dc:date>2022-08-31T14:36:03Z</dc:date>
    <item>
      <title>IMX8m Plus Boundary Scan Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8m-Plus-Boundary-Scan-Issue/m-p/1514704#M194543</link>
      <description>&lt;P&gt;I'm building a custom board using IMX8m Plus, and I want to use boundary scan to test the connections of the board. In order to do so, I am experimenting on the (8MPLUSLPD4-EVK) to check the JTAG connections and what need to be done to enter Boundary Scan Mode. I removed R32 (JTAG_MOD connection to GND) and soldered R313 2.2KOhm (JTAG_MOD to VDD_1V8). In addition, in SW4 I changed all the BOOT_MODE status to High, and I Measured the Voltage of POR and it is high. When I tried to check the chain to start the test, the Power LED (D25) turns off and when I disconnect XJLINK it goes back ON. The message I got from XJLINK2:&lt;/P&gt;&lt;P&gt;Starting Check Chain ...&lt;/P&gt;&lt;P&gt;No valid data returned from the JTAG chain.&lt;/P&gt;&lt;P&gt;perhaps the pin map is incorrect, or the board is not powered.&lt;/P&gt;&lt;P&gt;Check chain failed&lt;/P&gt;&lt;P&gt;Any idea what seems to be the problem?&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 14:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8m-Plus-Boundary-Scan-Issue/m-p/1514704#M194543</guid>
      <dc:creator>Talal</dc:creator>
      <dc:date>2022-08-31T14:36:03Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8m Plus Boundary Scan Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8m-Plus-Boundary-Scan-Issue/m-p/1519705#M194957</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203820"&gt;@Talal&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please accept my apologies for delay in response.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;One can refer&amp;nbsp;&lt;STRONG&gt;Example 3: No Valid Data Returned&lt;/STRONG&gt; from the below link to know the possible causes of the error:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.xjtag.com/support/application-notes/jtag-chain-debugging/" target="_blank"&gt;https://www.xjtag.com/support/application-notes/jtag-chain-debugging/&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In addition to the above, could you please also check what is the status of JTAG reset pin?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Ritesh M Patel&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Sep 2022 03:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8m-Plus-Boundary-Scan-Issue/m-p/1519705#M194957</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2022-09-09T03:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8m Plus Boundary Scan Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8m-Plus-Boundary-Scan-Issue/m-p/1520247#M195009</link>
      <description>&lt;P&gt;Thank you so much for your help Ritesh, the issue was with the test reset sequence, nRST was low and the PMIC reset pin is active low. I just changed the nRST state to high and it worked fine!&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Sun, 11 Sep 2022 08:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8m-Plus-Boundary-Scan-Issue/m-p/1520247#M195009</guid>
      <dc:creator>Talal</dc:creator>
      <dc:date>2022-09-11T08:35:55Z</dc:date>
    </item>
  </channel>
</rss>