<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMCIMX7SABRE Camera Module Specifications and HDMI Support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX7SABRE-Camera-Module-Specifications-and-HDMI-Support/m-p/1514576#M194530</link>
    <description>&lt;P&gt;Hallo,&lt;BR /&gt;&lt;BR /&gt;I want to use&amp;nbsp;MCIMX7SABRE for testing MiPi cable using image sensor having capabilities of 8MP or higher(4K resolution). I have read the 'Quick Start Guide SABRE Board for Smart Devices' and it mentions we can use OV5640 but this is a 5MP camera.&lt;BR /&gt;&lt;BR /&gt;Q) Do we have a sensor module with 8MP or higher (with free running clock output) that we can use with the&amp;nbsp;MCIMX7SABRE?&lt;BR /&gt;Q) Does the HDMI port support HDMI2.0 or higher?&lt;BR /&gt;&lt;BR /&gt;I am really looking forward for the answers. Thanks in advance.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Ubaid Ahmed Shafi&lt;BR /&gt;Munich, Germany&lt;/P&gt;</description>
    <pubDate>Wed, 31 Aug 2022 10:35:39 GMT</pubDate>
    <dc:creator>UbaidShafi</dc:creator>
    <dc:date>2022-08-31T10:35:39Z</dc:date>
    <item>
      <title>MCIMX7SABRE Camera Module Specifications and HDMI Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX7SABRE-Camera-Module-Specifications-and-HDMI-Support/m-p/1514576#M194530</link>
      <description>&lt;P&gt;Hallo,&lt;BR /&gt;&lt;BR /&gt;I want to use&amp;nbsp;MCIMX7SABRE for testing MiPi cable using image sensor having capabilities of 8MP or higher(4K resolution). I have read the 'Quick Start Guide SABRE Board for Smart Devices' and it mentions we can use OV5640 but this is a 5MP camera.&lt;BR /&gt;&lt;BR /&gt;Q) Do we have a sensor module with 8MP or higher (with free running clock output) that we can use with the&amp;nbsp;MCIMX7SABRE?&lt;BR /&gt;Q) Does the HDMI port support HDMI2.0 or higher?&lt;BR /&gt;&lt;BR /&gt;I am really looking forward for the answers. Thanks in advance.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Ubaid Ahmed Shafi&lt;BR /&gt;Munich, Germany&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 10:35:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX7SABRE-Camera-Module-Specifications-and-HDMI-Support/m-p/1514576#M194530</guid>
      <dc:creator>UbaidShafi</dc:creator>
      <dc:date>2022-08-31T10:35:39Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX7SABRE Camera Module Specifications and HDMI Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX7SABRE-Camera-Module-Specifications-and-HDMI-Support/m-p/1517367#M194763</link>
      <description>&lt;P&gt;Q) Do we have a sensor module with 8MP or higher (with free running clock output) that we can use with the MCIMX7SABRE?&lt;/P&gt;
&lt;P&gt;&amp;gt;refer to the imx7d reference manual,&lt;/P&gt;
&lt;P&gt;MIPI CSI-2 controller and D-PHY:&lt;BR /&gt;• Supports 2 data lanes and 1 clock lane&lt;BR /&gt;• Maximum bit rate of 1.5 Gbps&lt;/P&gt;
&lt;P&gt;so if you need 8MP camera, only can support 15fps max, you can check if your camera can meet this&lt;/P&gt;
&lt;P&gt;Q) Does the HDMI port support HDMI2.0 or higher?&lt;/P&gt;
&lt;P&gt;&amp;gt; current imx7d sabresd board uses SiI9022ACNU convert, I checked this chip which doesn't support HDMI 2.0, but you can use other convert chip to support this&lt;/P&gt;</description>
      <pubDate>Tue, 06 Sep 2022 04:39:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX7SABRE-Camera-Module-Specifications-and-HDMI-Support/m-p/1517367#M194763</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-09-06T04:39:29Z</dc:date>
    </item>
  </channel>
</rss>