<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Specifying J-Link Script location issues</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Specifying-J-Link-Script-location-issues/m-p/1514293#M194486</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/71022"&gt;@rshipman&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; To the JLINK script add to the MCUXPresso IDE, normally, we need to add it to the Debug configuration:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1661916218651.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191914i3F4922442B23796C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1661916218651.png" alt="kerryzhou_0-1661916218651.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If it is your own .jlinkscript, you can manually add it, we also manually add it.&lt;/P&gt;
&lt;P&gt;No other automatic method now.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 31 Aug 2022 03:24:44 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2022-08-31T03:24:44Z</dc:date>
    <item>
      <title>Specifying J-Link Script location issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Specifying-J-Link-Script-location-issues/m-p/1514067#M194473</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using a SEGGER J-Link debugger to debug a target board based on the RT1021-EVK.&lt;/P&gt;&lt;P&gt;I have created a J-Link script which seems to work well enough.&lt;/P&gt;&lt;P&gt;In the JLink Launch Configuration, in the JLink debugger tab, there is a Script field that is empty by default. So every time I recreate the launch file, I need to edit this field. Also the JLink Debugger does not look in the local directory for the file I enter.&lt;/P&gt;&lt;P&gt;There seems to be only two ways to pass a J-Link script to the J-Link debugger.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Put the script here: C:\Program Files\SEGGER\JLink\Default.JLinkScript&lt;/LI&gt;&lt;LI&gt;Or, put the script where you like and fill in the 'Script' field in the JLink Debugger tab in the JLink Launch Configuration.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Both of these methods are not very satisfactory to us.&lt;/P&gt;&lt;P&gt;In the LinkServer Launch Configuration, in the LinkServer debugger, there is a Connect script field. The script file name is automatically populated as RT1020_connect.scp. So I never need to edit it. Not only that, the LinkServer looks for this file in the project's local folder, before looking for the script in the nxp installation folders.&lt;/P&gt;&lt;P&gt;So, is there a way to automatically put a default entry in this Script field? I don't want to have to edit the Launch Configuration each time I create the launch file.&lt;/P&gt;&lt;P&gt;And is there a way to make it look in the project's local folder in the same way as the LinkServer one?&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Ronnie Shipman&lt;/P&gt;</description>
      <pubDate>Tue, 30 Aug 2022 16:53:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Specifying-J-Link-Script-location-issues/m-p/1514067#M194473</guid>
      <dc:creator>rshipman</dc:creator>
      <dc:date>2022-08-30T16:53:22Z</dc:date>
    </item>
    <item>
      <title>Re: Specifying J-Link Script location issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Specifying-J-Link-Script-location-issues/m-p/1514293#M194486</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/71022"&gt;@rshipman&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; To the JLINK script add to the MCUXPresso IDE, normally, we need to add it to the Debug configuration:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1661916218651.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191914i3F4922442B23796C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1661916218651.png" alt="kerryzhou_0-1661916218651.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If it is your own .jlinkscript, you can manually add it, we also manually add it.&lt;/P&gt;
&lt;P&gt;No other automatic method now.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 03:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Specifying-J-Link-Script-location-issues/m-p/1514293#M194486</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2022-08-31T03:24:44Z</dc:date>
    </item>
  </channel>
</rss>