<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx6SoloX: internal reset issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6SoloX-internal-reset-issue/m-p/1514057#M194472</link>
    <description>&lt;P&gt;I noticed few issues regarding internal reset on imx6Solox:&lt;/P&gt;&lt;P&gt;Linux kernel is used. The imx2_wdt driver well writes WDE and WDA bits in WDT_WCR register to trigger internal reset signal and reboot MPU.&lt;/P&gt;&lt;P&gt;But on few products (9 for now), it sometimes doesn't reset at all.&lt;/P&gt;&lt;P&gt;I currently have access to 2 products reproducing continuously this issue between 10 and 500 reboots.&lt;/P&gt;&lt;P&gt;The most mysterious behavior is that Watchdog timer is started but doesn't trig reset neither. (I thought it was impossible to disable watchdog once started).&lt;/P&gt;&lt;P&gt;However, an "HW reset" (glitch on POR_B) seems to solve this issue. But this is not acceptable for our customers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I saw that SoloX Sabre Reference design includes this note:&lt;/P&gt;&lt;P&gt;“Fix the SW reboot issue by togling WDOG_B to issue power reset (ENGR00338067).”&lt;/P&gt;&lt;P&gt;This issue doesn't seem to be referenced by any errata nor documentation excepting&amp;nbsp;AN5161.&lt;/P&gt;&lt;P&gt;But we don't use PMIC on our various designs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you explain what is this issue ?&lt;/P&gt;&lt;P&gt;Is this "SW reboot issue" is still present in last silicon version of SoloX ?&lt;/P&gt;&lt;P&gt;Is it also present in imx6ULL and imx8 family ?&lt;/P&gt;&lt;P&gt;Do you have any software workaround / recommandations ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 30 Aug 2022 16:24:13 GMT</pubDate>
    <dc:creator>mchaplet</dc:creator>
    <dc:date>2022-08-30T16:24:13Z</dc:date>
    <item>
      <title>imx6SoloX: internal reset issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6SoloX-internal-reset-issue/m-p/1514057#M194472</link>
      <description>&lt;P&gt;I noticed few issues regarding internal reset on imx6Solox:&lt;/P&gt;&lt;P&gt;Linux kernel is used. The imx2_wdt driver well writes WDE and WDA bits in WDT_WCR register to trigger internal reset signal and reboot MPU.&lt;/P&gt;&lt;P&gt;But on few products (9 for now), it sometimes doesn't reset at all.&lt;/P&gt;&lt;P&gt;I currently have access to 2 products reproducing continuously this issue between 10 and 500 reboots.&lt;/P&gt;&lt;P&gt;The most mysterious behavior is that Watchdog timer is started but doesn't trig reset neither. (I thought it was impossible to disable watchdog once started).&lt;/P&gt;&lt;P&gt;However, an "HW reset" (glitch on POR_B) seems to solve this issue. But this is not acceptable for our customers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I saw that SoloX Sabre Reference design includes this note:&lt;/P&gt;&lt;P&gt;“Fix the SW reboot issue by togling WDOG_B to issue power reset (ENGR00338067).”&lt;/P&gt;&lt;P&gt;This issue doesn't seem to be referenced by any errata nor documentation excepting&amp;nbsp;AN5161.&lt;/P&gt;&lt;P&gt;But we don't use PMIC on our various designs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you explain what is this issue ?&lt;/P&gt;&lt;P&gt;Is this "SW reboot issue" is still present in last silicon version of SoloX ?&lt;/P&gt;&lt;P&gt;Is it also present in imx6ULL and imx8 family ?&lt;/P&gt;&lt;P&gt;Do you have any software workaround / recommandations ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Aug 2022 16:24:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6SoloX-internal-reset-issue/m-p/1514057#M194472</guid>
      <dc:creator>mchaplet</dc:creator>
      <dc:date>2022-08-30T16:24:13Z</dc:date>
    </item>
    <item>
      <title>Re: imx6SoloX: internal reset issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6SoloX-internal-reset-issue/m-p/1518486#M194869</link>
      <description>&lt;P&gt;After few tests, I can confirm that the same Freeze issue happens also with WDOG3 and TemperatureSensor as reset sources.&lt;BR /&gt;&lt;BR /&gt;To be clear, our current conclusion is that:&lt;BR /&gt;&lt;BR /&gt;ALL internal reset sources are unreliable !&lt;BR /&gt;&lt;BR /&gt;Can you confirm ?&lt;BR /&gt;Is there a way to simulate reset from software in Linux environment ? (something like loading Romboot and jumping to it ?)&lt;/P&gt;</description>
      <pubDate>Wed, 07 Sep 2022 11:29:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6SoloX-internal-reset-issue/m-p/1518486#M194869</guid>
      <dc:creator>mchaplet</dc:creator>
      <dc:date>2022-09-07T11:29:18Z</dc:date>
    </item>
  </channel>
</rss>