<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CPU is getting hang while using 3 RS485 port in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CPU-is-getting-hang-while-using-3-RS485-port/m-p/1512378#M194327</link>
    <description>&lt;P&gt;CPU is getting hang while running the application with 3 RS485 port.&lt;/P&gt;&lt;P&gt;Imx8 with linux&amp;nbsp;5.4.181+ is being used and CPU is getting stuck.&lt;/P&gt;&lt;P&gt;Please help me to resolve this issue.&lt;/P&gt;&lt;P&gt;Getting below the kernel logs :&amp;nbsp;&lt;/P&gt;&lt;P&gt;watchdog: BUG: soft lockup - CPU#0 stuck for 22s!&lt;BR /&gt;[ 1444.538575] rcu: INFO: rcu_preempt self-detected stall on CPU&lt;BR /&gt;[ 1444.544327] rcu: 0-....: (5248 ticks this GP) idle=8d6/1/0x4000000000000004 softirq=478534/478534 fqs=2601&lt;BR /&gt;[ 1472.006575] watchdog: BUG: soft lockup - CPU#0 stuck for 22s!&lt;BR /&gt;[ 1507.550574] rcu: INFO: rcu_preempt self-detected stall on CPU&lt;BR /&gt;[ 1507.556325] rcu: 0-....: (20998 ticks this GP) idle=8d6/1/0x4000000000000004 softirq=478534/478534 fqs=10386&lt;BR /&gt;[ 1532.006574] watchdog: BUG: soft lockup - CPU#0 stuck for 22s!&lt;BR /&gt;[ 1570.562574] rcu: INFO: rcu_preempt self-detected stall on CPU&lt;BR /&gt;[ 1570.568324] rcu: 0-....: (36748 ticks this GP) idle=8d6/1/0x4000000000000004 softirq=478534/478534 fqs=18170&lt;BR /&gt;[ 1571.810625] INFO: task jbd2/dm-0-8:375 blocked for more than 120 seconds.&lt;BR /&gt;[ 1571.817422] Tainted: G O L 5.4.181+ #1&lt;BR /&gt;[ 1571.822827] "echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message.&lt;/P&gt;</description>
    <pubDate>Fri, 26 Aug 2022 12:59:12 GMT</pubDate>
    <dc:creator>pankajsolanki555</dc:creator>
    <dc:date>2022-08-26T12:59:12Z</dc:date>
    <item>
      <title>CPU is getting hang while using 3 RS485 port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU-is-getting-hang-while-using-3-RS485-port/m-p/1512378#M194327</link>
      <description>&lt;P&gt;CPU is getting hang while running the application with 3 RS485 port.&lt;/P&gt;&lt;P&gt;Imx8 with linux&amp;nbsp;5.4.181+ is being used and CPU is getting stuck.&lt;/P&gt;&lt;P&gt;Please help me to resolve this issue.&lt;/P&gt;&lt;P&gt;Getting below the kernel logs :&amp;nbsp;&lt;/P&gt;&lt;P&gt;watchdog: BUG: soft lockup - CPU#0 stuck for 22s!&lt;BR /&gt;[ 1444.538575] rcu: INFO: rcu_preempt self-detected stall on CPU&lt;BR /&gt;[ 1444.544327] rcu: 0-....: (5248 ticks this GP) idle=8d6/1/0x4000000000000004 softirq=478534/478534 fqs=2601&lt;BR /&gt;[ 1472.006575] watchdog: BUG: soft lockup - CPU#0 stuck for 22s!&lt;BR /&gt;[ 1507.550574] rcu: INFO: rcu_preempt self-detected stall on CPU&lt;BR /&gt;[ 1507.556325] rcu: 0-....: (20998 ticks this GP) idle=8d6/1/0x4000000000000004 softirq=478534/478534 fqs=10386&lt;BR /&gt;[ 1532.006574] watchdog: BUG: soft lockup - CPU#0 stuck for 22s!&lt;BR /&gt;[ 1570.562574] rcu: INFO: rcu_preempt self-detected stall on CPU&lt;BR /&gt;[ 1570.568324] rcu: 0-....: (36748 ticks this GP) idle=8d6/1/0x4000000000000004 softirq=478534/478534 fqs=18170&lt;BR /&gt;[ 1571.810625] INFO: task jbd2/dm-0-8:375 blocked for more than 120 seconds.&lt;BR /&gt;[ 1571.817422] Tainted: G O L 5.4.181+ #1&lt;BR /&gt;[ 1571.822827] "echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Aug 2022 12:59:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU-is-getting-hang-while-using-3-RS485-port/m-p/1512378#M194327</guid>
      <dc:creator>pankajsolanki555</dc:creator>
      <dc:date>2022-08-26T12:59:12Z</dc:date>
    </item>
  </channel>
</rss>