<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flash stuck in &amp;quot;No device connected&amp;quot; when using mfgtool in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Flash-stuck-in-quot-No-device-connected-quot-when-using-mfgtool/m-p/1511286#M194243</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Please help me providing the following information:&lt;BR /&gt;MFGTool version that you are using for flashing&lt;BR /&gt;Uboot version&lt;BR /&gt;Kernel version&lt;BR /&gt;Prebuilt image from NXP webpage or your own built image&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Wed, 24 Aug 2022 22:31:08 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2022-08-24T22:31:08Z</dc:date>
    <item>
      <title>Flash stuck in "No device connected" when using mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flash-stuck-in-quot-No-device-connected-quot-when-using-mfgtool/m-p/1510491#M194192</link>
      <description>&lt;P&gt;I have an&amp;nbsp;&lt;SPAN&gt;i.MX 6ULL EVK and I want to flash the uboot, kernel... using mfgtool. I insert my empty microSD card and connect the USB OTG port to my computer. SW602 set to serial downloader mode and SW601 set to MicroSD. The mfgtool can recognize the USB port and start to load kernel successfully. But when it shows " jump to OS image" the USB port seems disappear and "No device connected" shows up. When I push the reset button, I get the same failure.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Aug 2022 02:12:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flash-stuck-in-quot-No-device-connected-quot-when-using-mfgtool/m-p/1510491#M194192</guid>
      <dc:creator>MadPony</dc:creator>
      <dc:date>2022-08-24T02:12:42Z</dc:date>
    </item>
    <item>
      <title>Re: Flash stuck in "No device connected" when using mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flash-stuck-in-quot-No-device-connected-quot-when-using-mfgtool/m-p/1511286#M194243</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Please help me providing the following information:&lt;BR /&gt;MFGTool version that you are using for flashing&lt;BR /&gt;Uboot version&lt;BR /&gt;Kernel version&lt;BR /&gt;Prebuilt image from NXP webpage or your own built image&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Aug 2022 22:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flash-stuck-in-quot-No-device-connected-quot-when-using-mfgtool/m-p/1511286#M194243</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-08-24T22:31:08Z</dc:date>
    </item>
    <item>
      <title>Re: Flash stuck in "No device connected" when using mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flash-stuck-in-quot-No-device-connected-quot-when-using-mfgtool/m-p/1511428#M194250</link>
      <description>&lt;P&gt;Mfgtool version is L4.9.88_2.0.0_mfg-tool&lt;/P&gt;&lt;P&gt;I did not add my uboot or kernel image to the file. I just clicked mfgtool2-yocto-mx-evk-sdcard-sd2.vbs and I guess it would flash the default images which already exist in the file, correct?&lt;/P&gt;</description>
      <pubDate>Thu, 25 Aug 2022 05:09:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flash-stuck-in-quot-No-device-connected-quot-when-using-mfgtool/m-p/1511428#M194250</guid>
      <dc:creator>MadPony</dc:creator>
      <dc:date>2022-08-25T05:09:44Z</dc:date>
    </item>
    <item>
      <title>Re: Flash stuck in "No device connected" when using mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flash-stuck-in-quot-No-device-connected-quot-when-using-mfgtool/m-p/1515032#M194555</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Yes, that is correct it should work that way, are you running the MFGTool in a windows 10 PC?&lt;BR /&gt;If yes is there any possibility to try on a windows 7 PC on your side?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 23:16:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flash-stuck-in-quot-No-device-connected-quot-when-using-mfgtool/m-p/1515032#M194555</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-08-31T23:16:24Z</dc:date>
    </item>
  </channel>
</rss>