<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: [iMX8X] lpi2c FIFO buffer sizes</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8X-lpi2c-FIFO-buffer-sizes/m-p/1509963#M194155</link>
    <description>&lt;P&gt;Ok thanks a lot for clarifications.&lt;/P&gt;&lt;P&gt;I have expected that 4 words is a hard limit and it was not possible to extend it.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 23 Aug 2022 07:00:08 GMT</pubDate>
    <dc:creator>ykrons</dc:creator>
    <dc:date>2022-08-23T07:00:08Z</dc:date>
    <item>
      <title>[iMX8X] lpi2c FIFO buffer sizes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8X-lpi2c-FIFO-buffer-sizes/m-p/1509522#M194117</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have recently done some testing with lpi2c i2c interface on a Toradex iMX8DX Colibri board and I have been surprised to see that the RX and TX FIFO size returned by PARAM register is of 16 words (I get 0x44) whereas the Reference Manual (Rev. 0, 05/2020) is reporting 4 words size in §12.3.1.1 and in 12.3.3.1.3.3 Reset values.&lt;/P&gt;&lt;P&gt;Is it a typo in the Reference Manual or did I wrongly interpret the value in PARAM ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 12:04:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8X-lpi2c-FIFO-buffer-sizes/m-p/1509522#M194117</guid>
      <dc:creator>ykrons</dc:creator>
      <dc:date>2022-08-22T12:04:13Z</dc:date>
    </item>
    <item>
      <title>Re: [iMX8X] lpi2c FIFO buffer sizes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8X-lpi2c-FIFO-buffer-sizes/m-p/1509792#M194137</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Yes, what the reference manual says is correct, but it seems that the Toradex implementation makes some arrangements to use 16 words.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Diego.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 01:24:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8X-lpi2c-FIFO-buffer-sizes/m-p/1509792#M194137</guid>
      <dc:creator>Juan-Rodarte</dc:creator>
      <dc:date>2022-08-23T01:24:42Z</dc:date>
    </item>
    <item>
      <title>Re: [iMX8X] lpi2c FIFO buffer sizes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8X-lpi2c-FIFO-buffer-sizes/m-p/1509963#M194155</link>
      <description>&lt;P&gt;Ok thanks a lot for clarifications.&lt;/P&gt;&lt;P&gt;I have expected that 4 words is a hard limit and it was not possible to extend it.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 07:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8X-lpi2c-FIFO-buffer-sizes/m-p/1509963#M194155</guid>
      <dc:creator>ykrons</dc:creator>
      <dc:date>2022-08-23T07:00:08Z</dc:date>
    </item>
  </channel>
</rss>