<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Pin mapping of GPIO7 is missing in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Pin-mapping-of-GPIO7-is-missing/m-p/1509898#M194150</link>
    <description>&lt;P&gt;Yes, there is no GPIO7.&lt;/P&gt;&lt;P&gt;This is the pads of i.mx8qm defined in the bsp.&lt;/P&gt;&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/include/dt-bindings/pinctrl/pads-imx8qm.h?h=imx_5.4.70_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/include/dt-bindings/pinctrl/pads-imx8qm.h?h=imx_5.4.70_2.3.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 23 Aug 2022 05:37:32 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2022-08-23T05:37:32Z</dc:date>
    <item>
      <title>Pin mapping of GPIO7 is missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-mapping-of-GPIO7-is-missing/m-p/1504479#M193705</link>
      <description>&lt;P&gt;Where can I find the pin mapping of GPIO7 for the iMX8QM.&lt;/P&gt;&lt;P&gt;GPIO7 is defined in the address map, but there is no pin mapping defined in the Chip IO section of the SOCs reference manual.&lt;/P&gt;&lt;P&gt;As I am running out of GPIO pins, this information would be highly appreciated...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 11 Aug 2022 04:39:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-mapping-of-GPIO7-is-missing/m-p/1504479#M193705</guid>
      <dc:creator>K_Steinhammer</dc:creator>
      <dc:date>2022-08-11T04:39:21Z</dc:date>
    </item>
    <item>
      <title>Re: Pin mapping of GPIO7 is missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-mapping-of-GPIO7-is-missing/m-p/1509898#M194150</link>
      <description>&lt;P&gt;Yes, there is no GPIO7.&lt;/P&gt;&lt;P&gt;This is the pads of i.mx8qm defined in the bsp.&lt;/P&gt;&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/include/dt-bindings/pinctrl/pads-imx8qm.h?h=imx_5.4.70_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/include/dt-bindings/pinctrl/pads-imx8qm.h?h=imx_5.4.70_2.3.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 05:37:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-mapping-of-GPIO7-is-missing/m-p/1509898#M194150</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-08-23T05:37:32Z</dc:date>
    </item>
    <item>
      <title>Re: Pin mapping of GPIO7 is missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-mapping-of-GPIO7-is-missing/m-p/1509946#M194153</link>
      <description>&lt;P&gt;OK, thanks for the confirmation...&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 06:45:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-mapping-of-GPIO7-is-missing/m-p/1509946#M194153</guid>
      <dc:creator>K_Steinhammer</dc:creator>
      <dc:date>2022-08-23T06:45:34Z</dc:date>
    </item>
  </channel>
</rss>