<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8QM using GPIO3_IO24 as GPIO</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-using-GPIO3-IO24-as-GPIO/m-p/1508121#M193983</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204516"&gt;@yusufbavas_t&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In the i.MX8QM series (and i.MX8QXP) the GPIOs are handled by &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-started/ta-p/1121153" target="_self"&gt;the SCFW&lt;/A&gt;. And you can refer to the &lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_SCFWKIT-1.2.7.1&amp;amp;appType=license&amp;amp;_gl=1*13w381*_ga*Mjc0NjA3MTA4LjE2NjA4MDU3MTc.*_ga_WM5LE0KMSH*MTY2MDgxMTczNy4yLjEuMTY2MDgxMTk1Ny4wLjAuMA.." target="_self"&gt;documentation here&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Please refer to &lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8-ADC-IN0-pin-can-t-set-as-GPIO-function/m-p/959866" target="_self"&gt;this similar&lt;/A&gt; case.&lt;/P&gt;
&lt;P&gt;Hope it helps!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Dhruvit.&lt;/P&gt;</description>
    <pubDate>Thu, 18 Aug 2022 08:41:47 GMT</pubDate>
    <dc:creator>Dhruvit</dc:creator>
    <dc:date>2022-08-18T08:41:47Z</dc:date>
    <item>
      <title>IMX8QM using GPIO3_IO24 as GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-using-GPIO3-IO24-as-GPIO/m-p/1499519#M193311</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to use&amp;nbsp;GPIO3_IO24 pin as input, but i always read state low. I can use&amp;nbsp;GPIO5_IO16 pin without any problem but in&amp;nbsp;GPIO3_IO24, i always read 0 no matter the pin state. I tried to define pin in DTS&amp;nbsp;or define it in /sys/class/gpio folder (like described in &lt;A href="https://variwiki.com/index.php?title=MX8M_GPIO#Using_a_command_line_or_a_script" target="_blank" rel="noopener"&gt;https://variwiki.com/index.php?title=MX8M_GPIO#Using_a_command_line_or_a_script&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;I tried to define pin as output. In this situation, i measure pin state is always high and it is not changed. I can't control pin neither input nor output mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In datasheet, pin has 2 configurations controlled by other 2 pins (GPIO2_16 and GPIO2_7). I tried all alternatives in this configurations but result is same.&lt;/P&gt;&lt;P&gt;Am i doing something wrong, how do i use this pin as GPIO ?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Kernel version : 5.4.47 (android 10)&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 11:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-using-GPIO3-IO24-as-GPIO/m-p/1499519#M193311</guid>
      <dc:creator>yusufbavas_t</dc:creator>
      <dc:date>2022-08-02T11:01:28Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM using GPIO3_IO24 as GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-using-GPIO3-IO24-as-GPIO/m-p/1508121#M193983</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204516"&gt;@yusufbavas_t&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In the i.MX8QM series (and i.MX8QXP) the GPIOs are handled by &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-started/ta-p/1121153" target="_self"&gt;the SCFW&lt;/A&gt;. And you can refer to the &lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_SCFWKIT-1.2.7.1&amp;amp;appType=license&amp;amp;_gl=1*13w381*_ga*Mjc0NjA3MTA4LjE2NjA4MDU3MTc.*_ga_WM5LE0KMSH*MTY2MDgxMTczNy4yLjEuMTY2MDgxMTk1Ny4wLjAuMA.." target="_self"&gt;documentation here&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Please refer to &lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8-ADC-IN0-pin-can-t-set-as-GPIO-function/m-p/959866" target="_self"&gt;this similar&lt;/A&gt; case.&lt;/P&gt;
&lt;P&gt;Hope it helps!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Dhruvit.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Aug 2022 08:41:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-using-GPIO3-IO24-as-GPIO/m-p/1508121#M193983</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2022-08-18T08:41:47Z</dc:date>
    </item>
  </channel>
</rss>