<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDistro with NO GPU</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Distro-with-NO-GPU/m-p/1506117#M193850</link>
    <description>&lt;P&gt;I am currently using imx8mn-ddr4-evk with with&amp;nbsp;fsl-imx-xwayland distro and &lt;STRONG&gt;imx-image-core&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;My Target board application processor will have 1 core only with no GPU,no screen, no touchscreen, no audio in nor audio out.&lt;/P&gt;&lt;P&gt;I have updated the kernel device tree accordingly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have noticed the ditro still have the following services running:&lt;/P&gt;&lt;P&gt;psplash-basic&lt;BR /&gt;psplash-network&lt;BR /&gt;psplash-quit&lt;BR /&gt;psplash-systemd&lt;BR /&gt;weston&lt;/P&gt;&lt;P&gt;what is the way to modify the distro so it wont install these elements to the distro ?&lt;/P&gt;&lt;P&gt;is there any pros of having as part of the distro ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Roy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 15 Aug 2022 09:19:14 GMT</pubDate>
    <dc:creator>razriel</dc:creator>
    <dc:date>2022-08-15T09:19:14Z</dc:date>
    <item>
      <title>Distro with NO GPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Distro-with-NO-GPU/m-p/1506117#M193850</link>
      <description>&lt;P&gt;I am currently using imx8mn-ddr4-evk with with&amp;nbsp;fsl-imx-xwayland distro and &lt;STRONG&gt;imx-image-core&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;My Target board application processor will have 1 core only with no GPU,no screen, no touchscreen, no audio in nor audio out.&lt;/P&gt;&lt;P&gt;I have updated the kernel device tree accordingly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have noticed the ditro still have the following services running:&lt;/P&gt;&lt;P&gt;psplash-basic&lt;BR /&gt;psplash-network&lt;BR /&gt;psplash-quit&lt;BR /&gt;psplash-systemd&lt;BR /&gt;weston&lt;/P&gt;&lt;P&gt;what is the way to modify the distro so it wont install these elements to the distro ?&lt;/P&gt;&lt;P&gt;is there any pros of having as part of the distro ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Roy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Aug 2022 09:19:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Distro-with-NO-GPU/m-p/1506117#M193850</guid>
      <dc:creator>razriel</dc:creator>
      <dc:date>2022-08-15T09:19:14Z</dc:date>
    </item>
    <item>
      <title>Re: Distro with NO GPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Distro-with-NO-GPU/m-p/1506844#M193908</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You need weston if you are going to use Wayland, the ps* can be eliminated if you are not going to use LCD, eliminated from Kernel and device tree.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 16 Aug 2022 13:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Distro-with-NO-GPU/m-p/1506844#M193908</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-08-16T13:38:09Z</dc:date>
    </item>
    <item>
      <title>Re: Distro with NO GPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Distro-with-NO-GPU/m-p/1506902#M193911</link>
      <description>&lt;P&gt;I do not intend to use wayland my question is how do I eliminate parts of the distro without breaking stuff.&lt;/P&gt;</description>
      <pubDate>Tue, 16 Aug 2022 14:55:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Distro-with-NO-GPU/m-p/1506902#M193911</guid>
      <dc:creator>razriel</dc:creator>
      <dc:date>2022-08-16T14:55:40Z</dc:date>
    </item>
  </channel>
</rss>