<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1505125#M193746</link>
    <description>&lt;P&gt;You may be using the core-image-minimal. Can you start a new yocto build with&amp;nbsp;imx-image-multimedia or imx-image-full?&lt;/P&gt;
&lt;P&gt;Alternatively, you could use the prebuilt images to test this also from here:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=L5.4.70_2.3.0_MX8QM&amp;amp;appType=license" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=L5.4.70_2.3.0_MX8QM&amp;amp;appType=licens&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Then you could build the kernel sources from here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx&amp;nbsp;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;branch: remotes/origin/imx_5.4.70_2.3.0&lt;/P&gt;
&lt;P&gt;Remember to apply the patch attached here. I found the dts file was missing - &amp;nbsp;sorry. So use this patch!&lt;/P&gt;
&lt;P&gt;And Finally set the boot environment:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;=&amp;gt; setenv fdt_file imx8qm-mek-jdi-wuxga-lvds0-lvds1-panel-hdmi.dtb &lt;BR /&gt;=&amp;gt; saveenv&lt;BR /&gt;Saving Environment to MMC... Writing to MMC(1)... OK&lt;BR /&gt;=&amp;gt; boot&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Oliver&lt;/P&gt;</description>
    <pubDate>Thu, 11 Aug 2022 16:57:30 GMT</pubDate>
    <dc:creator>OliverB</dc:creator>
    <dc:date>2022-08-11T16:57:30Z</dc:date>
    <item>
      <title>iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1497355#M193166</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have built a yocto distro for fsl-imx-xwayland and iMX8QM-MEK machine with v5.4.70 kernel version as below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="yocto_imx8qm-mek.jpeg" style="width: 686px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/188269iBBE72ACED9CF5F06/image-size/large?v=v2&amp;amp;px=999" role="button" title="yocto_imx8qm-mek.jpeg" alt="yocto_imx8qm-mek.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I wish to output from 3 panels: 2 of them are LVDS outputs and 1 of them is HDMI output, all of them at the same time.&lt;/P&gt;&lt;P&gt;2 x panels have physical resolution &lt;A href="mailto:1920x1080@60" target="_blank" rel="noopener"&gt;1920x720@60&lt;/A&gt; and connected to iMX8QM-MEK eboard via LVDS lines with dual mode as represented figure below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="iMX8QM-MEK_LVDS_connection.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/188275i54301230C152A356/image-size/large?v=v2&amp;amp;px=999" role="button" title="iMX8QM-MEK_LVDS_connection.png" alt="iMX8QM-MEK_LVDS_connection.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;1 x panel has physical resolution &lt;A href="mailto:1920x1080@60" target="_blank" rel="noopener"&gt;2400x900@60&lt;/A&gt; and connected to iMX8QM-MEK eboard via HDMI port.&lt;/P&gt;&lt;P&gt;* When I use the attached DTS file &lt;SPAN class=""&gt;&lt;STRONG&gt;imx8qm-mek-hdmi.dts.txt, &lt;/STRONG&gt;&lt;A href="mailto:2400x900@60" target="_blank" rel="noopener"&gt;2400x900@60&lt;/A&gt; panel works fine which is connected to HDMI port. But there are no outputs on LVDS panels.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;* When I use the attached DTS files &lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;STRONG&gt;imx8qm-mek-jdi-wuxga-lvds1-panel.dts.txt&lt;/STRONG&gt; and &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN class=""&gt;imx8qm-mek-jdi-wuxga-lvds1-panel.dts&lt;/SPAN&gt;i, &lt;/STRONG&gt;both 1920x720 LVDS panels work fine but there is no output on &lt;A href="mailto:2400x900@60" target="_blank" rel="noopener"&gt;2400x900@60&lt;/A&gt; panel which is connected to HDMI port. If I unplug the HDMI connection from &lt;A href="mailto:2400x900@60" target="_blank" rel="noopener"&gt;2400x900@60&lt;/A&gt; panel and plug a standard &lt;A href="mailto:1280x720@60" target="_blank" rel="noopener"&gt;1280x720@60&lt;/A&gt; PC monitor via HDMI port, there is an output (works fine) on that PC monitor.&lt;/P&gt;&lt;P&gt;On the other hand, I have set the u-boot &lt;STRONG&gt;bootargs&lt;/STRONG&gt; variable to adjust the HDMI output setting as below.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;bootargs=root=/dev/mmcblk0p1 rootwait rw video=mxcdi0fb:RGB24,2400x900M@60,hdmi video=mxcdi1fb:RGB666,XGA,di0_primary ldb=di1 ip=none&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;How can I output from all of the panels (2 x LVDS &lt;A href="mailto:1920x720@60" target="_blank" rel="noopener"&gt;1920x720@60&lt;/A&gt; and 1 x HDMI &lt;A href="mailto:2400x900@60" target="_blank" rel="noopener"&gt;2400x900@60&lt;/A&gt;) at the same time. What should be the rootcause of that problem ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;STRONG&gt;Note&lt;/STRONG&gt;: DTS files are attached.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jul 2022 13:40:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1497355#M193166</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-07-28T13:40:08Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1501797#M193496</link>
      <description>&lt;P&gt;&lt;A href="mailto:oliver.brown@nxp.com" target="_blank"&gt;@Oliver Brown&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Aug 2022 12:08:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1501797#M193496</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-08-05T12:08:39Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1501800#M193498</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Aug 2022 12:18:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1501800#M193498</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-08-05T12:18:36Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1501949#M193508</link>
      <description>&lt;P&gt;I made the patch below for&amp;nbsp;imx8qm-mek-jdi-wuxga-lvds1-panel-rpmsg.dts and I can get the LVDS panel on LVDS1 and HDMI working together.&lt;/P&gt;
&lt;P&gt;$ git diff&lt;BR /&gt;diff --git a/arch/arm64/boot/dts/freescale/imx8qm-mek-jdi-wuxga-lvds1-panel-rpmsg.dts b/arch/arm64/boot/dts/freescale/imx8qm-mek-jdi-wuxga-lvds1-panel-rpmsg.dts&lt;BR /&gt;index b57423235fc7..37b0ccfe5d4f 100644&lt;BR /&gt;--- a/arch/arm64/boot/dts/freescale/imx8qm-mek-jdi-wuxga-lvds1-panel-rpmsg.dts&lt;BR /&gt;+++ b/arch/arm64/boot/dts/freescale/imx8qm-mek-jdi-wuxga-lvds1-panel-rpmsg.dts&lt;BR /&gt;@@ -4,5 +4,5 @@&lt;BR /&gt;* Copyright 2020 NXP&lt;BR /&gt;*/&lt;BR /&gt;&lt;BR /&gt;-#include "imx8qm-mek-rpmsg.dts"&lt;BR /&gt;+#include "imx8qm-mek-hdmi.dts"&lt;BR /&gt;#include "imx8qm-mek-jdi-wuxga-lvds1-panel.dtsi"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The problem getting LVDS0 and HDMI working is that in our default configuration display controller 0 is set to be used by HDMI only. So both display pipes are configured to be used by the HDMI. It should be possible to split the display controller to use one pipe for HDMI and one pipe for LVDS. I'll investigate what changes are required.&lt;/P&gt;
&lt;P&gt;Is it possible to MIPI &amp;nbsp;DSI1 for your use case? The default&amp;nbsp;imx8qm-mek-default.dts supports HDMI, LVDS1 and MIPI DSI1 (LVDS0 and MIPI DSI0 are disabled).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Oliver&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Aug 2022 18:17:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1501949#M193508</guid>
      <dc:creator>OliverB</dc:creator>
      <dc:date>2022-08-05T18:17:46Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1502017#M193510</link>
      <description>&lt;P&gt;I was able to get HDMI working with LVDS0 and LVDS1. The HDMI display needs to be limited to 2560 pixels or less and less than 300MHz pixel clock. Otherwise LVDS0 will not have a display. In this patch I also had to disable hdmi audio due to a probe conflict. Let me know if this is working for you.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Fri, 05 Aug 2022 22:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1502017#M193510</guid>
      <dc:creator>OliverB</dc:creator>
      <dc:date>2022-08-05T22:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1502120#M193522</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/7093"&gt;@OliverB&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;Firstly, thanks for your quick reply, this issue is so urgent and important to me.&lt;/P&gt;&lt;P&gt;I have applied your patch and 1 HDMI and 2 LVDS work now. However still I have a problem. Now just I can get 1920x1080 resolution from HDMI; but I need 2400x900 like FHD+. Without your patch if I use imx8qm-mek-hdmi.dtb, HDMI (2400x900) works; but not any LVDS. If I use imx8qm-mek-jdi-wuxga-lvds1-panel.dtb, just 2 LVDS work, no HDMI. When I apply your patch 2 LVDS OK; just HDMI (1920x1080) OK, not 2400x900. What is the reason of not working 2400x900 with LVDSs and how can I solve this problem? Or is this case possible?&lt;BR /&gt;&lt;BR /&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Aug 2022 05:23:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1502120#M193522</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-08-08T05:23:37Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1502667#M193582</link>
      <description>&lt;P&gt;Hi Nevozade,&lt;/P&gt;
&lt;P&gt;I'm not sure why it is not working for your resolution. Can you you provide the EDID from you 2400x900 monitor? You can just provide the output of "modtest" from when your monitor is working in HDMI mode. I'll have to set this mode on my analyzer and see what is causing the problem. Both the display controller driver and HDMI Driver should allow this mode in a single display pipe. It's possible "1920" &amp;nbsp;is hardcoded somewhere in the drivers.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Oliver&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Aug 2022 15:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1502667#M193582</guid>
      <dc:creator>OliverB</dc:creator>
      <dc:date>2022-08-08T15:22:02Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1502707#M193584</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/7093"&gt;@OliverB&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;Actually, we analyzed the EDID of our monitor before and we saw that 2400x900.&amp;nbsp;According to your request, I am sending you the edid file for you to analyze and find the problem.&amp;nbsp;I am asking for your support in this matter. (I attach the file as .zip because the .bin extension has failed to upload)&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Nevzat&lt;/P&gt;</description>
      <pubDate>Mon, 08 Aug 2022 16:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1502707#M193584</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-08-08T16:24:32Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503383#M193628</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I verified that HDMI 2400x900 and two LVDS 1920x1200 can work with your edid and 0001-arm64-boot-dts-freescale-Add-configuration-for-two-L.patch. I did not need any uboot changes or weston.ini changes. I also previously verified that 2560 width can work, this would be the upper limit of the width for a single display pipe.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Also the settings below are not for iMX8QM and should not be used:&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE&gt;video=mxcdi0fb:RGB24,2400x900M@60,hdmi video=mxcdi1fb:RGB666,XGA,di0_primary ldb=di1 &lt;/PRE&gt;&lt;P&gt;These are for iMX6DQ with IPUv3.&amp;nbsp;&lt;/P&gt;&lt;P&gt;To force a DRM mode the form should be&amp;nbsp;&lt;/P&gt;&lt;P&gt;video=HDMI-A-1:2400x900-32@60&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My patch supports the dual-channel 1920x1200 NXP display panel, so some change would be needed to get change the panel and disable dual channel mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 14:56:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503383#M193628</guid>
      <dc:creator>OliverB</dc:creator>
      <dc:date>2022-08-09T14:56:24Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503384#M193629</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/7093"&gt;@OliverB&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Even I use your patch, HDMI 2400x900 and LVDS not working for me. If I disabled&amp;nbsp;&lt;A href="mailto:lvds-channel@0" target="_blank"&gt;lvds-channel@0&lt;/A&gt;&amp;nbsp;HDMI works. If I make "okay"&amp;nbsp;&lt;A href="mailto:lvds-channel@0" target="_blank"&gt;lvds-channel@0&lt;/A&gt;&amp;nbsp;LVDS works. It seems when HDMI starts to work LVDS disabled automatically. You can my final dts as attached. What is the reason of this issue?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 15:07:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503384#M193629</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-08-09T15:07:36Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503417#M193631</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/7093"&gt;@OliverB&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Although I think I'm doing it right, just in case could you zip and share the &lt;STRONG&gt;freescale&lt;/STRONG&gt; folder (including dts and dtsis) in build/tmp/work-shared/imx8qmmek/kernel-source/arch/arm64/boot/dts/ path with me? I want to make sure I'm doing the same thing you did before I move forward.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 16:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503417#M193631</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-08-09T16:03:02Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503422#M193632</link>
      <description>&lt;P&gt;Can you provide the full log from powerup to the linux prompt?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 16:05:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503422#M193632</guid>
      <dc:creator>OliverB</dc:creator>
      <dc:date>2022-08-09T16:05:54Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503430#M193634</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/7093"&gt;@OliverB&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The case that 2 LVDS panels work together, but HDMI (2400x900) does not work -&amp;gt; &lt;STRONG&gt;lvds.log&lt;/STRONG&gt; and &lt;STRONG&gt;imx8qm-mek-jdi-wuxga-lvds1-panel-LVDS.dtsi&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;The case that HDMI (2400x900) works, but no display on LVDS panels -&amp;gt; &lt;STRONG&gt;hdmi.log&lt;/STRONG&gt; and &lt;STRONG&gt;imx8qm-mek-jdi-wuxga-lvds1-panel-HDMI.dtsi&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;All specified files exist in the attached zip file.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nevzat.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 16:13:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503430#M193634</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-08-09T16:13:00Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503447#M193635</link>
      <description>&lt;P&gt;Can you try this file? The LVDS nodes were disabled.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;All three display are working with this file included as follows:&lt;/P&gt;
&lt;P&gt;&lt;FONT face="courier new,courier"&gt;--- a/arch/arm64/boot/dts/freescale/imx8qm-mek-jdi-wuxga-lvds1-panel.dts&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;+++ b/arch/arm64/boot/dts/freescale/imx8qm-mek-jdi-wuxga-lvds1-panel.dts&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;@@ -5,4 +5,4 @@&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;*/&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;#include "imx8qm-mek.dts"&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;-#include "imx8qm-mek-jdi-wuxga-lvds1-panel.dtsi"&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;+#include "imx8qm-mek-jdi-wuxga-lvds1-panel-HDMI-fixed.dtsi"&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 17:13:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503447#M193635</guid>
      <dc:creator>OliverB</dc:creator>
      <dc:date>2022-08-09T17:13:57Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503454#M193637</link>
      <description>&lt;P&gt;Here are the device tree files. I hope they helps.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Oliver&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 17:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503454#M193637</guid>
      <dc:creator>OliverB</dc:creator>
      <dc:date>2022-08-09T17:29:36Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503736#M193656</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/7093"&gt;@OliverB&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Sorry, due to local time difference, I have just tried your suggestions.&lt;BR /&gt;&lt;BR /&gt;Firstly, I changed&amp;nbsp;imx8qm-mek-jdi-wuxga-lvds1-panel.dts file as you said (changed include file) with your attached dtsi file. Then, I make dtb files and write to SD card. However, although I set different dtb files on booting many times, there is no display at the same time LVDS and HDMI panels.&amp;nbsp;Even the HDMI with imx8qm-mek-hdmi.dtb that worked with us did not work with your dtb. Only way to get view on HDMI is disabling lvds-channel0, which gives HDMI output but closes LVDS panels.&lt;BR /&gt;&lt;BR /&gt;Secondly, I copy your freescale folder by overwriting mine. Then, write them into SD card but there is no change with the display issue. I set different fdt_file on booting such as imx8qm-mek-jdi-wuxga-panel.dtb, imx8qm-mek-hdmi.dtb, and imx8qm-mek-jdi-wuxga-lvds0-lvds1-hdmi.dtb , nothing changes. The HDMI monitor that you have is acting different from ours in my opinion. Any other suggestion?&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nevzat&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 06:53:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1503736#M193656</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-08-10T06:53:38Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1504092#M193677</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tempsnip.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/189829i28328ACE49C92FA1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tempsnip.png" alt="tempsnip.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;We cannot meet the criteria I show in the figure. What do I need to do to provide the resolutions in the options given here?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Even though I took 2 LVDS and HDMI together, it was not possible to reach the resolutions I wanted and shown in the figure.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 15:10:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1504092#M193677</guid>
      <dc:creator>tuncayyldrm</dc:creator>
      <dc:date>2022-08-10T15:10:32Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1504107#M193678</link>
      <description>&lt;P&gt;Can you provide the source for the slide "Seeris Display Output Capabilities"?&lt;/P&gt;&lt;P&gt;Can you also provide video mode definitions and/or EDIDs for the displays that you tried?&lt;/P&gt;&lt;P&gt;The current driver has a single display pipe width limit of 2560 pixels. This means that 2 2560 width displays are possible on a single display pipe. Which also means that up to 3 or 4 2560 width displays are possible. Or one larger display up to 5120 pixel width and two displays up to 2560 width.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 15:24:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1504107#M193678</guid>
      <dc:creator>OliverB</dc:creator>
      <dc:date>2022-08-10T15:24:17Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1504142#M193680</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/7093"&gt;@OliverB&lt;/a&gt;&amp;nbsp; ,&lt;/P&gt;&lt;P&gt;We are trying to get at least 2 panels (one of them HDMI, one of them LVDS). Now 1 LVDS(1920x720) and 1 HDMI(1920x720) work fine. However when we changed HDMI with 2400x900 monitor, there is no image in the monitor. You can see reference slide as attached. Could you please give a way to find root cause of this issue?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 16:33:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1504142#M193680</guid>
      <dc:creator>hkaracali</dc:creator>
      <dc:date>2022-08-10T16:33:34Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM-MEK HDMI Output 2400x900@60 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1504171#M193685</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/7093"&gt;@OliverB&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;We had already shared the EDID of our panel you before as zipped file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 17:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-HDMI-Output-2400x900-60-Problem/m-p/1504171#M193685</guid>
      <dc:creator>nevozade</dc:creator>
      <dc:date>2022-08-10T17:39:45Z</dc:date>
    </item>
  </channel>
</rss>