<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8dx linux driver v4l2 Support NV21 format</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1503132#M193613</link>
    <description>&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;I now hope that the v4l2 driver of imx8dx can support the format of V4L2_PIX_FMT_NV21, how do I need to modify it to achieve this function. I see that the driver already supports the V4L2_PIX_FMT_NV12 format.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Tue, 09 Aug 2022 08:50:18 GMT</pubDate>
    <dc:creator>songhongliang</dc:creator>
    <dc:date>2022-08-09T08:50:18Z</dc:date>
    <item>
      <title>imx8dx linux driver v4l2 Support NV21 format</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1503132#M193613</link>
      <description>&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;I now hope that the v4l2 driver of imx8dx can support the format of V4L2_PIX_FMT_NV21, how do I need to modify it to achieve this function. I see that the driver already supports the V4L2_PIX_FMT_NV12 format.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 08:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1503132#M193613</guid>
      <dc:creator>songhongliang</dc:creator>
      <dc:date>2022-08-09T08:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx8dx linux driver v4l2 Support NV21 format</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1504731#M193721</link>
      <description>&lt;P&gt;I don't know capture or output you mean, I assume that you mean capture, so do you mean your input video is format NV21?&lt;/P&gt;</description>
      <pubDate>Thu, 11 Aug 2022 08:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1504731#M193721</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-08-11T08:24:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx8dx linux driver v4l2 Support NV21 format</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1504793#M193725</link>
      <description>&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Yes, it is capture, I am using AHD to mipi chip bridge, I see that 9 capture formats are already supported in the imx8-isi-cap.c file, but format NV21 is not supported.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I hope that the video stream in NV21 format can be directly obtained in the application.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Aug 2022 09:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1504793#M193725</guid>
      <dc:creator>songhongliang</dc:creator>
      <dc:date>2022-08-11T09:01:04Z</dc:date>
    </item>
    <item>
      <title>Re: imx8dx linux driver v4l2 Support NV21 format</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1507421#M193939</link>
      <description>&lt;P&gt;the format from chip bridge is NV21 or you need to convert the input video to NV21?&lt;/P&gt;</description>
      <pubDate>Wed, 17 Aug 2022 09:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1507421#M193939</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-08-17T09:58:53Z</dc:date>
    </item>
    <item>
      <title>Re: imx8dx linux driver v4l2 Support NV21 format</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1507915#M193973</link>
      <description>&lt;P&gt;&lt;SPAN&gt;need to convert the input video to NV21&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Aug 2022 02:46:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1507915#M193973</guid>
      <dc:creator>songhongliang</dc:creator>
      <dc:date>2022-08-18T02:46:36Z</dc:date>
    </item>
    <item>
      <title>Re: imx8dx linux driver v4l2 Support NV21 format</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1512968#M194381</link>
      <description>&lt;P&gt;what is your real capture data? do you need convert raw data to NV12? if yes, you can use software ISP do this,&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12060.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12060.pdf&lt;/A&gt;"&lt;/P&gt;</description>
      <pubDate>Mon, 29 Aug 2022 07:46:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-linux-driver-v4l2-Support-NV21-format/m-p/1512968#M194381</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-08-29T07:46:22Z</dc:date>
    </item>
  </channel>
</rss>