<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: UART functionality without RTS &amp;amp; CTS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UART-functionality-without-RTS-amp-CTS/m-p/1501305#M193452</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Yes is possible, For custom design board you may disable the hardware flow control operations through software configurations.But in the&lt;/P&gt;</description>
    <pubDate>Thu, 04 Aug 2022 17:52:56 GMT</pubDate>
    <dc:creator>KalaimaniArumugamdev</dc:creator>
    <dc:date>2022-08-04T17:52:56Z</dc:date>
    <item>
      <title>UART functionality without RTS &amp; CTS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-functionality-without-RTS-amp-CTS/m-p/1501287#M193451</link>
      <description>&lt;P&gt;We have a custom board design with i.MX 8M Nano processor. In this we are using all the 3/4 UART instances.&amp;nbsp;&lt;/P&gt;&lt;P&gt;UART3_RXD - E18&lt;BR /&gt;UART3_TXD - D18&lt;/P&gt;&lt;P&gt;We have not connected RTS &amp;amp; CTS as we don't require hardware flow control.&lt;/P&gt;&lt;P&gt;Is it possible to connect the UART without RTS and CTS?&lt;/P&gt;</description>
      <pubDate>Thu, 04 Aug 2022 17:12:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-functionality-without-RTS-amp-CTS/m-p/1501287#M193451</guid>
      <dc:creator>Pavithra31R</dc:creator>
      <dc:date>2022-08-04T17:12:12Z</dc:date>
    </item>
    <item>
      <title>Re: UART functionality without RTS &amp; CTS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-functionality-without-RTS-amp-CTS/m-p/1501305#M193452</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Yes is possible, For custom design board you may disable the hardware flow control operations through software configurations.But in the&lt;/P&gt;</description>
      <pubDate>Thu, 04 Aug 2022 17:52:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-functionality-without-RTS-amp-CTS/m-p/1501305#M193452</guid>
      <dc:creator>KalaimaniArumugamdev</dc:creator>
      <dc:date>2022-08-04T17:52:56Z</dc:date>
    </item>
  </channel>
</rss>